Confirmation message body.
Public Attributes#
int32_t
Error code.
IP address of the remote peer.
uint16_t
Port number of the remote peer.
uint32_t
ID of the new connected socket.
uint16_t
Reserved, set to zero.
uint32_t
Status of the request.
Public Attribute Documentation#
remote_address#
in6_addr_t sl_wisun_msg_accept_on_socket_cnf_body_t::remote_address
IP address of the remote peer.
remote_port#
uint16_t sl_wisun_msg_accept_on_socket_cnf_body_t::remote_port
Port number of the remote peer.
remote_socket_id#
uint32_t sl_wisun_msg_accept_on_socket_cnf_body_t::remote_socket_id
ID of the new connected socket.