Request message body.

Public Attributes#

uint8_t

Maximum number of asynchronous solicitation sequences.

uint32_t

Pairwise Master Key (PMK) ID.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

mac_address#

sl_wisun_mac_address_t sl_wisun_msg_connect_to_direct_connect_server_req_body_t::mac_address

Server MAC address.


max_solicits_count#

uint8_t sl_wisun_msg_connect_to_direct_connect_server_req_body_t::max_solicits_count

Maximum number of asynchronous solicitation sequences.


pmk_id#

uint32_t sl_wisun_msg_connect_to_direct_connect_server_req_body_t::pmk_id

Pairwise Master Key (PMK) ID.


reserved#

uint8_t sl_wisun_msg_connect_to_direct_connect_server_req_body_t::reserved[3]

Reserved, set to zero.