Confirmation message body.

Public Attributes#

uint8_t

Number of neighbors read.

uint8_t

Reserved, set to zero.

uint32_t

Status of the request.

Public Attribute Documentation#

neighbor_count#

uint8_t sl_wisun_msg_get_neighbors_cnf_body_t::neighbor_count

Number of neighbors read.


neighbor_mac_addresses#

sl_wisun_mac_address_t sl_wisun_msg_get_neighbors_cnf_body_t::neighbor_mac_addresses[]

Neighbor MAC addresses read.


reserved#

uint8_t sl_wisun_msg_get_neighbors_cnf_body_t::reserved[3]

Reserved, set to zero.


status#

uint32_t sl_wisun_msg_get_neighbors_cnf_body_t::status

Status of the request.