Confirmation message body.
Public Attributes#
uint8_t
Indicate if the device is supporting MAC mode switch Feature currently unsupported.
uint8_t
Number of PhyModeId to configure.
uint8_t
List of phy_mode_id_count PhyModeId.
uint8_t
Reserved, set to zero.
uint32_t
Status of the request.
Public Attribute Documentation#
is_mdr_command_capable#
uint8_t sl_wisun_msg_get_pom_ie_cnf_body_t::is_mdr_command_capable
Indicate if the device is supporting MAC mode switch Feature currently unsupported.
Must be set to 0.
phy_mode_id_count#
uint8_t sl_wisun_msg_get_pom_ie_cnf_body_t::phy_mode_id_count
Number of PhyModeId to configure.
phy_mode_ids#
uint8_t sl_wisun_msg_get_pom_ie_cnf_body_t::phy_mode_ids[SL_WISUN_MAX_PHY_MODE_ID_COUNT]
List of phy_mode_id_count PhyModeId.