Confirmation message body.

Public Attributes#

uint8_t

option value

int32_t

Error code.

uint16_t

Socket option length.

uint16_t

reserved, set to zero

uint32_t

Status of the request.

Public Attribute Documentation#

data#

uint8_t sl_wisun_msg_get_socket_option_cnf_body_t::data[]

option value


error_code#

int32_t sl_wisun_msg_get_socket_option_cnf_body_t::error_code

Error code.


option_length#

uint16_t sl_wisun_msg_get_socket_option_cnf_body_t::option_length

Socket option length.


reserved#

uint16_t sl_wisun_msg_get_socket_option_cnf_body_t::reserved

reserved, set to zero


status#

uint32_t sl_wisun_msg_get_socket_option_cnf_body_t::status

Status of the request.