Confirmation message body.

Public Attributes#

int32_t

Amount of data sent in bytes Equal to SOCKET_RETVAL_ERROR in case of failure.

int32_t

Error code.

uint32_t

Status of the request.

Public Attribute Documentation#

data_length#

int32_t sl_wisun_msg_send_on_socket_cnf_body_t::data_length

Amount of data sent in bytes Equal to SOCKET_RETVAL_ERROR in case of failure.


error_code#

int32_t sl_wisun_msg_send_on_socket_cnf_body_t::error_code

Error code.


status#

uint32_t sl_wisun_msg_send_on_socket_cnf_body_t::status

Status of the request.