Request message body.

Public Attributes#

uint32_t

The listening interval desired to be used by the LFN in milliseconds.

uint32_t

Time to advance the beginning of the LFN’s Unicast Listening Interval in milliseconds.

Public Attribute Documentation#

listening_interval_ms#

uint32_t sl_wisun_msg_set_lfn_timings_req_body_t::listening_interval_ms

The listening interval desired to be used by the LFN in milliseconds.


listening_offset_ms#

uint32_t sl_wisun_msg_set_lfn_timings_req_body_t::listening_offset_ms

Time to advance the beginning of the LFN’s Unicast Listening Interval in milliseconds.


mac_address#

sl_wisun_mac_address_t sl_wisun_msg_set_lfn_timings_req_body_t::mac_address

LFN's EUI-64.