You are viewing documentation for version:2.13.0 (latest)PDFRequest message body. Public Attributes#uint8_tphy_mode_idPHY mode ID. uint8_treservedReserved, set to zero. int16_tsensitivity_dbmSensitivity in dBm. Public Attribute Documentation#phy_mode_id#uint8_t sl_wisun_msg_set_phy_sensitivity_req_body_t::phy_mode_idPHY mode ID. reserved#uint8_t sl_wisun_msg_set_phy_sensitivity_req_body_t::reserved[1]Reserved, set to zero. sensitivity_dbm#int16_t sl_wisun_msg_set_phy_sensitivity_req_body_t::sensitivity_dbmSensitivity in dBm.