You are viewing documentation for version:2.13.0 (latest)PDFRequest message body. Public Attributes#sl_wisun_mac_address_tneighborNeighbor MAC address. uint8_treservedReserved, set to zero. uint8_ttypeIndicate the rate algorithm type. Public Attribute Documentation#neighbor#sl_wisun_mac_address_t sl_wisun_msg_set_rate_algorithm_id_req_body_t::neighborNeighbor MAC address. reserved#uint8_t sl_wisun_msg_set_rate_algorithm_id_req_body_t::reserved[3]Reserved, set to zero. type#uint8_t sl_wisun_msg_set_rate_algorithm_id_req_body_t::typeIndicate the rate algorithm type.