Confirmation message body.

Public Attributes#

int32_t

error code

Remote IP address.

int32_t

Remote port.

uint32_t

Status of the request.

Public Attribute Documentation#

error_code#

int32_t sl_wisun_msg_socket_getpeername_cnf_body_t::error_code

error code


remote_address#

in6_addr_t sl_wisun_msg_socket_getpeername_cnf_body_t::remote_address

Remote IP address.


remote_port#

int32_t sl_wisun_msg_socket_getpeername_cnf_body_t::remote_port

Remote port.


status#

uint32_t sl_wisun_msg_socket_getpeername_cnf_body_t::status

Status of the request.