Confirmation message body.

Public Attributes#

int16_t

Number of bytes received;.

int32_t

code of the error

uint16_t

reserved, set to zero

uint32_t

Status of the request.

Public Attribute Documentation#

data_length#

int16_t sl_wisun_msg_socket_recvmsg_cnf_body_t::data_length

Number of bytes received;.


error_code#

int32_t sl_wisun_msg_socket_recvmsg_cnf_body_t::error_code

code of the error


reserved#

uint16_t sl_wisun_msg_socket_recvmsg_cnf_body_t::reserved

reserved, set to zero


status#

uint32_t sl_wisun_msg_socket_recvmsg_cnf_body_t::status

Status of the request.