WakeUp#
Modules#
Typedefs#
Functions#
Transmits a Wake Up Notification command and handles callback.
Used by the WakeUp Command Class configuration Returns with the default sleep time in second between Wake Up Notifications.
Used by the WakeUp Command Class configuration Returns with the minimum sleep time in second between Wake Up Notifications.
Used by the WakeUp Command Class configuration Returns with the maximum sleep time in second between Wake Up Notifications.
Used by the WakeUp Command Class configuration Returns with the sleep step time in second.
Macros#
Function Documentation#
CC_WakeUp_notification_tx#
void CC_WakeUp_notification_tx (void(*)(uint8_t txStatus, TX_STATUS_TYPE *pExtendedTxStatus) pCallback)
Transmits a Wake Up Notification command and handles callback.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void(*)(uint8_t txStatus, TX_STATUS_TYPE *pExtendedTxStatus) | [in] | pCallback | Pointer to function which will be called on Wake Up Notification ACK/NACK. |
cc_wake_up_config_get_default_sleep_time_sec#
uint32_t cc_wake_up_config_get_default_sleep_time_sec (void )
Used by the WakeUp Command Class configuration Returns with the default sleep time in second between Wake Up Notifications.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Default sleep time in second between Wake Up Notifications
cc_wake_up_config_get_minimum_sleep_time_sec#
uint32_t cc_wake_up_config_get_minimum_sleep_time_sec (void )
Used by the WakeUp Command Class configuration Returns with the minimum sleep time in second between Wake Up Notifications.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Minimum sleep time in second
cc_wake_up_config_get_maximum_sleep_time_sec#
uint32_t cc_wake_up_config_get_maximum_sleep_time_sec (void )
Used by the WakeUp Command Class configuration Returns with the maximum sleep time in second between Wake Up Notifications.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Maximum sleep time in second
cc_wake_up_config_get_sleep_step_time_sec#
uint32_t cc_wake_up_config_get_sleep_step_time_sec (void )
Used by the WakeUp Command Class configuration Returns with the sleep step time in second.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
sleep step time in second