Network statistics structure.

Public Attributes#

uint32_t

Transmitted Frames.

uint32_t

LBT backoffs.

uint32_t

Received Frames (No errors).

uint32_t

Checksum Errors.

uint32_t

CRC16 Errors.

uint32_t

Foreign Home ID.

uint32_t

Accumulated transmission time in ms for channel 0.

uint32_t

Accumulated transmission time in ms for channel 1.

uint32_t

Accumulated transmission time in ms for channel 2.

uint32_t

Accumulated transmission time in ms for channel 3, i.e., US_LR1.

uint32_t

Accumulated transmission time in ms for channel 4, i.e., US_LR2.

Public Attribute Documentation#

tx_frames#

uint32_t zpal_radio_network_stats_t::tx_frames

Transmitted Frames.


Definition at line 457 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

tx_lbt_back_offs#

uint32_t zpal_radio_network_stats_t::tx_lbt_back_offs

LBT backoffs.


Definition at line 458 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rx_frames#

uint32_t zpal_radio_network_stats_t::rx_frames

Received Frames (No errors).


Definition at line 459 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rx_lrc_errors#

uint32_t zpal_radio_network_stats_t::rx_lrc_errors

Checksum Errors.


Definition at line 460 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rx_crc_errors#

uint32_t zpal_radio_network_stats_t::rx_crc_errors

CRC16 Errors.


Definition at line 461 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

rx_foreign_home_id#

uint32_t zpal_radio_network_stats_t::rx_foreign_home_id

Foreign Home ID.


Definition at line 462 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

tx_time_channel_0#

uint32_t zpal_radio_network_stats_t::tx_time_channel_0

Accumulated transmission time in ms for channel 0.


Definition at line 463 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

tx_time_channel_1#

uint32_t zpal_radio_network_stats_t::tx_time_channel_1

Accumulated transmission time in ms for channel 1.


Definition at line 464 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

tx_time_channel_2#

uint32_t zpal_radio_network_stats_t::tx_time_channel_2

Accumulated transmission time in ms for channel 2.


Definition at line 465 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

tx_time_channel_3#

uint32_t zpal_radio_network_stats_t::tx_time_channel_3

Accumulated transmission time in ms for channel 3, i.e., US_LR1.


Definition at line 466 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h

tx_time_channel_4#

uint32_t zpal_radio_network_stats_t::tx_time_channel_4

Accumulated transmission time in ms for channel 4, i.e., US_LR2.


Definition at line 467 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/PAL/inc/zpal_radio.h