Radio Profile containing region, baud rate, and wakeup interval for this device.

Public Attributes#

Region in which this system operates.

Wakeup interval for the radio.

uint8_t

Primary Long Range Channel.

bool

Longe Range channel selection mode.

int8_t

LBT Threshold for Transmit backoff in dBm.

Z-Wave Transmit Power in deci dBm.

Adjustment for antenna gain in deci dBm.

Max transmit power for Z-Wave LR in deci dBm.

uint8_t *

Pointer to current HomeID(uint8_t homeID[4]).

Pointer to function called by RF on Rx Completion.

Pointer to function called by RF on Tx Completion.

Pointer to function called by RF on Region change.

Pointer to function called by RF on fatal Assert.

Pointer to structure where to RF Statistics are placed.

uint8_t

Enable radio debugging which is vendor specific.

Public Attribute Documentation#

region#

zpal_radio_region_t zpal_radio_profile_t::region

Region in which this system operates.


wakeup#

zpal_radio_wakeup_t zpal_radio_profile_t::wakeup

Wakeup interval for the radio.


primary_lr_channel#

uint8_t zpal_radio_profile_t::primary_lr_channel

Primary Long Range Channel.


lr_channel_auto_mode#

bool zpal_radio_profile_t::lr_channel_auto_mode

Longe Range channel selection mode.


listen_before_talk_threshold#

int8_t zpal_radio_profile_t::listen_before_talk_threshold

LBT Threshold for Transmit backoff in dBm.


tx_power_max#

zpal_tx_power_t zpal_radio_profile_t::tx_power_max

Z-Wave Transmit Power in deci dBm.


tx_power_adjust#

zpal_tx_power_t zpal_radio_profile_t::tx_power_adjust

Adjustment for antenna gain in deci dBm.


tx_power_max_lr#

zpal_tx_power_t zpal_radio_profile_t::tx_power_max_lr

Max transmit power for Z-Wave LR in deci dBm.


home_id#

uint8_t* zpal_radio_profile_t::home_id

Pointer to current HomeID(uint8_t homeID[4]).


rx_cb#

zpal_radio_callback_t zpal_radio_profile_t::rx_cb

Pointer to function called by RF on Rx Completion.


tx_cb#

zpal_radio_callback_t zpal_radio_profile_t::tx_cb

Pointer to function called by RF on Tx Completion.


region_change_cb#

zpal_radio_callback_t zpal_radio_profile_t::region_change_cb

Pointer to function called by RF on Region change.


assert_cb#

zpal_radio_callback_t zpal_radio_profile_t::assert_cb

Pointer to function called by RF on fatal Assert.


network_stats#

zpal_radio_network_stats_t* zpal_radio_profile_t::network_stats

Pointer to structure where to RF Statistics are placed.


radio_debug_enable#

uint8_t zpal_radio_profile_t::radio_debug_enable

Enable radio debugging which is vendor specific.


receive_handler_cb#

zpal_radio_receive_handler_t zpal_radio_profile_t::receive_handler_cb

Pointer to receive handler.