Multi Channel Configuration#

Multi Channel Configuration.

A multi channel device must specify the number of supported end points. An example of a multi channel device could be a Power Strip for which each outlet is represented by an end point.

Macros#

#define

Number of end points <0..255:1>

Macro Definition Documentation#

ZAF_CONFIG_NUMBER_OF_END_POINTS#

#define ZAF_CONFIG_NUMBER_OF_END_POINTS
Value:
0

Number of end points <0..255:1>


Definition at line 480 of file /mnt/raid/workspaces/ws.T7KR5OZRo/overlay/gsdk/protocol/z-wave/ZAF/configuration/config/zaf_config.h