Event Manager#
Enumerations#
System events.
Button events.
Functions#
Initializes event scheduler.
Adds a given event to the event queue.
Processes events.
Adds a given event to the job queue.
Deque job queue.
Get number of events on queue.
Macros#
Event groups for application state event machine.
Event group for keys 0x40 - 0x6F.
Event group for zaf 0x80 - 0xFF.
Enumeration Documentation#
_EVENT_SYSTEM_#
_EVENT_SYSTEM_
System events.
Enumerator | |
---|---|
EVENT_SYSTEM_RESET | |
EVENT_SYSTEM_LEARNMODE_START | |
EVENT_SYSTEM_LEARNMODE_FINISHED | |
EVENT_SYSTEM_LEARNMODE_STOP | |
EVENT_SYSTEM_LEARNMODE_TOGGLE | |
EVENT_SYSTEM_WATCHDOG_RESET | |
EVENT_SYSTEM_OTA_START | |
EVENT_SYSTEM_LEARNMODE_DSK_START | |
EVENT_SYSTEM_FLUSHMEM_READY | |
EVENT_SYSTEM_SMARTSTART_IN_PROGRESS | |
EVENT_SYSTEM_EMPTY |
40
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
_BUTTON_EVENT_
_BUTTON_EVENT_
Button events.
NB: For every button there MUST be the following events in this order: DOWN, UP, SHORT_PRESS, HOLD, LONG_PRESS The macros BTN_EVENT_xxx in board.h depends on it.
Enumerator | |
---|---|
EVENT_PB1_DOWN | |
EVENT_PB1_UP | |
EVENT_PB1_SHORT_PRESS | |
EVENT_PB1_HOLD | |
EVENT_PB1_LONG_PRESS | |
EVENT_PB2_DOWN | |
EVENT_PB2_UP | |
EVENT_PB2_SHORT_PRESS | |
EVENT_PB2_HOLD | |
EVENT_PB2_LONG_PRESS | |
EVENT_PB3_DOWN | |
EVENT_PB3_UP | |
EVENT_PB3_SHORT_PRESS | |
EVENT_PB3_HOLD | |
EVENT_PB3_LONG_PRESS | |
EVENT_PB4_DOWN | |
EVENT_PB4_UP | |
EVENT_PB4_SHORT_PRESS | |
EVENT_PB4_HOLD | |
EVENT_PB4_LONG_PRESS | |
EVENT_PB5_DOWN | |
EVENT_PB5_UP | |
EVENT_PB5_SHORT_PRESS | |
EVENT_PB5_HOLD | |
EVENT_PB5_LONG_PRESS | |
EVENT_PB6_DOWN | |
EVENT_PB6_UP | |
EVENT_PB6_SHORT_PRESS | |
EVENT_PB6_HOLD | |
EVENT_PB6_LONG_PRESS | |
EVENT_SLIDER1_DOWN | |
EVENT_SLIDER1_UP | |
EVENT_SLIDER1_SHORT_PRESS | |
EVENT_SLIDER1_HOLD | |
EVENT_SLIDER1_LONG_PRESS | |
EVENT_BTN_MAX | EVENT_BTN_MAX define the last enum type. |
62
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
Typedef Documentation#
EVENT_SYSTEM#
typedef enum _EVENT_SYSTEM_ EVENT_SYSTEM
System events.
53
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
BUTTON_EVENT
typedef enum _BUTTON_EVENT_ BUTTON_EVENT
Button events.
NB: For every button there MUST be the following events in this order: DOWN, UP, SHORT_PRESS, HOLD, LONG_PRESS The macros BTN_EVENT_xxx in board.h depends on it.
100
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
Function Documentation#
ZAF_eventSchedulerInit#
void ZAF_eventSchedulerInit (void(*)(uint8_t) pApplicationStateMachine)
Initializes event scheduler.
N/A | pApplicationStateMachine |
108
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZCB_eventSchedulerEventAdd#
bool ZCB_eventSchedulerEventAdd (uint8_t event)
Adds a given event to the event queue.
N/A | event | A given event. |
Returns
true if given event is added to queue, false if queue full.
117
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZCB_eventScheduler#
bool ZCB_eventScheduler (void )
Processes events.
N/A |
124
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZAF_jobEnqueue#
bool ZAF_jobEnqueue (uint8_t event)
Adds a given event to the job queue.
N/A | event | A given event. |
Returns
true if given event is added to queue, false if queue full.
133
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZAF_jobDequeue#
bool ZAF_jobDequeue (uint8_t * pEvent)
Deque job queue.
[out] | pEvent | return event from the queue. |
Returns
false if queue is empty else true.
142
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZAF_jobQueueCount#
uint8_t ZAF_jobQueueCount (void )
Get number of events on queue.
N/A |
Returns
number of events on queue
149
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
Macro Definition Documentation#
DEFINE_EVENT_WAKEUP_NBR#
#define DEFINE_EVENT_WAKEUP_NBRValue:
0x01
Event groups for application state event machine.
22
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
DEFINE_EVENT_KEYPAD_NBR#
#define DEFINE_EVENT_KEYPAD_NBRValue:
0x10
23
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
DEFINE_EVENT_IR_NBR#
#define DEFINE_EVENT_IR_NBRValue:
0x20
24
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
DEFINE_EVENT_SYSTEM_NBR#
#define DEFINE_EVENT_SYSTEM_NBRValue:
0x30
25
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
DEFINE_EVENT_KEY_NBR#
#define DEFINE_EVENT_KEY_NBRValue:
0x40
Event group for keys 0x40 - 0x6F.
30
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
DEFINE_EVENT_APP_NBR#
#define DEFINE_EVENT_APP_NBRValue:
0x70
Event group for zaf 0x80 - 0xFF.
35
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
BTN_EVENT_FILTER#
#define BTN_EVENT_FILTERValue:
(btnEvent)
102
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
EventSchedulerInit#
#define EventSchedulerInitValue:
ZAF_eventSchedulerInit
104
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZCB_EventSchedulerEventAdd#
#define ZCB_EventSchedulerEventAddValue:
ZCB_eventSchedulerEventAdd
111
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZCB_EventScheduler#
#define ZCB_EventSchedulerValue:
ZCB_eventScheduler
120
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZCB_EventEnqueue#
#define ZCB_EventEnqueueValue:
ZAF_jobEnqueue
127
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h
ZCB_EventDequeue#
#define ZCB_EventDequeueValue:
ZAF_jobDequeue
136
of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/ev_man.h