Struct used to pass operational data to TSE module.

See ZAF_TSE_Trigger() for more information.

  • Receive options MUST be the first element as TSE relies on the receive options.

Public Attributes#

uint8_t

Indicator Id.

Public Attribute Documentation#

rxOptions#

RECEIVE_OPTIONS_TYPE_EX s_CC_indicator_data_t_::rxOptions

rxOptions


Definition at line 42 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Indicator/inc/CC_Indicator.h

indicatorId#

uint8_t s_CC_indicator_data_t_::indicatorId

Indicator Id.


Definition at line 43 of file /mnt/raid/workspaces/ws.Mh9rMZz8x/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Indicator/inc/CC_Indicator.h