Public Attributes#
uint8_t
Basic Device Type, is it a Controller, Controller_Static, Slave or a Slave_Routing Device Type.
uint8_t
Generic Device Type.
uint8_t
Specific Device Type.
Public Attribute Documentation#
basic#
uint8_t _NODE_TYPE_::basic
Basic Device Type, is it a Controller, Controller_Static, Slave or a Slave_Routing Device Type.
Definition at line
47
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h
generic#
uint8_t _NODE_TYPE_::generic
Generic Device Type.
Definition at line
49
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h
specific#
uint8_t _NODE_TYPE_::specific
Specific Device Type.
Definition at line
50
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h