Public Attributes#
uint32_t
void *
FreeRTOS timer handle.
uint8_t
Identifies timer to SwTimerLiaison.
void *
User pointer, which is free to be used.
Pointer to TimerLiaison object which timer is registered to.
void(*
Callback function pointer.
Public Attribute Documentation#
dummy#
uint32_t SSwTimer::dummy[PRIVATE_TIMER_SIZE]
Definition at line
73
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimer.h
TimerHandle#
void* SSwTimer::TimerHandle
FreeRTOS timer handle.
Definition at line
74
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimer.h
Id#
uint8_t SSwTimer::Id
Identifies timer to SwTimerLiaison.
Definition at line
75
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimer.h
ptr#
void* SSwTimer::ptr
User pointer, which is free to be used.
Definition at line
76
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimer.h
pLiaison#
SSwTimerLiaisonPtr SSwTimer::pLiaison
Pointer to TimerLiaison object which timer is registered to.
Definition at line
77
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimer.h
pCallback#
void(* SSwTimer::pCallback) (struct SSwTimer *pTimer)
Callback function pointer.
Definition at line
79
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Components/SwTimer/SwTimer.h