Public Attributes#

uint8_t

Basic Device Type, is it a Controller, Controller_Static, Slave or a Slave_Routing Device Type.

uint8_t

Generic Device Type.

uint8_t

Specific Device Type.

Public Attribute Documentation#

basic#

uint8_t _NODE_TYPE_::basic

Basic Device Type, is it a Controller, Controller_Static, Slave or a Slave_Routing Device Type.


Definition at line 47 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h

generic#

uint8_t _NODE_TYPE_::generic

Generic Device Type.


Definition at line 49 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h

specific#

uint8_t _NODE_TYPE_::specific

Specific Device Type.


Definition at line 50 of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_basis_api.h