Transmit Options#
Transmit frame option flags.
Macros#
#define
TRANSMIT_OPTION_ACK 0x01
Request acknowledge from destination node.
#define
Rransmit at low output power level (1/3 of normal RF range)
#define
The multicast frame should be send as a broadcast.
#define
Request retransmission via repeater nodes.
#define
Do not use response route - Even if available.
#define
Use explore frame if needed.
Macro Definition Documentation#
TRANSMIT_OPTION_ACK#
#define TRANSMIT_OPTION_ACKValue:
0x01
Request acknowledge from destination node.
Definition at line
47
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
TRANSMIT_OPTION_LOW_POWER#
#define TRANSMIT_OPTION_LOW_POWERValue:
0x02
Rransmit at low output power level (1/3 of normal RF range)
Definition at line
48
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
TRANSMIT_OPTION_MULTICAST_AS_BROADCAST#
#define TRANSMIT_OPTION_MULTICAST_AS_BROADCASTValue:
0x02
The multicast frame should be send as a broadcast.
Definition at line
49
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
TRANSMIT_OPTION_AUTO_ROUTE#
#define TRANSMIT_OPTION_AUTO_ROUTEValue:
0x04
Request retransmission via repeater nodes.
Definition at line
50
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
TRANSMIT_OPTION_NO_ROUTE#
#define TRANSMIT_OPTION_NO_ROUTEValue:
0x10
Do not use response route - Even if available.
Definition at line
51
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
TRANSMIT_OPTION_EXPLORE#
#define TRANSMIT_OPTION_EXPLOREValue:
0x20
Use explore frame if needed.
Definition at line
52
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h