ZAF Interface#
Enumerations#
Used to indicate node inclusion type that related to it working over Long Range or Z-Wave mode.
Typedefs#
Functions#
Initializes the Z-Wave Application Framework.
Reset ZAF and command classes that have registered a reset function with a REGISTER_CC macro.
Returns the task handle set by ZAF_Init().
Makes the node stay awake for either 2 or 10 seconds.
Function called when the EVENT_SYSTEM_LEARNMODE_FINISHED is received.
Pass an application handle to the ZAF framework with pointers to application resources.
Pass an application power lock handle to the ZAF framework.
Set the CP context.
Get m_pAppHandles object.
Get Protocol Info object.
Get Notifying queue object.
Get Notifying queue object used for ZW Command Queue.
Get Network Statistics object.
Get m_PowerLock object.
Returns the granted security keys.
Get Command Publisher handle Any other module can request the address of the CP context to use the API.
Check if device is FLiRS based on device option mask.
Returns the current inclusion state of the node.
Returns the current ID of the node.
Returns the current home ID.
Returns the current Suc node ID.
Returns the current inclusion mode of the node, which indicates whether the node is acting as a Z-Wave or Z-Wave LR node.
Checks if region is supported by Z-Wave stack.
Check if eRegion is a Long Range region.
Registers a wake up function to keep the node awake.
Returns the wake up callback.
Enumeration Documentation#
EInclusionMode_t#
EInclusionMode_t
Used to indicate node inclusion type that related to it working over Long Range or Z-Wave mode.
This information will be used to distinguish between these two mode in order to indicate the needed operations when they differ between Z-Wave and Long Range.
Enumerator | |
---|---|
EINCLUSIONMODE_NOT_SET | |
EINCLUSIONMODE_ZWAVE_CLS | !< Does not indicate inclusion state, but that it is undefined! |
EINCLUSIONMODE_ZWAVE_LR | !< This node was included as a Z-Wave Classic device. |
36
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
Typedef Documentation#
zaf_wake_up_callback_t#
typedef void(* zaf_wake_up_callback_t) (void) )(void)
29
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
Function Documentation#
ZAF_Init#
void ZAF_Init (TaskHandle_t AppTaskHandle, SApplicationHandles * pAppHandles)
Initializes the Z-Wave Application Framework.
N/A | AppTaskHandle | Task handle |
N/A | pAppHandles | pointer to Application Handle in application |
This function must be invoked by end devices and portable controllers, but not Serial API.
It initializes the following stuff:
Application timer
Board
Application file system
Power lock for FLiRS
True Status
Command Publisher
All command classes that have registered an init function.
Generates the three lists of command classes used for Node Information Frame, etc.
40
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_helper.h
ZAF_Reset#
void ZAF_Reset (void )
Reset ZAF and command classes that have registered a reset function with a REGISTER_CC macro.
N/A |
45
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_helper.h
ZAF_getAppTaskHandle#
TaskHandle_t ZAF_getAppTaskHandle (void )
Returns the task handle set by ZAF_Init().
N/A |
Returns
Task handle.
51
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_helper.h
zaf_stay_awake#
void zaf_stay_awake (void )
Makes the node stay awake for either 2 or 10 seconds.
N/A |
For an LS (listening sleeping) node, the node will stay awake for 2 seconds. If the node supports CC Wake Up, it will stay awake for 10 seconds, if CC Wake Up is active.
For RS (reporting sleeping), the node will stay awake for 10 seconds, if CC Wake Up is active.
61
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_helper.h
zaf_learn_mode_finished#
void zaf_learn_mode_finished (void )
Function called when the EVENT_SYSTEM_LEARNMODE_FINISHED is received.
N/A |
This function is weakly defined and can be overwritten by one command class. Applications should not overwrite this function instead they should handle the event. CC WakeUp overwrites it.
71
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_helper.h
ZAF_setAppHandle#
void ZAF_setAppHandle (SApplicationHandles * pAppHandle)
Pass an application handle to the ZAF framework with pointers to application resources.
N/A | pAppHandle | pointer to Application Handle in application |
Can be later used by CC-s.
49
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_setPowerLock#
void ZAF_setPowerLock (zpal_pm_handle_t powerLock)
Pass an application power lock handle to the ZAF framework.
N/A | powerLock | pointer to power lock object in application |
Can be later used by CC-s. Used for Power management in case of wake up of FLiRS nodes.
57
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_SetCPHandle#
void ZAF_SetCPHandle (CP_Handle_t handle)
Set the CP context.
N/A | handle | to set |
The application should use this an initialization, so the ZAF_Common interface can redistribute the pContext address subsequently
65
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_getAppHandle#
SApplicationHandles * ZAF_getAppHandle (void )
Get m_pAppHandles object.
N/A |
Returns
m_pAppHandles
74
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_getProtocolInfo#
const SProtocolInfo * ZAF_getProtocolInfo (void )
Get Protocol Info object.
N/A |
Returns
pProtocolInfo member of m_pAppHandles
80
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_getZwTxQueue#
SQueueNotifying * ZAF_getZwTxQueue (void )
Get Notifying queue object.
N/A |
It is stored in m_pAppHandles Returns
pZwTxQueue member of m_pAppHandles
86
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_getZwCommandQueue#
SQueueNotifying * ZAF_getZwCommandQueue (void )
Get Notifying queue object used for ZW Command Queue.
N/A |
Returns
pZwCommandQueue member of m_pAppHandles
92
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_getNetworkStatistics#
const zpal_radio_network_stats_t * ZAF_getNetworkStatistics (void )
Get Network Statistics object.
N/A |
Returns
pNetworkStatistics member of m_pAppHandles
98
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_getPowerLock#
zpal_pm_handle_t ZAF_getPowerLock (void )
Get m_PowerLock object.
N/A |
Returns
m_PowerLock
104
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_GetSecurityKeys#
uint8_t ZAF_GetSecurityKeys (void )
Returns the granted security keys.
N/A |
Refer to ZW_security_api.h for the security key masks. Returns
8 bit mask where a set bit indicates that a security key is granted.
112
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_getCPHandle#
CP_Handle_t ZAF_getCPHandle (void )
Get Command Publisher handle Any other module can request the address of the CP context to use the API.
N/A |
Returns
Pointer to Command Publisher context
120
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
isFLiRS#
bool isFLiRS (const SAppNodeInfo_t * pAppNodeInfo)
Check if device is FLiRS based on device option mask.
N/A | pAppNodeInfo |
Returns
True or false, based on pAppNodeInfo
129
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_GetInclusionState#
EInclusionState_t ZAF_GetInclusionState (void )
Returns the current inclusion state of the node.
N/A |
Returns
EInclusionState_t
135
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_GetNodeID#
node_id_t ZAF_GetNodeID (void )
Returns the current ID of the node.
N/A |
If the node is not added to a network, the node ID is zero. Returns
Node ID
143
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_GetHomeID#
uint32_t ZAF_GetHomeID (void )
Returns the current home ID.
N/A |
Returns
Home ID
150
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_GetSucNodeId#
node_id_t ZAF_GetSucNodeId (void )
Returns the current Suc node ID.
N/A |
Returns
Suc Node ID
157
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_GetInclusionMode#
EInclusionMode_t ZAF_GetInclusionMode (void )
Returns the current inclusion mode of the node, which indicates whether the node is acting as a Z-Wave or Z-Wave LR node.
N/A |
Returns
EInclusionMode_t
165
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
isRfRegionValid#
bool isRfRegionValid (zpal_radio_region_t region)
Checks if region is supported by Z-Wave stack.
N/A | region | Region to check |
Returns
True if region is valid, false if it isn't.
172
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
ZAF_isLongRangeRegion#
bool ZAF_isLongRangeRegion (zpal_radio_region_t eRegion)
Check if eRegion is a Long Range region.
N/A | eRegion | Region to check |
Warning: the function does not check that the region is supported by the zpal. Returns
True if the region support Long Range, False otherwise.
180
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
zaf_set_stay_awake_callback#
void zaf_set_stay_awake_callback (zaf_wake_up_callback_t callback)
Registers a wake up function to keep the node awake.
N/A | callback | Function to invoke to keep the node awake. |
The function will be invoked on every reception of a frame to keep the node awake.
188
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h
zaf_get_stay_awake_callback#
zaf_wake_up_callback_t zaf_get_stay_awake_callback (void )
Returns the wake up callback.
N/A |
Returns
Wake up callback
194
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/ApplicationUtilities/_commonIF/ZAF_Common_interface.h