Zpal-bootloader#
Defines a platform abstraction layer for the Z-Wave bootloader.
How to use the bootloader API
The ZPAL bootloader API is required if an application would like to store and use a new firmware image.
zpal_bootloader_init() and zpal_bootloader_get_info() must be implemented as Z-Wave always invokes these. The remaining API functions are optional in case a bootloader is not present in the ZPAL implementation.
The following outlines an example of use:
- To enable the bootloader functionality, invoke zpal_bootloader_init(). 
- zpal_bootloader_get_info() must be invoked to check whether a bootloader is present. 
- For every received fragment, zpal_bootloader_write_data() must be invoked to store the new firmware image. 
- When all fragments are received, zpal_bootloader_verify_image() must be invoked to verify the integrity of the received firmware image. 
- If the received firmware image is valid, invoke zpal_bootloader_reboot_and_install() install and boot from the new firmware image. 
Requirements:
- The ZPAL bootloader requires that a storage is available for storing a received firmware image. Z-Wave has no requirements on how and where the image is stored. 
Modules#
Enumerations#
Type of bootloader.
Functions#
//zpal-bootloader-info-version
Initialize components of the bootloader so the app can use the interface.
Reboot into the bootloader to install something.
Verify that the image is valid.
Writes a fragment of a firmware image to the bootloader storage.
Returns whether the software is running on the first boot after a new firmware image was written.
Resets the bootloader page counters.
Macros#
Bootloader has the capability of storing data in an internal or external storage medium.
Enumeration Documentation#
zpal_bootloader_type_t#
zpal_bootloader_type_t
Type of bootloader.
| Enumerator | |
|---|---|
| ZPAL_BOOTLOADER_NOT_PRESENT | No bootloader present. | 
| ZPAL_BOOTLOADER_PRESENT | Bootloader present. | 
Function Documentation#
zpal_bootloader_get_info#
void zpal_bootloader_get_info (zpal_bootloader_info_t * info)
//zpal-bootloader-info-version
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| zpal_bootloader_info_t * | [out] | info | Pointer to the bootloader information struct. | 
Get information about the bootloader on this device. The information returned is fetched from the main bootloader information table.
zpal_bootloader_init#
zpal_status_t zpal_bootloader_init (void )
Initialize components of the bootloader so the app can use the interface.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This typically includes initializing serial peripherals for communication with external SPI flashes, and so on.
Returns
- Error code. ZPAL_STATUS_OK on success, else ZPAL_STATUS_FAIL 
zpal_bootloader_reboot_and_install#
void zpal_bootloader_reboot_and_install (void )
Reboot into the bootloader to install something.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
If there is a storage component and a slot is marked for bootload, install the image in that slot after verifying it. If a communication component is present, open the communication channel and receive an image to be installed.
zpal_bootloader_verify_image#
zpal_status_t zpal_bootloader_verify_image (void )
Verify that the image is valid.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Returns
- ZPAL_STATUS_OK if the image is valid, else ZPAL_STATUS_FAIL. 
zpal_bootloader_write_data#
zpal_status_t zpal_bootloader_write_data (uint32_t offset, uint8_t * data, uint16_t length)
Writes a fragment of a firmware image to the bootloader storage.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint32_t | [in] | offset | Offset from the storage start. | 
| uint8_t * | [in] | data | Pointer to fragment of firmware image. | 
| uint16_t | [in] | length | Length of firmware image fragment. | 
Returns
- ZPAL_STATUS_OK on success, and ZPAL_STATUS_FAIL otherwise. 
zpal_bootloader_is_first_boot#
bool zpal_bootloader_is_first_boot (bool * updated_successfully)
Returns whether the software is running on the first boot after a new firmware image was written.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| bool * | [in] | updated_successfully | Set to true if update was successful, false otherwise. Valid only when it's the first boot. | 
Returns
- True if it's the first boot, false otherwise. 
zpal_bootloader_reset_page_counters#
void zpal_bootloader_reset_page_counters (void )
Resets the bootloader page counters.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Used when initiating an upgrade to jump back to the start of the storage slot.