Basic#

Functions#

CC_Basic_Report_tx(AGI_PROFILE *pProfile, uint8_t sourceEndpoint, uint8_t bValue, ZAF_TX_Callback_t callback)

Send unsolicited command class Basic report.

CC_Basic_Set_tx(agi_profile_t const *const p_profile, const uint8_t source_endpoint, const uint8_t value, const bool use_supervision, ZAF_TX_Callback_t callback)

Sends an unsolicited Basic Set command.

Function Documentation#

CC_Basic_Report_tx#

JOB_STATUS CC_Basic_Report_tx (AGI_PROFILE * pProfile, uint8_t sourceEndpoint, uint8_t bValue, ZAF_TX_Callback_t callback)

Send unsolicited command class Basic report.

Parameters
TypeDirectionArgument NameDescription
AGI_PROFILE *[in]pProfile

pointer to AGI profile

uint8_t[in]sourceEndpoint

source endpoint

uint8_t[in]bValue

Basic Report value

ZAF_TX_Callback_t[out]callback

callback function pointer returning status on job. Can be initialized to NULL.

Returns

  • status of the job of type JOB_STATUS


CC_Basic_Set_tx#

zaf_job_status_t CC_Basic_Set_tx (agi_profile_t const *const p_profile, const uint8_t source_endpoint, const uint8_t value, const bool use_supervision, ZAF_TX_Callback_t callback)

Sends an unsolicited Basic Set command.

Parameters
TypeDirectionArgument NameDescription
agi_profile_t const *const[in]p_profile

Pointer to an AGI profile defined in the configuration of CC AGI.

const uint8_t[in]source_endpoint

Source endpoint if the sending device use endpoints. Otherwise 0.

const uint8_t[in]value

Value as defined in the specification of the command.

const bool[in]use_supervision

Use Supervision for transmission of this Basic Set.

ZAF_TX_Callback_t[out]callback

Callback function pointer giving a result of the transmission.

Returns

  • Status on whether the transmission could be initiated.