MfgTokens#
Functions#
Function for initializing manufacturing module.
Function for setting the manufacturing token data.
Function for Getting the manufacturing token data.
Wrapper function for getting the manufacturing "country freq" token.
Writes Rf Region to manufacturing token.
Lock manufacturing token storage.
Macros#
Function Documentation#
ZW_MfgTokenModuleInit#
void ZW_MfgTokenModuleInit (void)
Function for initializing manufacturing module.
N/A |
60
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
ZW_SetMfgTokenData#
void ZW_SetMfgTokenData (uint16_t token, void *data, uint8_t len)
Function for setting the manufacturing token data.
[in] | token | Token to be set |
[in] | data | Pointer to object data to write |
[in] | len | Size of object to write in bytes |
71
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
ZW_GetMfgTokenData#
void ZW_GetMfgTokenData (void *data, uint16_t token, uint8_t len)
Function for Getting the manufacturing token data.
[out] | data | Pointer to object data where the value will be written to. |
[in] | token | Type of the token to get |
[in] | len | Size of output object |
80
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
ZW_GetMfgTokenDataCountryFreq#
void ZW_GetMfgTokenDataCountryFreq (void *data)
Wrapper function for getting the manufacturing "country freq" token.
[out] | data | Country frequency token |
87
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
ZW_SetMfgTokenDataCountryRegion#
void ZW_SetMfgTokenDataCountryRegion (void *region)
Writes Rf Region to manufacturing token.
[in] | region | Region to write |
93
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
ZW_LockMfgTokenData#
void ZW_LockMfgTokenData (void)
Lock manufacturing token storage.
N/A |
98
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
Macro Definition Documentation#
TOKEN_MFG_ZWAVE_COUNTRY_FREQ_ID#
#define TOKEN_MFG_ZWAVE_COUNTRY_FREQ_IDValue:
0x0001
45
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZW_PRK_ID#
#define TOKEN_MFG_ZW_PRK_IDValue:
0x0002
46
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZW_PUK_ID#
#define TOKEN_MFG_ZW_PUK_IDValue:
0x0003
47
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZW_INITIALIZED_ID#
#define TOKEN_MFG_ZW_INITIALIZED_IDValue:
0x0004
48
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZW_QR_CODE_ID#
#define TOKEN_MFG_ZW_QR_CODE_IDValue:
0x0005
49
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZWAVE_COUNTRY_FREQ_SIZE#
#define TOKEN_MFG_ZWAVE_COUNTRY_FREQ_SIZEValue:
1
51
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZW_PRK_SIZE#
#define TOKEN_MFG_ZW_PRK_SIZEValue:
32
52
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZW_PUK_SIZE#
#define TOKEN_MFG_ZW_PUK_SIZEValue:
32
53
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZW_INITIALIZED_SIZE#
#define TOKEN_MFG_ZW_INITIALIZED_SIZEValue:
1
54
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h
TOKEN_MFG_ZW_QR_CODE_SIZE#
#define TOKEN_MFG_ZW_QR_CODE_SIZEValue:
106
55
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/Components/MfgTokens/MfgTokens.h