Z-Wave System Startup API#

Functions#

bool

Was the device woken up by an RTCC timer interrupt?

uint32_t

Get number of milliseconds the device has spent sleeping in deep sleep before it was woken up.

uint32_t

Get the sleeptimer tick value of the device when it woke up from deep sleep.

uint32_t

Get the sleeptimer tick value of the device when it last went to Deep Sleep.

Get the reset reason of the device when it was last reset or woke up from EM4 sleep.

bool
ZW_ApplicationRegisterTask(void(*appTaskFunc)(SApplicationHandles *), uint8_t iZwRxQueueTaskNotificationBitNumber, uint8_t iZwCommandStatusQueueTaskNotificationBitNumber, const SProtocolConfig_t *pProtocolConfig)

Please.

Used to get the pointer to the application handles structure! Needed to insert task related data when creating user task.

void
ZW_system_startup_SetEventNotificationBitNumbers(uint8_t iZwRxQueueTaskNotificationBitNumber, uint8_t iZwCommandStatusQueueTaskNotificationBitNumber, const SProtocolConfig_t *pProtocolConfig)

Used by ZW_UserTask_ApplicationRegisterTask() in ZW_UserTask.h to set the Event Notification Bit Numbers in the Application Interface structure!

void

Used by ZW_UserTask_ApplicationRegisterTask() in ZW_UserTask.h to set the Main Application Task Handle in the Application Interface structure, after ZW_UserTask_ApplicationRegisterTask() has created the task!

void
ZW_system_startup_SetCCSet(SCommandClassSet_t *CCSet)

Passed the Command Class set from the Application to the Protocol using a shared variable.

Gets the Command Class Set.

bool

INCLUDE_xTaskGetSchedulerState did not include xTaskGetSchedulerState in the build.

Used to get a pointer to The Application node information SAppNodeInfo_t structure.

Function Documentation#

IsWakeupCausedByRtccTimeout#

bool IsWakeupCausedByRtccTimeout (void )

Was the device woken up by an RTCC timer interrupt?

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function can safely be called from multiple threads.

Returns

  • true if woken up by RTCC timeout, false otherwise.


GetCompletedSleepDurationMs#

uint32_t GetCompletedSleepDurationMs (void )

Get number of milliseconds the device has spent sleeping in deep sleep before it was woken up.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function can safely be called from multiple threads.

Returns

  • Number of milliseconds.


GetDeepSleepWakeupTick#

uint32_t GetDeepSleepWakeupTick (void )

Get the sleeptimer tick value of the device when it woke up from deep sleep.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function can safely be called from multiple threads.

Returns

  • RTCC ticks.


GetLastTickBeforeDeepSleep#

uint32_t GetLastTickBeforeDeepSleep (void )

Get the sleeptimer tick value of the device when it last went to Deep Sleep.

Parameters
TypeDirectionArgument NameDescription
voidN/A

(It is stored in retention RAM)

This function can safely be called from multiple threads.

Returns

  • RTCC ticks.


GetResetReason#

zpal_reset_reason_t GetResetReason (void )

Get the reset reason of the device when it was last reset or woke up from EM4 sleep.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function can safely be called from multiple threads.

Returns

  • reset reason.


ZW_ApplicationRegisterTask#

bool ZW_ApplicationRegisterTask (void(*)(SApplicationHandles *) appTaskFunc, uint8_t iZwRxQueueTaskNotificationBitNumber, uint8_t iZwCommandStatusQueueTaskNotificationBitNumber, const SProtocolConfig_t * pProtocolConfig)

Please.

Parameters
TypeDirectionArgument NameDescription
void(*)(SApplicationHandles *)N/AappTaskFunc
uint8_tN/AiZwRxQueueTaskNotificationBitNumber
uint8_tN/AiZwCommandStatusQueueTaskNotificationBitNumber
const SProtocolConfig_t *N/ApProtocolConfig

See Also


ZW_system_startup_getAppHandles#

SApplicationHandles * ZW_system_startup_getAppHandles (void )

Used to get the pointer to the application handles structure! Needed to insert task related data when creating user task.

Parameters
TypeDirectionArgument NameDescription
voidN/A

ZW_system_startup_SetEventNotificationBitNumbers#

void ZW_system_startup_SetEventNotificationBitNumbers (uint8_t iZwRxQueueTaskNotificationBitNumber, uint8_t iZwCommandStatusQueueTaskNotificationBitNumber, const SProtocolConfig_t * pProtocolConfig)

Used by ZW_UserTask_ApplicationRegisterTask() in ZW_UserTask.h to set the Event Notification Bit Numbers in the Application Interface structure!

Parameters
TypeDirectionArgument NameDescription
uint8_tN/AiZwRxQueueTaskNotificationBitNumber
uint8_tN/AiZwCommandStatusQueueTaskNotificationBitNumber
const SProtocolConfig_t *N/ApProtocolConfig

ZW_system_startup_SetMainApplicationTaskHandle#

void ZW_system_startup_SetMainApplicationTaskHandle (TaskHandle_t xHandle)

Used by ZW_UserTask_ApplicationRegisterTask() in ZW_UserTask.h to set the Main Application Task Handle in the Application Interface structure, after ZW_UserTask_ApplicationRegisterTask() has created the task!

Parameters
TypeDirectionArgument NameDescription
TaskHandle_tN/AxHandle

ZW_system_startup_SetCCSet#

void ZW_system_startup_SetCCSet (SCommandClassSet_t * CCSet)

Passed the Command Class set from the Application to the Protocol using a shared variable.

Parameters
TypeDirectionArgument NameDescription
SCommandClassSet_t *[in]CCSet

Command Class Set


ZW_system_startup_GetCCSet#

SCommandClassSet_t * ZW_system_startup_GetCCSet (void )

Gets the Command Class Set.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • SCommandClassSet_t* A pointer to the Command Class Set


ZW_system_startup_IsSchedulerStarted#

bool ZW_system_startup_IsSchedulerStarted (void )

INCLUDE_xTaskGetSchedulerState did not include xTaskGetSchedulerState in the build.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This is a workaround!

This function indicated whether the Scheduler has ever been started. This will not indicate the current state, e.g. whether the scheduler is in suspended state or running!


ZW_system_startup_getAppNodeInfo#

const SAppNodeInfo_t * ZW_system_startup_getAppNodeInfo (void )

Used to get a pointer to The Application node information SAppNodeInfo_t structure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • const SAppNodeInfo_t*