Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

sof#

uint8_t tx_beam_start_frame_t::sof

Definition at line 94 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

type#

uint8_t tx_beam_start_frame_t::type

Definition at line 95 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

timestamp1#

uint8_t tx_beam_start_frame_t::timestamp1

Definition at line 96 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

timestamp2#

uint8_t tx_beam_start_frame_t::timestamp2

Definition at line 97 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

ch_speed#

uint8_t tx_beam_start_frame_t::ch_speed

Definition at line 98 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

region_no#

uint8_t tx_beam_start_frame_t::region_no

Definition at line 99 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

rssi#

uint8_t tx_beam_start_frame_t::rssi

Definition at line 100 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h

payload#

uint8_t tx_beam_start_frame_t::payload[4]

Definition at line 101 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/Apps/zwave_ncp_zniffer/comm_interface.h