Notifications#

The following section defines how notifications are given to ZAP users in the UI.

Package Notifications#

Package notifications are the warnings or error messages associated for any specific package loaded into ZAP. For example, in the images below, clicking the warning icon under the status column will lead you to a dialog showing all notifications for that package.

Package Notification Config PagePackage Notification Config Page

Warning DialogWarning Dialog

Package Notice Notification pagePackage Notice Notification page

Session Notifications#

Session notifications are the warnings or error messages which are associated with a user session. These warnings/errors can be seen by clicking on the Notifications button in the toolbar on top of the ZAP UI.

For example, the image below shows the session notifications page after an isc file was loaded into ZAP.

Display NotificationDisplay Notification