Multi-Network Manager

Functions

uint8_t emberGetCurrentNetwork (void)
Returns the current network index.
EmberStatus emberSetCurrentNetwork (uint8_t index)
Sets the current network.
uint8_t emberGetCallbackNetwork (void)
Can only be called inside an application callback.

Detailed Description

See multi-network.h for source code.

Function Documentation

uint8_t emberGetCallbackNetwork ( void )

Can only be called inside an application callback.

Returns
the index of the network the callback refers to. If this function is called outside of a callback, it returns 0xFF.
uint8_t emberGetCurrentNetwork ( void )

Returns the current network index.

EmberStatus emberSetCurrentNetwork ( uint8_t index )

Sets the current network.

Parameters
index The network index.
Returns
EMBER_INDEX_OUT_OF_RANGE if the index does not correspond to a valid network, and EMBER_SUCCESS otherwise.