EmberTokTypeStackZllData Struct Reference
#include <
zll-types.h
>
Data Fields |
|
uint32_t | bitmask |
uint16_t | freeNodeIdMin |
uint16_t | freeNodeIdMax |
uint16_t | myGroupIdMin |
uint16_t | freeGroupIdMin |
uint16_t | freeGroupIdMax |
uint8_t | rssiCorrection |
Field Documentation
uint32_t EmberTokTypeStackZllData::bitmask |
uint16_t EmberTokTypeStackZllData::freeGroupIdMax |
uint16_t EmberTokTypeStackZllData::freeGroupIdMin |
uint16_t EmberTokTypeStackZllData::freeNodeIdMax |
uint16_t EmberTokTypeStackZllData::freeNodeIdMin |
uint16_t EmberTokTypeStackZllData::myGroupIdMin |
uint8_t EmberTokTypeStackZllData::rssiCorrection |
The documentation for this struct was generated from the following file:
-
zll-types.h