Modules#
EmberAfDefaultOrMinMaxAttributeValue
EmberAfPluginMessagingClientMessage
EmberAfImageBlockRequestCallbackStruct
EmberAfStandaloneBootloaderQueryResponseData
EmberAfDeviceManagementTenancy
EmberAfDeviceManagementSupplier
EmberAfDeviceManagementSupplyStatusFlags
EmberAfDeviceManagementUncontrolledFlowThreshold
EmberAfDeviceManagementSupplyStatus
EmberAfDeviceManagementPassword
EmberAfDeviceManagementAttributeRange
EmberAfDeviceManagementAttributeTable
The include file for all the types for Ember ApplicationFramework.
License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
/***************************************************************************/
#ifndef SILABS_AF_API_TYPES
#define SILABS_AF_API_TYPES
#include "enums.h"
#ifdef EZSP_HOST
#include "app/util/ezsp/ezsp-enum.h"
#endif
typedef uint16_t EmberAfProfileId;
typedef uint16_t EmberAfAttributeId;
typedef uint16_t EmberAfClusterId;
typedef uint8_t EmberAfAttributeType;
typedef uint8_t EmberAfClusterMask;
typedef uint8_t EmberAfAttributeMask;
typedef void (*EmberAfGenericClusterFunction)(void);
#define EMBER_AF_NULL_MANUFACTURER_CODE 0x0000
#define EMBER_AF_INVALID_PROFILE_ID 0xFFFF
typedef union {
uint8_t *ptrToDefaultValue;
uint16_t defaultValue;
} EmberAfDefaultAttributeValue;
typedef struct {
EmberAfDefaultAttributeValue defaultValue;
EmberAfDefaultAttributeValue minValue;
EmberAfDefaultAttributeValue maxValue;
} EmberAfAttributeMinMaxValue;
typedef union {
uint8_t *ptrToDefaultValue;
uint16_t defaultValue;
EmberAfAttributeMinMaxValue *ptrToMinMaxValue;
} EmberAfDefaultOrMinMaxAttributeValue;
typedef struct {
EmberAfAttributeId attributeId;
EmberAfAttributeType attributeType;
uint8_t size;
EmberAfAttributeMask mask;
EmberAfDefaultOrMinMaxAttributeValue defaultValue;
} EmberAfAttributeMetadata;
typedef struct {
EmberAfClusterId clusterId;
EmberAfAttributeMetadata *attributes;
uint16_t attributeCount;
uint16_t clusterSize;
EmberAfClusterMask mask;
const EmberAfGenericClusterFunction *functions;
} EmberAfCluster;
typedef struct {
uint8_t endpoint;
EmberAfClusterId clusterId;
EmberAfClusterMask clusterMask;
EmberAfAttributeId attributeId;
uint16_t manufacturerCode;
} EmberAfAttributeSearchRecord;
typedef struct {
uint16_t index;
uint16_t manufacturerCode;
} EmberAfManufacturerCodeEntry;
#ifdef HAL_HAS_INT64
typedef uint64_t EmberAfDifferenceType;
#else
typedef uint32_t EmberAfDifferenceType;
#endif
typedef struct {
EmberIncomingMessageType type;
EmberApsFrame* apsFrame;
uint8_t* message;
uint16_t msgLen;
uint16_t source;
uint8_t lastHopLqi;
int8_t lastHopRssi;
uint8_t bindingTableIndex;
uint8_t addressTableIndex;
uint8_t networkIndex;
} EmberAfIncomingMessage;
typedef uint8_t EmberAfInterpanMessageType;
#define EMBER_AF_INTER_PAN_UNICAST 0x00
#define EMBER_AF_INTER_PAN_BROADCAST 0x08
#define EMBER_AF_INTER_PAN_MULTICAST 0x0C
// Legacy names
#define INTER_PAN_UNICAST EMBER_AF_INTER_PAN_UNICAST
#define INTER_PAN_BROADCAST EMBER_AF_INTER_PAN_BROADCAST
#define INTER_PAN_MULTICAST EMBER_AF_INTER_PAN_MULTICAST
#define EMBER_AF_INTERPAN_OPTION_NONE 0x0000
#define EMBER_AF_INTERPAN_OPTION_APS_ENCRYPT 0x0001
#define EMBER_AF_INTERPAN_OPTION_MAC_HAS_LONG_ADDRESS 0x0002
typedef uint16_t EmberAfInterpanOptions;
typedef struct {
EmberAfInterpanMessageType messageType;
EmberEUI64 longAddress;
EmberNodeId shortAddress;
EmberPanId panId;
EmberAfProfileId profileId;
EmberAfClusterId clusterId;
EmberMulticastId groupId;
EmberAfInterpanOptions options;
} EmberAfInterpanHeader;
// Legacy Name
#define InterPanHeader EmberAfInterpanHeader
typedef uint8_t EmberAfAllowedInterpanOptions;
#define EMBER_AF_INTERPAN_DIRECTION_CLIENT_TO_SERVER 0x01
#define EMBER_AF_INTERPAN_DIRECTION_SERVER_TO_CLIENT 0x02
#define EMBER_AF_INTERPAN_DIRECTION_BOTH 0x03
#define EMBER_AF_INTERPAN_GLOBAL_COMMAND 0x04
#define EMBER_AF_INTERPAN_MANUFACTURER_SPECIFIC 0x08
typedef struct {
EmberAfProfileId profileId;
EmberAfClusterId clusterId;
uint8_t commandId;
EmberAfAllowedInterpanOptions options;
} EmberAfAllowedInterPanMessage;
typedef struct {
EmberApsFrame *apsFrame;
EmberIncomingMessageType type;
EmberNodeId source;
uint8_t *buffer;
uint16_t bufLen;
bool clusterSpecific;
bool mfgSpecific;
uint16_t mfgCode;
uint8_t seqNum;
uint8_t commandId;
uint8_t payloadStartIndex;
uint8_t direction;
EmberAfInterpanHeader *interPanHeader;
uint8_t networkIndex;
} EmberAfClusterCommand;
typedef struct {
EmberAfCluster *cluster;
uint8_t clusterCount;
uint16_t endpointSize;
} EmberAfEndpointType;
#ifdef EZSP_HOST
typedef EzspDecisionId EmberAfTcLinkKeyRequestPolicy;
typedef EzspDecisionId EmberAfAppLinkKeyRequestPolicy;
#define EMBER_AF_ALLOW_TC_KEY_REQUESTS EZSP_ALLOW_TC_KEY_REQUESTS_AND_SEND_CURRENT_KEY
#define EMBER_AF_DENY_TC_KEY_REQUESTS EZSP_DENY_TC_KEY_REQUESTS
#define EMBER_AF_ALLOW_APP_KEY_REQUESTS EZSP_ALLOW_APP_KEY_REQUESTS
#define EMBER_AF_DENY_APP_KEY_REQUESTS EZSP_DENY_APP_KEY_REQUESTS
#else
typedef EmberTcLinkKeyRequestPolicy EmberAfTcLinkKeyRequestPolicy;
typedef EmberAppLinkKeyRequestPolicy EmberAfAppLinkKeyRequestPolicy;
#define EMBER_AF_ALLOW_TC_KEY_REQUESTS EMBER_ALLOW_TC_LINK_KEY_REQUEST_AND_SEND_CURRENT_KEY
#define EMBER_AF_DENY_TC_KEY_REQUESTS EMBER_DENY_TC_LINK_KEY_REQUESTS
#define EMBER_AF_ALLOW_APP_KEY_REQUESTS EMBER_ALLOW_APP_LINK_KEY_REQUEST
#define EMBER_AF_DENY_APP_KEY_REQUESTS EMBER_DENY_APP_LINK_KEY_REQUESTS
#endif
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfSecurityProfile
#else
typedef uint8_t EmberAfSecurityProfile;
enum
#endif
{
EMBER_AF_SECURITY_PROFILE_NONE = 0x00,
EMBER_AF_SECURITY_PROFILE_HA = 0x01,
EMBER_AF_SECURITY_PROFILE_HA12 = 0x02,
EMBER_AF_SECURITY_PROFILE_SE_TEST = 0x03,
EMBER_AF_SECURITY_PROFILE_SE_FULL = 0x04,
EMBER_AF_SECURITY_PROFILE_Z3 = 0x05,
EMBER_AF_SECURITY_PROFILE_CUSTOM = 0xFF,
};
typedef struct {
EmberAfSecurityProfile securityProfile;
uint16_t tcBitmask;
EmberExtendedSecurityBitmask tcExtendedBitmask;
uint16_t nodeBitmask;
EmberExtendedSecurityBitmask nodeExtendedBitmask;
EmberAfTcLinkKeyRequestPolicy tcLinkKeyRequestPolicy;
EmberAfAppLinkKeyRequestPolicy appLinkKeyRequestPolicy;
EmberKeyData preconfiguredKey;
} EmberAfSecurityProfileData;
#ifndef DOXYGEN_SHOULD_SKIP_THIS
typedef struct {
EmberNodeType nodeType;
EmberAfSecurityProfile securityProfile;
} EmAfZigbeeProNetwork;
#endif
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfEndpointBitmask;
#else
typedef uint8_t EmberAfEndpointBitmask;
enum
#endif
{
EMBER_AF_ENDPOINT_DISABLED = 0x00,
EMBER_AF_ENDPOINT_ENABLED = 0x01,
};
typedef struct {
uint8_t endpoint;
EmberAfProfileId profileId;
uint16_t deviceId;
uint8_t deviceVersion;
EmberAfEndpointType *endpointType;
uint8_t networkIndex;
EmberAfEndpointBitmask bitmask;
} EmberAfDefinedEndpoint;
// Cluster specific types
#if (EMBER_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 8)
typedef uint8_t EmberAfPluginEsiManagementBitmask;
#elif (EMBER_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 16)
typedef uint16_t EmberAfPluginEsiManagementBitmask;
#elif (EMBER_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE <= 32)
typedef uint32_t EmberAfPluginEsiManagementBitmask;
#else
#error "EMBER_AF_PLUGIN_ESI_MANAGEMENT_ESI_TABLE_SIZE cannot exceed 32"
#endif
typedef struct {
uint32_t eventId;
#ifdef EMBER_AF_PLUGIN_DRLC_SERVER
EmberEUI64 source;
uint8_t sourceEndpoint;
#endif //EMBER_AF_PLUGIN_DRLC_SERVER
#ifdef EMBER_AF_PLUGIN_DRLC
EmberAfPluginEsiManagementBitmask esiBitmask;
#endif //EMBER_AF_PLUGIN_DRLC
uint8_t destinationEndpoint;
uint16_t deviceClass;
uint8_t utilityEnrollmentGroup;
uint32_t startTime;
uint16_t duration;
uint8_t criticalityLevel;
uint8_t coolingTempOffset;
uint8_t heatingTempOffset;
int16_t coolingTempSetPoint;
int16_t heatingTempSetPoint;
int8_t avgLoadPercentage;
uint8_t dutyCycle;
uint8_t eventControl;
uint32_t startRand;
uint32_t durationRand;
uint8_t optionControl;
} EmberAfLoadControlEvent;
typedef enum {
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE = 0x00,
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED = 0x01,
EMBER_AF_UNICAST_SERVICE_DISCOVERY_TIMEOUT = 0x02,
EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE = 0x03,
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE = 0x04,
EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE = 0x05,
EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE = 0x06,
} EmberAfServiceDiscoveryStatus;
#define EM_AF_DISCOVERY_RESPONSE_MASK (0x05)
#define emberAfHaveDiscoveryResponseStatus(status) ((status) & EM_AF_DISCOVERY_RESPONSE_MASK)
typedef struct {
EmberAfServiceDiscoveryStatus status;
uint16_t zdoRequestClusterId;
EmberNodeId matchAddress;
const void* responseData;
} EmberAfServiceDiscoveryResult;
typedef struct {
uint8_t count;
const uint8_t* list;
} EmberAfEndpointList;
typedef struct {
uint8_t inClusterCount;
const uint16_t* inClusterList;
uint8_t outClusterCount;
const uint16_t* outClusterList;
EmberAfProfileId profileId;
uint16_t deviceId;
uint8_t endpoint;
} EmberAfClusterList;
typedef void (EmberAfServiceDiscoveryCallback)(const EmberAfServiceDiscoveryResult* result);
typedef void (EmberAfPartnerLinkKeyExchangeCallback)(bool success);
typedef enum {
EMBER_AF_LONG_POLL,
EMBER_AF_SHORT_POLL,
} EmberAfEventPollControl;
typedef enum {
EMBER_AF_OK_TO_SLEEP,
EMBER_AF_OK_TO_HIBERNATE = EMBER_AF_OK_TO_SLEEP,
EMBER_AF_OK_TO_NAP,
EMBER_AF_STAY_AWAKE,
} EmberAfEventSleepControl;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfApplicationTask
#else
typedef uint32_t EmberAfApplicationTask;
enum
#endif
{
// we may be able to remove these top two since they are
// handled by the stack on the SOC.
EMBER_AF_WAITING_FOR_DATA_ACK = 0x00000001, //not needed?
EMBER_AF_LAST_POLL_GOT_DATA = 0x00000002, //not needed?
EMBER_AF_WAITING_FOR_SERVICE_DISCOVERY = 0x00000004,
EMBER_AF_WAITING_FOR_ZDO_RESPONSE = 0x00000008,
EMBER_AF_WAITING_FOR_ZCL_RESPONSE = 0x00000010,
EMBER_AF_WAITING_FOR_REGISTRATION = 0x00000020,
EMBER_AF_WAITING_FOR_PARTNER_LINK_KEY_EXCHANGE = 0x00000040,
EMBER_AF_FORCE_SHORT_POLL = 0x00000080,
EMBER_AF_FRAGMENTATION_IN_PROGRESS = 0x00000100,
EMBER_AF_FORCE_SHORT_POLL_FOR_PARENT_CONNECTIVITY = 0x00000200,
EMBER_AF_WAITING_FOR_TC_KEY_UPDATE = 0x00000400,
};
typedef struct {
uint8_t endpoint;
EmberAfClusterId clusterId;
bool isClient;
EmberAfEventPollControl pollControl;
EmberAfEventSleepControl sleepControl;
EmberEventControl *eventControl;
} EmberAfEventContext;
typedef void (*EmberAfNetworkEventHandler)(void);
typedef void (*EmberAfEndpointEventHandler)(uint8_t endpoint);
#ifdef EMBER_AF_PLUGIN_GROUPS_SERVER
#define EMBER_AF_GROUP_TABLE_NULL_INDEX 0xFF
#define EMBER_AF_GROUP_TABLE_UNUSED_ENDPOINT_ID 0x00
#define ZCL_GROUPS_CLUSTER_MAXIMUM_NAME_LENGTH 16
typedef struct {
uint8_t endpoint; // 0x00 when not in use
uint16_t groupId;
uint8_t bindingIndex;
#ifdef EMBER_AF_PLUGIN_GROUPS_SERVER_NAME_SUPPORT
uint8_t name[ZCL_GROUPS_CLUSTER_MAXIMUM_NAME_LENGTH + 1];
#endif
} EmberAfGroupTableEntry;
#endif //EMBER_AF_PLUGIN_GROUPS_SERVER
#define EMBER_AF_SCENE_TABLE_NULL_INDEX 0xFF
#define EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID 0x00
#define ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTH 16
#define ZCL_SCENES_GLOBAL_SCENE_GROUP_ID 0x0000
#define ZCL_SCENES_GLOBAL_SCENE_SCENE_ID 0x00
typedef struct {
uint8_t endpoint; // 0x00 when this record is not in use
uint16_t groupId; // 0x0000 if not associated with a group
uint8_t sceneId;
#ifdef EMBER_AF_PLUGIN_SCENES_NAME_SUPPORT
uint8_t name[ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTH + 1];
#endif
uint16_t transitionTime; // in seconds
uint8_t transitionTime100ms; // in tenths of a seconds
#ifdef ZCL_USING_ON_OFF_CLUSTER_SERVER
bool hasOnOffValue;
bool onOffValue;
#endif
#ifdef ZCL_USING_LEVEL_CONTROL_CLUSTER_SERVER
bool hasCurrentLevelValue;
uint8_t currentLevelValue;
#endif
#ifdef ZCL_USING_THERMOSTAT_CLUSTER_SERVER
bool hasOccupiedCoolingSetpointValue;
int16_t occupiedCoolingSetpointValue;
bool hasOccupiedHeatingSetpointValue;
int16_t occupiedHeatingSetpointValue;
bool hasSystemModeValue;
uint8_t systemModeValue;
#endif
#ifdef ZCL_USING_COLOR_CONTROL_CLUSTER_SERVER
bool hasCurrentXValue;
uint16_t currentXValue;
bool hasCurrentYValue;
uint16_t currentYValue;
bool hasEnhancedCurrentHueValue;
uint16_t enhancedCurrentHueValue;
bool hasCurrentSaturationValue;
uint8_t currentSaturationValue;
bool hasColorLoopActiveValue;
uint8_t colorLoopActiveValue;
bool hasColorLoopDirectionValue;
uint8_t colorLoopDirectionValue;
bool hasColorLoopTimeValue;
uint16_t colorLoopTimeValue;
bool hasColorTemperatureMiredsValue;
uint16_t colorTemperatureMiredsValue;
#endif //ZCL_USING_COLOR_CONTROL_CLUSTER_SERVER
#ifdef ZCL_USING_DOOR_LOCK_CLUSTER_SERVER
bool hasLockStateValue;
uint8_t lockStateValue;
#endif
#ifdef ZCL_USING_WINDOW_COVERING_CLUSTER_SERVER
bool hasCurrentPositionLiftPercentageValue;
uint8_t currentPositionLiftPercentageValue;
bool hasCurrentPositionTiltPercentageValue;
uint8_t currentPositionTiltPercentageValue;
#endif
} EmberAfSceneTableEntry;
#if !defined(EMBER_AF_PLUGIN_MESSAGING_CLIENT)
// In order to be able to forward declare callbacks regardless of whether the plugin
// is enabled, we need to define all data structures. In order to be able to define
// the messaging client data struct, we need to declare this variable.
#define EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE 0
#endif
typedef struct {
bool valid;
bool active;
EmberAfPluginEsiManagementBitmask esiBitmask;
uint8_t clientEndpoint;
uint32_t messageId;
uint8_t messageControl;
uint32_t startTime;
uint32_t endTime;
uint16_t durationInMinutes;
uint8_t message[EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE + 1];
} EmberAfPluginMessagingClientMessage;
#define ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH 11
typedef struct {
bool valid;
bool active;
uint8_t clientEndpoint;
uint32_t providerId;
uint8_t rateLabel[ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH + 1];
uint32_t issuerEventId;
uint32_t currentTime;
uint8_t unitOfMeasure;
uint16_t currency;
uint8_t priceTrailingDigitAndPriceTier;
uint8_t numberOfPriceTiersAndRegisterTier;
uint32_t startTime;
uint32_t endTime;
uint16_t durationInMinutes;
uint32_t price;
uint8_t priceRatio;
uint32_t generationPrice;
uint8_t generationPriceRatio;
uint32_t alternateCostDelivered;
uint8_t alternateCostUnit;
uint8_t alternateCostTrailingDigit;
uint8_t numberOfBlockThresholds;
uint8_t priceControl;
} EmberAfPluginPriceClientPrice;
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfPluginPriceCppAuth
#else
typedef uint8_t EmberAfPluginPriceCppAuth;
enum
#endif
{
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_PENDING = 0,
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_ACCEPTED = 1,
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_REJECTED = 2,
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_FORCED = 3,
EMBER_AF_PLUGIN_PRICE_CPP_AUTH_RESERVED = 4
};
#define EMBER_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_ID 0x00
typedef struct {
EmberAfReportingDirection direction;
uint8_t endpoint;
EmberAfClusterId clusterId;
EmberAfAttributeId attributeId;
uint8_t mask;
uint16_t manufacturerCode;
union {
struct {
uint16_t minInterval;
uint16_t maxInterval;
uint32_t reportableChange;
} reported;
struct {
EmberNodeId source;
uint8_t endpoint;
uint16_t timeout;
} received;
} data;
} EmberAfPluginReportingEntry;
typedef enum {
EMBER_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS = 0x00,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_BUSY = 0x01,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_NO_MORE_TUNNEL_IDS = 0x02,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_PROTOCOL_NOT_SUPPORTED = 0x03,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_FLOW_CONTROL_NOT_SUPPORTED = 0x04,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_REQUEST_FAILED = 0xF9,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_NOT_FOUND = 0xFA,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_ADDRESS_TABLE_FULL = 0xFB,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_REQUEST_FAILED = 0xFC,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_FAILED = 0xFD,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_FAILED = 0xFE,
EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_TIMEOUT = 0xFF,
} EmberAfPluginTunnelingClientStatus;
#ifdef EMBER_AF_PLUGIN_ZLL_COMMISSIONING_COMMON
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfZllCommissioningStatus
#else
typedef uint8_t EmberAfZllCommissioningStatus;
enum
#endif
{
EMBER_AF_ZLL_ABORTED_BY_APPLICATION = 0x00,
EMBER_AF_ZLL_CHANNEL_CHANGE_FAILED = 0x01,
EMBER_AF_ZLL_JOINING_FAILED = 0x02,
EMBER_AF_ZLL_NO_NETWORKS_FOUND = 0x03,
EMBER_AF_ZLL_PREEMPTED_BY_STACK = 0x04,
EMBER_AF_ZLL_SENDING_START_JOIN_FAILED = 0x05,
EMBER_AF_ZLL_SENDING_DEVICE_INFORMATION_REQUEST_FAILED = 0x06,
EMBER_AF_ZLL_SENDING_IDENTIFY_REQUEST_FAILED = 0x07,
EMBER_AF_ZLL_SENDING_RESET_TO_FACTORY_NEW_REQUEST_FAILED = 0x08,
EMBER_AF_ZLL_NETWORK_FORMATION_FAILED = 0x09,
EMBER_AF_ZLL_NETWORK_UPDATE_OPERATION = 0x0A,
};
typedef struct {
EmberMulticastId groupId;
uint8_t groupType;
} EmberAfPluginZllCommissioningGroupInformationRecord;
typedef struct {
EmberNodeId networkAddress;
uint8_t endpointId;
uint16_t profileId;
uint16_t deviceId;
uint8_t version;
} EmberAfPluginZllCommissioningEndpointInformationRecord;
#endif
typedef struct {
uint16_t manufacturerId;
uint16_t imageTypeId;
uint32_t firmwareVersion;
uint8_t deviceSpecificFileEui64[EUI64_SIZE];
} EmberAfOtaImageId;
enum {
EMBER_AF_IMAGE_BLOCK_REQUEST_OPTIONS_NONE = 0x00,
// Client supports Min Block Request field
EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_CLIENT = 0x01,
// Server supports Min Block Request field
EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_SERVER = 0x02,
// The Image Block Request is actually simulated in place of an actually
// received Image Page Request
EMBER_AF_IMAGE_BLOCK_REQUEST_SIMULATED_FROM_PAGE_REQUEST = 0x04
};
typedef uint8_t EmberAfImageBlockRequestOptions;
typedef struct {
const EmberAfOtaImageId* id;
uint32_t offset;
uint32_t waitTimeSecondsResponse;
EmberNodeId source;
EmberEUI64 sourceEui; // optionally present in messages
// The minBlockRequestPeriod can be treated as milliseconds or seconds on the
// client. The OTA server plugin has optional support to probe clients and
// treat this field with appropriate units (ms or sec)
uint16_t minBlockRequestPeriod; // optionally present in messages
uint8_t maxDataSize;
uint8_t clientEndpoint;
EmberAfImageBlockRequestOptions bitmask;
} EmberAfImageBlockRequestCallbackStruct;
typedef enum {
EMBER_AF_OTA_STORAGE_SUCCESS = 0,
EMBER_AF_OTA_STORAGE_ERROR = 1,
EMBER_AF_OTA_STORAGE_RETURN_DATA_TOO_LONG = 2,
EMBER_AF_OTA_STORAGE_PARTIAL_FILE_FOUND = 3,
EMBER_AF_OTA_STORAGE_OPERATION_IN_PROGRESS = 4,
} EmberAfOtaStorageStatus;
enum {
EMBER_AF_OTA_DOWNLOAD_AND_VERIFY_SUCCESS = 0,
EMBER_AF_OTA_DOWNLOAD_TIME_OUT = 1,
EMBER_AF_OTA_VERIFY_FAILED = 2,
EMBER_AF_OTA_SERVER_ABORTED = 3,
EMBER_AF_OTA_CLIENT_ABORTED = 4,
EMBER_AF_OTA_ERASE_FAILED = 5,
};
typedef uint8_t EmberAfOtaDownloadResult;
#define EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH 32
#define UID_SIZE 32
typedef struct {
// Magic Number omitted since it is always the same.
uint16_t headerVersion;
uint16_t headerLength;
uint16_t fieldControl;
uint16_t manufacturerId;
uint16_t imageTypeId; // a.k.a. Device ID
uint32_t firmwareVersion;
uint16_t zigbeeStackVersion;
uint8_t headerString[EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH + 1];
uint32_t imageSize;
uint8_t securityCredentials;
union {
uint8_t EUI64[EUI64_SIZE];
uint8_t UID[UID_SIZE];
} upgradeFileDestination;
uint16_t minimumHardwareVersion;
uint16_t maximumHardwareVersion;
} EmberAfOtaHeader;
typedef struct {
uint16_t id;
uint32_t length;
} EmberAfTagData;
typedef enum {
NO_APP_MESSAGE = 0,
RECEIVED_PARTNER_CERTIFICATE = 1,
GENERATING_EPHEMERAL_KEYS = 2,
GENERATING_SHARED_SECRET = 3,
KEY_GENERATION_DONE = 4,
GENERATE_SHARED_SECRET_DONE = 5,
LINK_KEY_ESTABLISHED = 6,
NO_LOCAL_RESOURCES = 7,
PARTNER_NO_RESOURCES = 8,
TIMEOUT_OCCURRED = 9,
INVALID_APP_COMMAND = 10,
MESSAGE_SEND_FAILURE = 11,
PARTNER_SENT_TERMINATE = 12,
INVALID_PARTNER_MESSAGE = 13,
PARTNER_SENT_DEFAULT_RESPONSE_ERROR = 14,
BAD_CERTIFICATE_ISSUER = 15,
KEY_CONFIRM_FAILURE = 16,
BAD_KEY_ESTABLISHMENT_SUITE = 17,
KEY_TABLE_FULL = 18,
NO_ESTABLISHMENT_ALLOWED = 19,
/* 283k1 certificates need to have valid key usage
*/
INVALID_CERTIFICATE_KEY_USAGE = 20,
} EmberAfKeyEstablishmentNotifyMessage;
#define APP_NOTIFY_ERROR_CODE_START NO_LOCAL_RESOURCES
#define APP_NOTIFY_MESSAGE_TEXT { \
"None", \
"Received Cert", \
"Generate keys", \
"Generate secret", \
"Key generate done", \
"Generate secret done", \
"Link key verified", \
\
/* Transient Error codes */ \
"No local resources", \
"Partner no resources", \
"Timeout", \
"Invalid app. command", \
"Message send failure", \
"Partner sent terminate", \
"Bad message", \
"Partner sent Default Rsp", \
\
/* Fatal errors */ \
"Bad cert issuer", \
"Key confirm failure", \
"Bad key est. suite", \
"Key table full", \
"Not allowed", \
"Invalid Key Usage", \
}
typedef enum {
EMBER_AF_IMAGE_GOOD = 0,
EMBER_AF_IMAGE_BAD = 1,
EMBER_AF_IMAGE_VERIFY_IN_PROGRESS = 2,
#ifndef DOXYGEN_SHOULD_SKIP_THIS
// Internal use only.
EMBER_AF_IMAGE_VERIFY_WAIT = 3,
EMBER_AF_IMAGE_VERIFY_ERROR = 4,
EMBER_AF_IMAGE_UNKNOWN = 5,
EMBER_AF_NO_IMAGE_VERIFY_SUPPORT = 6,
#endif
} EmberAfImageVerifyStatus;
typedef void (*EmberAfTickFunction)(uint8_t endpoint);
typedef void (*EmberAfInitFunction)(uint8_t endpoint);
typedef void (*EmberAfClusterAttributeChangedCallback)(uint8_t endpoint,
EmberAfAttributeId attributeId);
typedef void (*EmberAfManufacturerSpecificClusterAttributeChangedCallback)(uint8_t endpoint,
EmberAfAttributeId attributeId,
uint16_t manufacturerCode);
typedef EmberAfStatus (*EmberAfClusterPreAttributeChangedCallback)(uint8_t endpoint,
EmberAfAttributeId attributeId,
EmberAfAttributeType attributeType,
uint8_t size,
uint8_t *value);
typedef void (*EmberAfDefaultResponseFunction)(uint8_t endpoint,
uint8_t commandId,
EmberAfStatus status);
typedef void (*EmberAfMessageSentFunction)(EmberOutgoingMessageType type,
uint16_t indexOrDestination,
EmberApsFrame *apsFrame,
uint16_t msgLen,
uint8_t *message,
EmberStatus status);
typedef struct {
EmberAfMessageSentFunction callback;
EmberApsFrame* apsFrame;
uint8_t* message;
uint16_t indexOrDestination;
uint16_t messageLength;
EmberOutgoingMessageType type;
bool broadcast;
} EmberAfMessageStruct;
typedef struct {
EmberEUI64 deviceId;
EmberKeyData key;
} EmberAfLinkKeyBackupData;
typedef struct {
EmberEUI64 extendedPanId;
uint8_t keyListLength;
uint8_t maxKeyListLength;
EmberAfLinkKeyBackupData* keyList;
} EmberAfTrustCenterBackupData;
#define EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH 16
typedef struct {
uint8_t hardwareTag[EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH];
uint8_t eui64[EUI64_SIZE];
uint16_t mfgId;
uint16_t bootloaderVersion;
uint8_t capabilities;
uint8_t platform;
uint8_t micro;
uint8_t phy;
bool bootloaderActive;
} EmberAfStandaloneBootloaderQueryResponseData;
typedef struct {
uint16_t clusterId;
uint8_t commandId;
uint8_t mask;
} EmberAfCommandMetadata;
typedef struct {
uint16_t year;
uint8_t month;
uint8_t day;
uint8_t hours;
uint8_t minutes;
uint8_t seconds;
} EmberAfTimeStruct;
typedef struct {
uint8_t year;
uint8_t month;
uint8_t dayOfMonth;
uint8_t dayOfWeek;
} EmberAfDate;
/* Simple Metering Server Test Code */
#define EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_ELECTRIC_METER 0
#define EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_GAS_METER 1
// Functional Notification Flags
// Also #defined in enums.h under slightly different names
#define EMBER_AF_METERING_FNF_NEW_OTA_FIRMWARE 0x00000001
#define EMBER_AF_METERING_FNF_CBKE_UPDATE_REQUEST 0x00000002
#define EMBER_AF_METERING_FNF_TIME_SYNC 0x00000004
#define EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_HAN 0x00000010
#define EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_WAN 0x00000020
#define EMBER_AF_METERING_FNF_PUSH_HISTORICAL_METERING_DATA_ATTRIBUTE_SET 0x000001C0
#define EMBER_AF_METERING_FNF_PUSH_HISTORICAL_PREPAYMENT_DATA_ATTRIBUTE_SET 0x00000E00
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_BASIC_CLUSTER 0x00001000
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_METERING_CLUSTER 0x00002000
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_PREPAYMENT_CLUSTER 0x00004000
#define EMBER_AF_METERING_FNF_NETWORK_KEY_ACTIVE 0x00008000
#define EMBER_AF_METERING_FNF_DISPLAY_MESSAGE 0x00010000
#define EMBER_AF_METERING_FNF_CANCEL_ALL_MESSAGES 0x00020000
#define EMBER_AF_METERING_FNF_CHANGE_SUPPLY 0x00040000
#define EMBER_AF_METERING_FNF_LOCAL_CHANGE_SUPPLY 0x00080000
#define EMBER_AF_METERING_FNF_SET_UNCONTROLLED_FLOW_THRESHOLD 0x00100000
#define EMBER_AF_METERING_FNF_TUNNEL_MESSAGE_PENDING 0x00200000
#define EMBER_AF_METERING_FNF_GET_SNAPSHOT 0x00400000
#define EMBER_AF_METERING_FNF_GET_SAMPLED_DATA 0x00800000
#define EMBER_AF_METERING_FNF_NEW_SUB_GHZ_CHANNEL_MASKS_AVAILABLE 0x01000000
#define EMBER_AF_METERING_FNF_ENERGY_SCAN_PENDING 0x02000000
#define EMBER_AF_METERING_FNF_CHANNEL_CHANGE_PENDING 0x04000000
// Notification Flags 2
#define EMBER_AF_METERING_NF2_PUBLISH_PRICE 0x00000001
#define EMBER_AF_METERING_NF2_PUBLISH_BLOCK_PERIOD 0x00000002
#define EMBER_AF_METERING_NF2_PUBLISH_TARIFF_INFORMATION 0x00000004
#define EMBER_AF_METERING_NF2_PUBLISH_CONVERSION_FACTOR 0x00000008
#define EMBER_AF_METERING_NF2_PUBLISH_CALORIFIC_VALUE 0x00000010
#define EMBER_AF_METERING_NF2_PUBLISH_CO2_VALUE 0x00000020
#define EMBER_AF_METERING_NF2_PUBLISH_BILLING_PERIOD 0x00000040
#define EMBER_AF_METERING_NF2_PUBLISH_CONSOLIDATED_BILL 0x00000080
#define EMBER_AF_METERING_NF2_PUBLISH_PRICE_MATRIX 0x00000100
#define EMBER_AF_METERING_NF2_PUBLISH_BLOCK_THRESHOLDS 0x00000200
#define EMBER_AF_METERING_NF2_PUBLISH_CURRENCY_CONVERSION 0x00000400
#define EMBER_AF_METERING_NF2_PUBLISH_CREDIT_PAYMENT_INFO 0x00001000
#define EMBER_AF_METERING_NF2_PUBLISH_CPP_EVENT 0x00002000
#define EMBER_AF_METERING_NF2_PUBLISH_TIER_LABELS 0x00004000
#define EMBER_AF_METERING_NF2_CANCEL_TARIFF 0x00008000
// Notification Flags 3
#define EMBER_AF_METERING_NF3_PUBLISH_CALENDAR 0x00000001
#define EMBER_AF_METERING_NF3_PUBLISH_SPECIAL_DAYS 0x00000002
#define EMBER_AF_METERING_NF3_PUBLISH_SEASONS 0x00000004
#define EMBER_AF_METERING_NF3_PUBLISH_WEEK 0x00000008
#define EMBER_AF_METERING_NF3_PUBLISH_DAY 0x00000010
#define EMBER_AF_METERING_NF3_CANCEL_CALENDAR 0x00000020
// Notification Flags 4
#define EMBER_AF_METERING_NF4_SELECT_AVAILABLE_EMERGENCY_CREDIT 0x00000001
#define EMBER_AF_METERING_NF4_CHANGE_DEBT 0x00000002
#define EMBER_AF_METERING_NF4_EMERGENCY_CREDIT_SETUP 0x00000004
#define EMBER_AF_METERING_NF4_CONSUMER_TOP_UP 0x00000008
#define EMBER_AF_METERING_NF4_CREDIT_ADJUSTMENT 0x00000010
#define EMBER_AF_METERING_NF4_CHANGE_PAYMENT_MODE 0x00000020
#define EMBER_AF_METERING_NF4_GET_PREPAY_SNAPSHOT 0x00000040
#define EMBER_AF_METERING_NF4_GET_TOP_UP_LOG 0x00000080
#define EMBER_AF_METERING_NF4_SET_LOW_CREDIT_WARNING_LEVEL 0x00000100
#define EMBER_AF_METERING_NF4_GET_DEBT_REPAYMENT_LOG 0x00000200
#define EMBER_AF_METERING_NF4_SET_MAXIMUM_CREDIT_LIMIT 0x00000400
#define EMBER_AF_METERING_NF4_SET_OVERALL_DEBT_CAP 0x00000800
// Notification Flags 5
#define EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_TENANCY 0x00000001
#define EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_SUPPLIER 0x00000002
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_1_RESPONSE 0x00000004
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_2_RESPONSE 0x00000008
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_3_RESPONSE 0x00000010
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_4_RESPONSE 0x00000020
#define EMBER_AF_METERING_NF5_UPDATE_SITE_ID 0x00000040
#define EMBER_AF_METERING_NF5_RESET_BATTERY_COUNTER 0x00000080
#define EMBER_AF_METERING_NF5_UPDATE_CIN 0x00000100
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfCbkeKeyEstablishmentSuite
#else
typedef uint16_t EmberAfCbkeKeyEstablishmentSuite;
enum
#endif
{
EMBER_AF_INVALID_KEY_ESTABLISHMENT_SUITE = 0x0000,
EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1 = 0x0001,
EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1 = 0x0002,
};
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH (16)
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH (18)
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH (32)
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH (24)
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH (10)
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfDeviceManagementPasswordType
#else
typedef uint16_t EmberAfDeviceManagementPasswordType;
enum
#endif
{
UNUSED_PASSWORD = 0x00,
SERVICE_PASSWORD = 0x01,
CONSUMER_PASSWORD = 0x02,
};
#ifdef DOXYGEN_SHOULD_SKIP_THIS
enum EmberAfDeviceManagementChangePendingFlags
#else
typedef uint8_t EmberAfDeviceManagementChangePendingFlags;
enum
#endif
{
EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_TENANCY_PENDING_MASK = 0x01,
EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_SUPPLIER_PENDING_MASK = 0x02,
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SITE_ID_PENDING_MASK = 0x04,
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CIN_PENDING_MASK = 0x08,
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SERVICE_PASSWORD_PENDING_MASK = 0x10,
EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CONSUMER_PASSWORD_PENDING_MASK = 0x20,
};
typedef struct {
// Optional fields only used by Gas Proxy Function plugin.
uint32_t providerId;
uint32_t issuerEventId;
uint8_t tariffType;
// always used fields
uint32_t implementationDateTime;
uint32_t tenancy;
} EmberAfDeviceManagementTenancy;
typedef struct {
uint32_t proposedProviderId;
uint32_t implementationDateTime;
uint32_t providerChangeControl;
uint8_t proposedProviderName[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH + 1];
uint8_t proposedProviderContactDetails[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH + 1];
} EmberAfDeviceManagementSupplier;
typedef struct {
uint32_t requestDateTime;
uint32_t implementationDateTime;
uint8_t supplyStatus;
uint8_t originatorIdSupplyControlBits;
} EmberAfDeviceManagementSupply;
typedef struct {
uint8_t siteId[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH + 1];
uint32_t implementationDateTime;
uint32_t issuerEventId;
} EmberAfDeviceManagementSiteId;
typedef struct {
uint8_t cin[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH + 1];
uint32_t implementationDateTime;
uint32_t issuerEventId;
} EmberAfDeviceManagementCIN;
typedef struct {
bool supplyTamperState;
bool supplyDepletionState;
bool supplyUncontrolledFlowState;
bool loadLimitSupplyState;
} EmberAfDeviceManagementSupplyStatusFlags;
typedef struct {
uint16_t uncontrolledFlowThreshold;
uint16_t multiplier;
uint16_t divisor;
uint16_t measurementPeriod;
uint8_t unitOfMeasure;
uint8_t stabilisationPeriod;
} EmberAfDeviceManagementUncontrolledFlowThreshold;
typedef struct {
uint32_t implementationDateTime;
uint8_t supplyStatus;
} EmberAfDeviceManagementSupplyStatus;
typedef struct {
uint8_t password[EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH + 1];
uint32_t implementationDateTime;
uint16_t durationInMinutes;
EmberAfDeviceManagementPasswordType passwordType;
} EmberAfDeviceManagementPassword;
typedef struct {
EmberAfDeviceManagementTenancy tenancy;
EmberAfDeviceManagementSupplier supplier;
EmberAfDeviceManagementSupply supply;
EmberAfDeviceManagementSiteId siteId;
EmberAfDeviceManagementCIN cin;
EmberAfDeviceManagementSupplyStatusFlags supplyStatusFlags;
EmberAfDeviceManagementSupplyStatus supplyStatus;
//TODO: These passwords ought to be tokenized / hashed
EmberAfDeviceManagementPassword servicePassword;
EmberAfDeviceManagementPassword consumerPassword;
EmberAfDeviceManagementUncontrolledFlowThreshold threshold;
uint32_t providerId;
uint32_t issuerEventId;
uint8_t proposedLocalSupplyStatus;
EmberAfTariffType tariffType;
EmberAfDeviceManagementChangePendingFlags pendingUpdates;
} EmberAfDeviceManagementInfo;
typedef struct {
uint8_t startIndex;
uint8_t endIndex;
} EmberAfDeviceManagementAttributeRange;
// attrRange is a list of attributeId values in a cluster. It's needed to track contigous
// segments of valid attributeId's with gaps in the middle.
// attributeSetId is the value of the upper byte in the attributeId. It ranges from 0x01(Price)
// to 0x08(OTA Event Configuration)
// Eg. {0x00,0x05} and {0x08,0x0A}
// We're betting that there isn't a list of cluster attributes that has more than 5 gaps.
typedef struct {
uint8_t attributeSetId;
EmberAfDeviceManagementAttributeRange attributeRange[7];
} EmberAfDeviceManagementAttributeTable;
typedef struct {
bool encryption;
uint8_t * plainPayload;
uint16_t plainPayloadLength;
uint8_t * encryptedPayload;
uint16_t encryptedPayloadLength;
} EmberAfGbzMessageData;
typedef struct {
uint8_t * gbzCommands;
uint16_t gbzCommandsLength;
uint8_t * gbzCommandsResponse;
uint16_t gbzCommandsResponseLength;
uint16_t messageCode;
} EmberAfGpfMessage;
typedef uint16_t EmberAfRemoteClusterType;
#define EMBER_AF_REMOTE_CLUSTER_TYPE_NONE 0x0000
#define EMBER_AF_REMOTE_CLUSTER_TYPE_SERVER 0x0001
#define EMBER_AF_REMOTE_CLUSTER_TYPE_CLIENT 0x0002
#define EMBER_AF_REMOTE_CLUSTER_TYPE_INVALID 0xFFFF
typedef struct {
EmberAfClusterId clusterId;
EmberAfProfileId profileId;
uint16_t deviceId;
uint8_t endpoint;
EmberAfRemoteClusterType type;
} EmberAfRemoteClusterStruct;
typedef struct {
EmberEUI64 targetEUI64;
uint8_t sourceEndpoint;
uint8_t destEndpoint;
uint16_t clusterId;
EmberEUI64 destEUI64;
EmberEUI64 sourceEUI64;
} EmberAfRemoteBindingStruct;
typedef struct {
EmberAfClusterId clusterId;
bool server;
} EmberAfClusterInfo;
#if !defined(EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT)
#define EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT 3
#endif
typedef struct {
EmberAfClusterInfo clusters[EMBER_AF_MAX_CLUSTERS_PER_ENDPOINT];
EmberAfProfileId profileId;
uint16_t deviceId;
uint8_t endpoint;
uint8_t clusterCount;
} EmberAfEndpointInfoStruct;
#if !defined(EMBER_AF_MAX_ENDPOINTS_PER_DEVICE)
#define EMBER_AF_MAX_ENDPOINTS_PER_DEVICE 1
#endif
// Although we treat this like a bitmap, only 1 bit is set at a time.
// We use the bitmap feature to allow us to find all devices
// with any in a set of status codes using
// emberAfPluginDeviceDatabaseFindDeviceByStatus().
typedef enum {
EMBER_AF_DEVICE_DISCOVERY_STATUS_NONE = 0x00,
EMBER_AF_DEVICE_DISCOVERY_STATUS_NEW = 0x01,
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_ENDPOINTS = 0x02,
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_CLUSTERS = 0x04,
EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_STACK_REVISION = 0x08,
EMBER_AF_DEVICE_DISCOVERY_STATUS_DONE = 0x40,
EMBER_AF_DEVICE_DISCOVERY_STATUS_FAILED = 0x80,
} EmberAfDeviceDiscoveryStatus;
typedef struct {
EmberEUI64 eui64;
EmberAfEndpointInfoStruct endpoints[EMBER_AF_MAX_ENDPOINTS_PER_DEVICE];
EmberAfDeviceDiscoveryStatus status;
uint8_t discoveryFailures;
uint8_t capabilities;
uint8_t endpointCount;
uint8_t stackRevision;
} EmberAfDeviceInfo;
typedef struct {
uint16_t deviceIndex;
} EmberAfDeviceDatabaseIterator;
typedef struct {
EmberNodeId emberNodeId;
uint32_t timeStamp;
} EmberAfJoiningDevice;
#define EMBER_AF_INVALID_CLUSTER_ID 0xFFFF
#define EMBER_AF_INVALID_ENDPOINT 0xFF
#define EMBER_AF_INVALID_PAN_ID 0xFFFF
#define EMBER_AF_PERMIT_JOIN_FOREVER 0xFF
#define EMBER_AF_PERMIT_JOIN_MAX_TIMEOUT 0xFE
#define EMBER_AF_ZDO_RESPONSE_OVERHEAD 2
#endif // SILABS_AF_API_TYPES
Macros#
A distinguished manufacturer code that is used to indicate the absence of a manufacturer-specific profile, cluster, command, or attribute.
An invalid profile ID This is a reserved profileId.
A simple way to determine if the service discovery callback has a response.
Indicates the absence of a Scene table entry.
Value used when setting or getting the endpoint in a Scene table entry. It indicates that the entry is not in use.
Maximum length of Scene names, not including the length byte.
The group identifier for the global scene.
The scene identifier for the global scene.
Value used when setting or getting the endpoint in a report table entry. It indicates that the entry is not in use.
The maximum size of the string that is present in the header of the zigbee Over-the-air file format.
The length of the hardware tag in the Ember Bootloader Query Response.
Device Management plugin types.
Permit join times.
The overhead of the ZDO response. 1 byte for the sequence and 1 byte for the status code.
Enumerations#
This is an enum used to indicate the result of the service discovery. Unicast discoveries are completed as soon as a response is received. Broadcast discoveries wait a period of time for multiple responses to be received.
This is an enum used to control how the device will poll for a given active cluster-related event. When the event is scheduled, the application can pass a poll control value which will be stored along with the event. The processor is only allowed to poll according to the most restrictive value for all active event. For instance, if two events are active, one with EMBER_AF_LONG_POLL and the other with EMBER_AF_SHORT_POLL, then the processor will short poll until the second event is deactivated.
This is an enum used to control how the device will sleep for a given active cluster related event. When the event is scheduled, the scheduling code can pass a sleep control value which will be stored along with the event. The processor is only allowed to sleep according to the most restrictive sleep control value for any active event. For instance, if two events are active, one with EMBER_AF_OK_TO_HIBERNATE and the other with EMBER_AF_OK_TO_NAP, then the processor will only be allowed to nap until the second event is deactivated.
An enum used to track the tasks that the Application framework cares about. These are intended to be tasks that should keep the device out of hibernation like an application level request / response. If the response does not come in as a data ack, then the application will need to stay out of hibernation to wait and poll for it.
Specifies CPP Authorization values.
The list of options possible for the image block request/response.
This status contains the success or error code of an OTA storage device operation.
This status contains the success or error code of an OTA download operation.
This enumeration is used to indicate the state of an OTA bootload image undergoing verification. This is used both for cryptographic verification and manufacturer specific verification.
CBKE Library types.
Typedefs#
Type for referring to zigbee application profile id.
Type for referring to ZCL attribute id.
Type for referring to ZCL cluster id.
Type for referring to ZCL attribute type.
Type for the cluster mask.
Type for the attribute mask.
Generic function type, used for either of the cluster function.
Interpan Message type: unicast, broadcast, or multicast.
The options for sending/receiving interpan messages.
The options for what interpan messages are allowed.
Bitmask data type for storing one bit of information for each ESI in the ESI table.
This defines a callback where a code element or cluster can be informed as to the result of a service discovery they have requested. For each match, the callback is fired with all the resulting matches from that source. If the discovery was unicast to a specific device, then the callback will only be fired once with either MATCH_FOUND or COMPLETE (no matches found). If the discovery is broadcast then multiple callbacks may be fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED. After a couple seconds the callback will then be fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE or EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE as the result.
This defines a callback where a code element or cluster can be informed as to the result of a request to initiate a partner link key exchange. The callback will be triggered with success equal to true if the exchange completed successfully.
Type for referring to the handler for network events.
Type for referring to the handler for endpoint events.
Type for referring to the tick callback for cluster.
Type for referring to the init callback for cluster.
Type for referring to the attribute changed callback function.
Type for referring to the manufacturer specific attribute changed callback function.
Type for referring to the pre-attribute changed callback function.
Type for referring to the default response callback function.
Type for referring to the message sent callback function.
Zigbee Internet Client/Server Remote Cluster Types.
Macro Definition Documentation#
EMBER_AF_NULL_MANUFACTURER_CODE#
#define EMBER_AF_NULL_MANUFACTURER_CODEValue:
0x0000
A distinguished manufacturer code that is used to indicate the absence of a manufacturer-specific profile, cluster, command, or attribute.
EMBER_AF_INVALID_PROFILE_ID#
#define EMBER_AF_INVALID_PROFILE_IDValue:
0xFFFF
An invalid profile ID This is a reserved profileId.
EMBER_AF_INTERPAN_OPTION_MAC_HAS_LONG_ADDRESS#
#define EMBER_AF_INTERPAN_OPTION_MAC_HAS_LONG_ADDRESSValue:
0x0002
EMBER_AF_INTERPAN_DIRECTION_CLIENT_TO_SERVER#
#define EMBER_AF_INTERPAN_DIRECTION_CLIENT_TO_SERVERValue:
0x01
EMBER_AF_INTERPAN_DIRECTION_SERVER_TO_CLIENT#
#define EMBER_AF_INTERPAN_DIRECTION_SERVER_TO_CLIENTValue:
0x02
EMBER_AF_ALLOW_TC_KEY_REQUESTS#
#define EMBER_AF_ALLOW_TC_KEY_REQUESTSValue:
EMBER_ALLOW_TC_LINK_KEY_REQUEST_AND_SEND_CURRENT_KEY
EMBER_AF_DENY_TC_KEY_REQUESTS#
#define EMBER_AF_DENY_TC_KEY_REQUESTSValue:
EMBER_DENY_TC_LINK_KEY_REQUESTS
EMBER_AF_ALLOW_APP_KEY_REQUESTS#
#define EMBER_AF_ALLOW_APP_KEY_REQUESTSValue:
EMBER_ALLOW_APP_LINK_KEY_REQUEST
EMBER_AF_DENY_APP_KEY_REQUESTS#
#define EMBER_AF_DENY_APP_KEY_REQUESTSValue:
EMBER_DENY_APP_LINK_KEY_REQUESTS
emberAfHaveDiscoveryResponseStatus#
#define emberAfHaveDiscoveryResponseStatusValue:
(status)
A simple way to determine if the service discovery callback has a response.
EMBER_AF_SCENE_TABLE_NULL_INDEX#
#define EMBER_AF_SCENE_TABLE_NULL_INDEXValue:
0xFF
Indicates the absence of a Scene table entry.
EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_ID#
#define EMBER_AF_SCENE_TABLE_UNUSED_ENDPOINT_IDValue:
0x00
Value used when setting or getting the endpoint in a Scene table entry. It indicates that the entry is not in use.
ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTH#
#define ZCL_SCENES_CLUSTER_MAXIMUM_NAME_LENGTHValue:
16
Maximum length of Scene names, not including the length byte.
ZCL_SCENES_GLOBAL_SCENE_GROUP_ID#
#define ZCL_SCENES_GLOBAL_SCENE_GROUP_IDValue:
0x0000
The group identifier for the global scene.
ZCL_SCENES_GLOBAL_SCENE_SCENE_ID#
#define ZCL_SCENES_GLOBAL_SCENE_SCENE_IDValue:
0x00
The scene identifier for the global scene.
EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZE#
#define EMBER_AF_PLUGIN_MESSAGING_CLIENT_MESSAGE_SIZEValue:
0
ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTH#
#define ZCL_PRICE_CLUSTER_MAXIMUM_RATE_LABEL_LENGTHValue:
11
EMBER_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_ID#
#define EMBER_AF_PLUGIN_REPORTING_UNUSED_ENDPOINT_IDValue:
0x00
Value used when setting or getting the endpoint in a report table entry. It indicates that the entry is not in use.
EMBER_AF_OTA_MAX_HEADER_STRING_LENGTH#
#define EMBER_AF_OTA_MAX_HEADER_STRING_LENGTHValue:
32
The maximum size of the string that is present in the header of the zigbee Over-the-air file format.
APP_NOTIFY_MESSAGE_TEXT#
#define APP_NOTIFY_MESSAGE_TEXTValue:
EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH#
#define EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTHValue:
16
The length of the hardware tag in the Ember Bootloader Query Response.
EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_ELECTRIC_METER#
#define EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_ELECTRIC_METERValue:
0
EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_GAS_METER#
#define EMBER_AF_PLUGIN_SIMPLE_METERING_SERVER_GAS_METERValue:
1
EMBER_AF_METERING_FNF_NEW_OTA_FIRMWARE#
#define EMBER_AF_METERING_FNF_NEW_OTA_FIRMWAREValue:
0x00000001
EMBER_AF_METERING_FNF_CBKE_UPDATE_REQUEST#
#define EMBER_AF_METERING_FNF_CBKE_UPDATE_REQUESTValue:
0x00000002
EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_HAN#
#define EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_HANValue:
0x00000010
EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_WAN#
#define EMBER_AF_METERING_FNF_STAY_AWAKE_REQUEST_WANValue:
0x00000020
EMBER_AF_METERING_FNF_PUSH_HISTORICAL_METERING_DATA_ATTRIBUTE_SET#
#define EMBER_AF_METERING_FNF_PUSH_HISTORICAL_METERING_DATA_ATTRIBUTE_SETValue:
0x000001C0
EMBER_AF_METERING_FNF_PUSH_HISTORICAL_PREPAYMENT_DATA_ATTRIBUTE_SET#
#define EMBER_AF_METERING_FNF_PUSH_HISTORICAL_PREPAYMENT_DATA_ATTRIBUTE_SETValue:
0x00000E00
EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_BASIC_CLUSTER#
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_BASIC_CLUSTERValue:
0x00001000
EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_METERING_CLUSTER#
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_METERING_CLUSTERValue:
0x00002000
EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_PREPAYMENT_CLUSTER#
#define EMBER_AF_METERING_FNF_PUSH_ALL_STATIC_DATA_PREPAYMENT_CLUSTERValue:
0x00004000
EMBER_AF_METERING_FNF_NETWORK_KEY_ACTIVE#
#define EMBER_AF_METERING_FNF_NETWORK_KEY_ACTIVEValue:
0x00008000
EMBER_AF_METERING_FNF_CANCEL_ALL_MESSAGES#
#define EMBER_AF_METERING_FNF_CANCEL_ALL_MESSAGESValue:
0x00020000
EMBER_AF_METERING_FNF_LOCAL_CHANGE_SUPPLY#
#define EMBER_AF_METERING_FNF_LOCAL_CHANGE_SUPPLYValue:
0x00080000
EMBER_AF_METERING_FNF_SET_UNCONTROLLED_FLOW_THRESHOLD#
#define EMBER_AF_METERING_FNF_SET_UNCONTROLLED_FLOW_THRESHOLDValue:
0x00100000
EMBER_AF_METERING_FNF_TUNNEL_MESSAGE_PENDING#
#define EMBER_AF_METERING_FNF_TUNNEL_MESSAGE_PENDINGValue:
0x00200000
EMBER_AF_METERING_FNF_GET_SAMPLED_DATA#
#define EMBER_AF_METERING_FNF_GET_SAMPLED_DATAValue:
0x00800000
EMBER_AF_METERING_FNF_NEW_SUB_GHZ_CHANNEL_MASKS_AVAILABLE#
#define EMBER_AF_METERING_FNF_NEW_SUB_GHZ_CHANNEL_MASKS_AVAILABLEValue:
0x01000000
EMBER_AF_METERING_FNF_ENERGY_SCAN_PENDING#
#define EMBER_AF_METERING_FNF_ENERGY_SCAN_PENDINGValue:
0x02000000
EMBER_AF_METERING_FNF_CHANNEL_CHANGE_PENDING#
#define EMBER_AF_METERING_FNF_CHANNEL_CHANGE_PENDINGValue:
0x04000000
EMBER_AF_METERING_NF2_PUBLISH_BLOCK_PERIOD#
#define EMBER_AF_METERING_NF2_PUBLISH_BLOCK_PERIODValue:
0x00000002
EMBER_AF_METERING_NF2_PUBLISH_TARIFF_INFORMATION#
#define EMBER_AF_METERING_NF2_PUBLISH_TARIFF_INFORMATIONValue:
0x00000004
EMBER_AF_METERING_NF2_PUBLISH_CONVERSION_FACTOR#
#define EMBER_AF_METERING_NF2_PUBLISH_CONVERSION_FACTORValue:
0x00000008
EMBER_AF_METERING_NF2_PUBLISH_CALORIFIC_VALUE#
#define EMBER_AF_METERING_NF2_PUBLISH_CALORIFIC_VALUEValue:
0x00000010
EMBER_AF_METERING_NF2_PUBLISH_CO2_VALUE#
#define EMBER_AF_METERING_NF2_PUBLISH_CO2_VALUEValue:
0x00000020
EMBER_AF_METERING_NF2_PUBLISH_BILLING_PERIOD#
#define EMBER_AF_METERING_NF2_PUBLISH_BILLING_PERIODValue:
0x00000040
EMBER_AF_METERING_NF2_PUBLISH_CONSOLIDATED_BILL#
#define EMBER_AF_METERING_NF2_PUBLISH_CONSOLIDATED_BILLValue:
0x00000080
EMBER_AF_METERING_NF2_PUBLISH_PRICE_MATRIX#
#define EMBER_AF_METERING_NF2_PUBLISH_PRICE_MATRIXValue:
0x00000100
EMBER_AF_METERING_NF2_PUBLISH_BLOCK_THRESHOLDS#
#define EMBER_AF_METERING_NF2_PUBLISH_BLOCK_THRESHOLDSValue:
0x00000200
EMBER_AF_METERING_NF2_PUBLISH_CURRENCY_CONVERSION#
#define EMBER_AF_METERING_NF2_PUBLISH_CURRENCY_CONVERSIONValue:
0x00000400
EMBER_AF_METERING_NF2_PUBLISH_CREDIT_PAYMENT_INFO#
#define EMBER_AF_METERING_NF2_PUBLISH_CREDIT_PAYMENT_INFOValue:
0x00001000
EMBER_AF_METERING_NF2_PUBLISH_CPP_EVENT#
#define EMBER_AF_METERING_NF2_PUBLISH_CPP_EVENTValue:
0x00002000
EMBER_AF_METERING_NF2_PUBLISH_TIER_LABELS#
#define EMBER_AF_METERING_NF2_PUBLISH_TIER_LABELSValue:
0x00004000
EMBER_AF_METERING_NF3_PUBLISH_CALENDAR#
#define EMBER_AF_METERING_NF3_PUBLISH_CALENDARValue:
0x00000001
EMBER_AF_METERING_NF3_PUBLISH_SPECIAL_DAYS#
#define EMBER_AF_METERING_NF3_PUBLISH_SPECIAL_DAYSValue:
0x00000002
EMBER_AF_METERING_NF4_SELECT_AVAILABLE_EMERGENCY_CREDIT#
#define EMBER_AF_METERING_NF4_SELECT_AVAILABLE_EMERGENCY_CREDITValue:
0x00000001
EMBER_AF_METERING_NF4_EMERGENCY_CREDIT_SETUP#
#define EMBER_AF_METERING_NF4_EMERGENCY_CREDIT_SETUPValue:
0x00000004
EMBER_AF_METERING_NF4_CREDIT_ADJUSTMENT#
#define EMBER_AF_METERING_NF4_CREDIT_ADJUSTMENTValue:
0x00000010
EMBER_AF_METERING_NF4_CHANGE_PAYMENT_MODE#
#define EMBER_AF_METERING_NF4_CHANGE_PAYMENT_MODEValue:
0x00000020
EMBER_AF_METERING_NF4_GET_PREPAY_SNAPSHOT#
#define EMBER_AF_METERING_NF4_GET_PREPAY_SNAPSHOTValue:
0x00000040
EMBER_AF_METERING_NF4_SET_LOW_CREDIT_WARNING_LEVEL#
#define EMBER_AF_METERING_NF4_SET_LOW_CREDIT_WARNING_LEVELValue:
0x00000100
EMBER_AF_METERING_NF4_GET_DEBT_REPAYMENT_LOG#
#define EMBER_AF_METERING_NF4_GET_DEBT_REPAYMENT_LOGValue:
0x00000200
EMBER_AF_METERING_NF4_SET_MAXIMUM_CREDIT_LIMIT#
#define EMBER_AF_METERING_NF4_SET_MAXIMUM_CREDIT_LIMITValue:
0x00000400
EMBER_AF_METERING_NF4_SET_OVERALL_DEBT_CAP#
#define EMBER_AF_METERING_NF4_SET_OVERALL_DEBT_CAPValue:
0x00000800
EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_TENANCY#
#define EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_TENANCYValue:
0x00000001
EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_SUPPLIER#
#define EMBER_AF_METERING_NF5_PUBLISH_CHANGE_OF_SUPPLIERValue:
0x00000002
EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_1_RESPONSE#
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_1_RESPONSEValue:
0x00000004
EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_2_RESPONSE#
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_2_RESPONSEValue:
0x00000008
EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_3_RESPONSE#
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_3_RESPONSEValue:
0x00000010
EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_4_RESPONSE#
#define EMBER_AF_METERING_NF5_REQUEST_NEW_PASSWORD_4_RESPONSEValue:
0x00000020
EMBER_AF_METERING_NF5_RESET_BATTERY_COUNTER#
#define EMBER_AF_METERING_NF5_RESET_BATTERY_COUNTERValue:
0x00000080
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTH#
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_NAME_LENGTHValue:
(16)
Device Management plugin types.
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTH#
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PROPOSED_PROVIDER_CONTACT_DETAILS_LENGTHValue:
(18)
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTH#
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_SITE_ID_LENGTHValue:
(32)
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTH#
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_CIN_LENGTHValue:
(24)
EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTH#
#define EMBER_AF_DEVICE_MANAGEMENT_MAXIMUM_PASSWORD_LENGTHValue:
(10)
EMBER_AF_ZDO_RESPONSE_OVERHEAD#
#define EMBER_AF_ZDO_RESPONSE_OVERHEADValue:
2
The overhead of the ZDO response. 1 byte for the sequence and 1 byte for the status code.
Enumeration Documentation#
EmberAfSecurityProfile#
EmberAfSecurityProfile
| Enumerator | |
|---|---|
| EMBER_AF_SECURITY_PROFILE_NONE | |
| EMBER_AF_SECURITY_PROFILE_HA | |
| EMBER_AF_SECURITY_PROFILE_HA12 | |
| EMBER_AF_SECURITY_PROFILE_SE_TEST | |
| EMBER_AF_SECURITY_PROFILE_SE_FULL | |
| EMBER_AF_SECURITY_PROFILE_Z3 | |
| EMBER_AF_SECURITY_PROFILE_CUSTOM | |
EmberAfServiceDiscoveryStatus#
EmberAfServiceDiscoveryStatus
This is an enum used to indicate the result of the service discovery. Unicast discoveries are completed as soon as a response is received. Broadcast discoveries wait a period of time for multiple responses to be received.
| Enumerator | |
|---|---|
| EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE | |
| EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED | |
| EMBER_AF_UNICAST_SERVICE_DISCOVERY_TIMEOUT | |
| EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE | |
| EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE | |
| EMBER_AF_UNICAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE | |
| EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE | |
EmberAfEventPollControl#
EmberAfEventPollControl
This is an enum used to control how the device will poll for a given active cluster-related event. When the event is scheduled, the application can pass a poll control value which will be stored along with the event. The processor is only allowed to poll according to the most restrictive value for all active event. For instance, if two events are active, one with EMBER_AF_LONG_POLL and the other with EMBER_AF_SHORT_POLL, then the processor will short poll until the second event is deactivated.
| Enumerator | |
|---|---|
| EMBER_AF_LONG_POLL | |
| EMBER_AF_SHORT_POLL | |
EmberAfEventSleepControl#
EmberAfEventSleepControl
This is an enum used to control how the device will sleep for a given active cluster related event. When the event is scheduled, the scheduling code can pass a sleep control value which will be stored along with the event. The processor is only allowed to sleep according to the most restrictive sleep control value for any active event. For instance, if two events are active, one with EMBER_AF_OK_TO_HIBERNATE and the other with EMBER_AF_OK_TO_NAP, then the processor will only be allowed to nap until the second event is deactivated.
| Enumerator | |
|---|---|
| EMBER_AF_OK_TO_SLEEP | |
| EMBER_AF_OK_TO_HIBERNATE | Deprecated |
| EMBER_AF_OK_TO_NAP | Deprecated |
| EMBER_AF_STAY_AWAKE | |
| EMBER_AF_OK_TO_SLEEP | |
| EMBER_AF_OK_TO_HIBERNATE | Deprecated |
| EMBER_AF_OK_TO_NAP | Deprecated |
| EMBER_AF_STAY_AWAKE | |
EmberAfApplicationTask#
EmberAfApplicationTask
An enum used to track the tasks that the Application framework cares about. These are intended to be tasks that should keep the device out of hibernation like an application level request / response. If the response does not come in as a data ack, then the application will need to stay out of hibernation to wait and poll for it.
Of course some tasks do not necessarily have a response. For instance, a ZDO request may or may not have a response. In this case, the application framework cannot rely on the fact that a response will come in to end the wake cycle, so the Application framework must timeout the wake cycle if no expected response is received or no other event can be relied upon to end the wake cycle.
Tasks of this type should be added to the wake timeout mask by calling emberAfSetWakeTimeoutBitmaskCallback so that they can be governed by a timeout instead of a request / response
the current tasks bitmask is an uint32_t bitmask used to track which tasks are active at any given time. The bottom 16 bits, values 0x01 - 0x8000 are reserved for Ember's use. The top 16 bits are reserved for the customer, values 0x10000 - 0x80000000
| Enumerator | |
|---|---|
| EMBER_AF_WAITING_FOR_DATA_ACK | |
| EMBER_AF_LAST_POLL_GOT_DATA | |
| EMBER_AF_WAITING_FOR_SERVICE_DISCOVERY | |
| EMBER_AF_WAITING_FOR_ZDO_RESPONSE | |
| EMBER_AF_WAITING_FOR_ZCL_RESPONSE | |
| EMBER_AF_WAITING_FOR_REGISTRATION | |
| EMBER_AF_WAITING_FOR_PARTNER_LINK_KEY_EXCHANGE | |
| EMBER_AF_FORCE_SHORT_POLL | |
| EMBER_AF_FRAGMENTATION_IN_PROGRESS | |
| EMBER_AF_FORCE_SHORT_POLL_FOR_PARENT_CONNECTIVITY | |
| EMBER_AF_WAITING_FOR_TC_KEY_UPDATE | |
EmberAfPluginPriceCppAuth#
EmberAfPluginPriceCppAuth
Specifies CPP Authorization values.
| Enumerator | |
|---|---|
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_PENDING | |
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_ACCEPTED | |
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_REJECTED | |
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_FORCED | |
| EMBER_AF_PLUGIN_PRICE_CPP_AUTH_RESERVED | |
EmberAfPluginTunnelingClientStatus#
EmberAfPluginTunnelingClientStatus
| Enumerator | |
|---|---|
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_SUCCESS | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_BUSY | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_NO_MORE_TUNNEL_IDS | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_PROTOCOL_NOT_SUPPORTED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_FLOW_CONTROL_NOT_SUPPORTED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_REQUEST_FAILED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_IEEE_ADDRESS_NOT_FOUND | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_ADDRESS_TABLE_FULL | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_REQUEST_FAILED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_LINK_KEY_EXCHANGE_FAILED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_FAILED | |
| EMBER_AF_PLUGIN_TUNNELING_CLIENT_REQUEST_TUNNEL_TIMEOUT | |
@0#
@0
The list of options possible for the image block request/response.
| Enumerator | |
|---|---|
| EMBER_AF_IMAGE_BLOCK_REQUEST_OPTIONS_NONE | |
| EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_CLIENT | |
| EMBER_AF_IMAGE_BLOCK_REQUEST_MIN_BLOCK_REQUEST_SUPPORTED_BY_SERVER | |
| EMBER_AF_IMAGE_BLOCK_REQUEST_SIMULATED_FROM_PAGE_REQUEST | |
| EMBER_AF_DATA_TYPE_ANALOG | |
| EMBER_AF_DATA_TYPE_DISCRETE | |
| EMBER_AF_DATA_TYPE_NONE | |
| PRIORITIZE_BEACONS_BASED_ON_PARENT_CLASSIFICATION | |
| PRIORITIZE_BEACONS_BASED_ON_TC_CONNECTVITY | |
| TC_CONNECTIVITY | |
| LONG_UPTIME | |
| BAD_PARENT_CONNECTIVITY | |
EmberAfOtaStorageStatus#
EmberAfOtaStorageStatus
This status contains the success or error code of an OTA storage device operation.
| Enumerator | |
|---|---|
| EMBER_AF_OTA_STORAGE_SUCCESS | |
| EMBER_AF_OTA_STORAGE_ERROR | |
| EMBER_AF_OTA_STORAGE_RETURN_DATA_TOO_LONG | |
| EMBER_AF_OTA_STORAGE_PARTIAL_FILE_FOUND | |
| EMBER_AF_OTA_STORAGE_OPERATION_IN_PROGRESS | |
@1#
@1
This status contains the success or error code of an OTA download operation.
| Enumerator | |
|---|---|
| EMBER_AF_OTA_DOWNLOAD_AND_VERIFY_SUCCESS | |
| EMBER_AF_OTA_DOWNLOAD_TIME_OUT | |
| EMBER_AF_OTA_VERIFY_FAILED | |
| EMBER_AF_OTA_SERVER_ABORTED | |
| EMBER_AF_OTA_CLIENT_ABORTED | |
| EMBER_AF_OTA_ERASE_FAILED | |
| EMBER_POLL_TIMEOUT_10_SECONDS | |
| EMBER_POLL_TIMEOUT_2_MINUTES | |
| EMBER_POLL_TIMEOUT_4_MINUTES | |
| EMBER_POLL_TIMEOUT_8_MINUTES | |
| EMBER_POLL_TIMEOUT_16_MINUTES | |
| EMBER_POLL_TIMEOUT_32_MINUTES | |
| EMBER_POLL_TIMEOUT_64_MINUTES | |
| EMBER_POLL_TIMEOUT_128_MINUTES | |
| EMBER_POLL_TIMEOUT_256_MINUTES | |
| EMBER_POLL_TIMEOUT_512_MINUTES | |
| EMBER_POLL_TIMEOUT_1024_MINUTES | |
| EMBER_POLL_TIMEOUT_2048_MINUTES | |
| EMBER_POLL_TIMEOUT_4096_MINUTES | |
| EMBER_POLL_TIMEOUT_8192_MINUTES | |
| EMBER_POLL_TIMEOUT_16384_MINUTES | |
EmberAfKeyEstablishmentNotifyMessage#
EmberAfKeyEstablishmentNotifyMessage
| Enumerator | |
|---|---|
| NO_APP_MESSAGE | |
| RECEIVED_PARTNER_CERTIFICATE | |
| GENERATING_EPHEMERAL_KEYS | |
| GENERATING_SHARED_SECRET | |
| KEY_GENERATION_DONE | |
| GENERATE_SHARED_SECRET_DONE | |
| LINK_KEY_ESTABLISHED | LINK_KEY_ESTABLISHED indicates Success, key establishment done. |
| NO_LOCAL_RESOURCES | Error codes: Transient failures where Key Establishment could be retried |
| PARTNER_NO_RESOURCES | |
| TIMEOUT_OCCURRED | |
| INVALID_APP_COMMAND | |
| MESSAGE_SEND_FAILURE | |
| PARTNER_SENT_TERMINATE | |
| INVALID_PARTNER_MESSAGE | |
| PARTNER_SENT_DEFAULT_RESPONSE_ERROR | |
| BAD_CERTIFICATE_ISSUER | Fatal Errors: These results are not worth retrying because the outcome will not change |
| KEY_CONFIRM_FAILURE | |
| BAD_KEY_ESTABLISHMENT_SUITE | |
| KEY_TABLE_FULL | |
| NO_ESTABLISHMENT_ALLOWED | Neither initiator nor responder is an ESP/TC so the key establishment is not allowed per the spec. |
| INVALID_CERTIFICATE_KEY_USAGE | |
EmberAfImageVerifyStatus#
EmberAfImageVerifyStatus
This enumeration is used to indicate the state of an OTA bootload image undergoing verification. This is used both for cryptographic verification and manufacturer specific verification.
| Enumerator | |
|---|---|
| EMBER_AF_IMAGE_GOOD | |
| EMBER_AF_IMAGE_BAD | |
| EMBER_AF_IMAGE_VERIFY_IN_PROGRESS | |
EmberAfCbkeKeyEstablishmentSuite#
EmberAfCbkeKeyEstablishmentSuite
CBKE Library types.
| Enumerator | |
|---|---|
| EMBER_AF_INVALID_KEY_ESTABLISHMENT_SUITE | |
| EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_163K1 | |
| EMBER_AF_CBKE_KEY_ESTABLISHMENT_SUITE_283K1 | |
EmberAfDeviceManagementPasswordType#
EmberAfDeviceManagementPasswordType
| Enumerator | |
|---|---|
| UNUSED_PASSWORD | |
| SERVICE_PASSWORD | |
| CONSUMER_PASSWORD | |
EmberAfDeviceManagementChangePendingFlags#
EmberAfDeviceManagementChangePendingFlags
| Enumerator | |
|---|---|
| EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_TENANCY_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_CHANGE_OF_SUPPLIER_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SITE_ID_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CIN_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_UPDATE_SERVICE_PASSWORD_PENDING_MASK | |
| EMBER_AF_DEVICE_MANAGEMENT_UPDATE_CONSUMER_PASSWORD_PENDING_MASK | |
EmberAfDeviceDiscoveryStatus#
EmberAfDeviceDiscoveryStatus
| Enumerator | |
|---|---|
| EMBER_AF_DEVICE_DISCOVERY_STATUS_NONE | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_NEW | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_ENDPOINTS | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_CLUSTERS | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_FIND_STACK_REVISION | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_DONE | |
| EMBER_AF_DEVICE_DISCOVERY_STATUS_FAILED | |
Typedef Documentation#
EmberAfProfileId#
typedef uint16_t EmberAfProfileId
Type for referring to zigbee application profile id.
EmberAfGenericClusterFunction#
typedef void(* EmberAfGenericClusterFunction) (void) )(void)
Generic function type, used for either of the cluster function.
This type is used for the array of the cluster functions, and should always be cast into one of the specific functions before being called.
EmberAfDifferenceType#
typedef uint32_t EmberAfDifferenceType
This type is used to compare two ZCL attribute values. The size of this data type depends on the platform.
EmberAfInterpanMessageType#
typedef uint8_t EmberAfInterpanMessageType
Interpan Message type: unicast, broadcast, or multicast.
EmberAfInterpanOptions#
typedef uint16_t EmberAfInterpanOptions
The options for sending/receiving interpan messages.
EmberAfAllowedInterpanOptions#
typedef uint8_t EmberAfAllowedInterpanOptions
The options for what interpan messages are allowed.
EmberAfPluginEsiManagementBitmask#
typedef uint8_t EmberAfPluginEsiManagementBitmask
Bitmask data type for storing one bit of information for each ESI in the ESI table.
EmberAfServiceDiscoveryCallback#
typedef void() EmberAfServiceDiscoveryCallback(const EmberAfServiceDiscoveryResult *result) (const EmberAfServiceDiscoveryResult *result)
This defines a callback where a code element or cluster can be informed as to the result of a service discovery they have requested. For each match, the callback is fired with all the resulting matches from that source. If the discovery was unicast to a specific device, then the callback will only be fired once with either MATCH_FOUND or COMPLETE (no matches found). If the discovery is broadcast then multiple callbacks may be fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_RESPONSE_RECEIVED. After a couple seconds the callback will then be fired with EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_RESPONSE or EMBER_AF_BROADCAST_SERVICE_DISCOVERY_COMPLETE_WITH_EMPTY_RESPONSE as the result.
EmberAfPartnerLinkKeyExchangeCallback#
typedef void() EmberAfPartnerLinkKeyExchangeCallback(bool success) (bool success)
This defines a callback where a code element or cluster can be informed as to the result of a request to initiate a partner link key exchange. The callback will be triggered with success equal to true if the exchange completed successfully.
EmberAfNetworkEventHandler#
typedef void(* EmberAfNetworkEventHandler) (void) )(void)
Type for referring to the handler for network events.
EmberAfEndpointEventHandler#
typedef void(* EmberAfEndpointEventHandler) (uint8_t endpoint) )(uint8_t endpoint)
Type for referring to the handler for endpoint events.
EmberAfTickFunction#
typedef void(* EmberAfTickFunction) (uint8_t endpoint) )(uint8_t endpoint)
Type for referring to the tick callback for cluster.
Tick function will be called once for each tick for each endpoint in the cluster. The rate of tick is determined by the metadata of the cluster.
EmberAfInitFunction#
typedef void(* EmberAfInitFunction) (uint8_t endpoint) )(uint8_t endpoint)
Type for referring to the init callback for cluster.
Init function is called when the application starts up, once for each cluster/endpoint combination.
EmberAfClusterAttributeChangedCallback#
typedef void(* EmberAfClusterAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId) )(uint8_t endpoint, EmberAfAttributeId attributeId)
Type for referring to the attribute changed callback function.
This function is called just after an attribute changes.
EmberAfManufacturerSpecificClusterAttributeChangedCallback#
typedef void(* EmberAfManufacturerSpecificClusterAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId, uint16_t manufacturerCode) )(uint8_t endpoint, EmberAfAttributeId attributeId, uint16_t manufacturerCode)
Type for referring to the manufacturer specific attribute changed callback function.
This function is called just after a manufacturer specific attribute changes.
EmberAfClusterPreAttributeChangedCallback#
typedef EmberAfStatus(* EmberAfClusterPreAttributeChangedCallback) (uint8_t endpoint, EmberAfAttributeId attributeId, EmberAfAttributeType attributeType, uint8_t size, uint8_t *value) )(uint8_t endpoint, EmberAfAttributeId attributeId, EmberAfAttributeType attributeType, uint8_t size, uint8_t *value)
Type for referring to the pre-attribute changed callback function.
This function is called before an attribute changes.
EmberAfDefaultResponseFunction#
typedef void(* EmberAfDefaultResponseFunction) (uint8_t endpoint, uint8_t commandId, EmberAfStatus status) )(uint8_t endpoint, uint8_t commandId, EmberAfStatus status)
Type for referring to the default response callback function.
This function is called when default response is received, before the global callback. Global callback is called immediately afterwards.
EmberAfMessageSentFunction#
typedef void(* EmberAfMessageSentFunction) (EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, uint16_t msgLen, uint8_t *message, EmberStatus status) )(EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, uint16_t msgLen, uint8_t *message, EmberStatus status)
Type for referring to the message sent callback function.
This function is called when a message is sent.
EmberAfRemoteClusterType#
typedef uint16_t EmberAfRemoteClusterType
Zigbee Internet Client/Server Remote Cluster Types.