Battery Monitor Callbacks#
These callbacks are contributed by the Battery Monitor plugin.
Functions#
void
emberAfPluginBatteryMonitorDataReadyCallback(uint16_t batteryVoltageMilliV)
Data Ready.
Function Documentation#
emberAfPluginBatteryMonitorDataReadyCallback#
void emberAfPluginBatteryMonitorDataReadyCallback (uint16_t batteryVoltageMilliV)
Data Ready.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | batteryVoltageMilliV | The battery voltage, in milli Volts Ver.: always |
This function is called whenever the battery monitor has generated a new valid battery level.