Multiple RAIL Demo Code Callbacks#
These callbacks are contributed by the Multiple RAIL Demo Code plugin.
Functions#
void
emberAfPluginMultirailDemoRailEventCallback(RAIL_Handle_t handle, RAIL_Events_t events)
A callback called whenever a secondary instance RAIL event occurs.
Function Documentation#
emberAfPluginMultirailDemoRailEventCallback#
void emberAfPluginMultirailDemoRailEventCallback (RAIL_Handle_t handle, RAIL_Events_t events)
A callback called whenever a secondary instance RAIL event occurs.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | handle | A handle for a RAIL instance. |
| RAIL_Events_t | [in] | events | A bit mask of RAIL events (full list in rail_types.h) |