Microphone Codec MSADPCM Callbacks#
These callbacks are contributed by the Microphone Codec MSADPCM plugin.
Functions#
void
halMicrophoneCodecMsadpcmDataReadyCallback(uint8_t *data, uint8_t length)
Called when new microphone data is ready.
Function Documentation#
halMicrophoneCodecMsadpcmDataReadyCallback#
void halMicrophoneCodecMsadpcmDataReadyCallback (uint8_t * data, uint8_t length)
Called when new microphone data is ready.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | data | Pointer to the data that is ready. |
| uint8_t | N/A | length | Length of the data. |
@appusage This function is called by the plugin when new data has been processed and is ready to be processed by other parts of the system.