Modules#
Stack Information#
See stack-info.h for source code.
See also config.h.
This documentation was produced from the following software release and build.
SOFTWARE_VERSION | 0x4700 | High byte = release number, low byte = patch number |
|---|
This file provides definitions relevant to libraries. A running image may probe information about included libraries using the APIs defined in this section.
See library.h for more information.
Radio-specific Functions#
Enable boost power mode and/or the alternate transmit path.
Return the current configuration of boost power mode and alternate transmitter output.
Set the short node ID of the node. Notice that it can only be set if the stack is in the INITAL state.
Return the number of PHY interfaces present.
The radio calibration callback function.
Calibrate the current channel. The stack will notify the application of the need for channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Calibration can take up to 150 ms. Note if this function is called when the radio is off, it will turn the radio on and leave it on.
Set the device uptime to be long or short the uptime is then advertised in the beacons.
Set the hub connectivity to be true or false the hub connectivity is then advertised in the beacons.
Get the current scheduler priorities used for Zigbee multiprotocol operations.
Set the current scheduler priorities used for Zigbee multiprotocol operations.
Set the multiprotocol slip time.
Get the multiprotocol slip time.
Get current beacon classification parameter settings.
Set current beacon classification parameters.
Set the route record policy.
Get the route record policy.
Variables#
The application must provide a definition for this variable.
The application must provide a definition for this variable.
If emberEndpointCount is nonzero, the application must provide descriptions for each endpoint.
Functions#
A callback invoked when the status of the stack changes. If the status parameter equals EMBER_NETWORK_UP, the emberGetNetworkParameters() function can be called to get the new network parameters. If any of the parameters are stored in nonvolatile memory by the application, the stored values should be updated.
Return the current join status.
Indicate whether the stack is currently up.
Write node data to the stack token.
Check when the next stack event is scheduled to run.
Set the power descriptor to the specified value. The power descriptor is a dynamic value, therefore this function should be called whenever the value changes.
Return the EUI64 ID of the local node.
Determine whether eui64 is the local node's EUI64 ID.
Return the 16-bit node ID of local node on the current logical network.
Return the 16-bit node ID of local node on the network it is currently tuned on.
Set the manufacturer code to the specified value. The manufacturer code is one of the fields of the node descriptor.
Set the maximum incoming transfer size to the specified value. The maximum incoming transfer size is one of the fields of the node descriptor.
Set the maximum outgoing transfer size to the specified value. The maximum outgoing transfer size is one of the fields of the node descriptor.
Set the descriptor capability field of the node.
Copy the current network parameters into the structure provided by the caller.
Copy the current radio parameters into the structure provided by the caller.
Copy the current node type into the location provided by the caller.
Set the channel to use for sending and receiving messages on the current logical network. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
Set the current logical and physical channel.
Get the radio channel to which a node is set on the current logical network. The possible return values depend on the radio in use. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
Set the radio output power at which a node is to operate for the current logical network. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit. Note that using this API on a running network will directly impact the established link qualities which the neighboring nodes have with the node on which it is called. This can lead to disruption of existing routes and erratic network behavior. Note that, if the requested power level is not available on a given radio, this function will use the next higher available power level.
Get the radio output power of the current logical network at which a node is operating. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit.
Return the RAIL level handle required to make RAIL API calls. Will return NULL if RAIL is not in use.
Return the local node's PAN ID of the current logical network.
Return the local node's PAN ID of the current radio network.
Set the configured 802.15.4 CCA mode in the radio. For a list of CCA modes, please refer to RAIL documentation regarding RAIL_IEEE802154_CcaMode_t.
Fetch a node's 8 byte Extended PAN identifier. If this is called when a device is not currently on a network (see emberNetworkState), the Extended PAN ID returned will be an invalid value.
Retrieve the endpoint number for the index'th endpoint. index must be less than the value of emberEndpointCount.
Retrieve the endpoint description for the given endpoint.
Retrieve a cluster ID from one of the cluster lists associated with the given endpoint.
Determine whether nodeId is valid.
Return the node ID that corresponds to the specified EUI64. The node ID is found by searching through all stack tables for the specified EUI64.
Return the EUI64 that corresponds to the specified node ID. The EUI64 is found by searching through all stack tables for the specified node ID.
A callback invoked to inform the application of the occurrence of an event defined by EmberCounterType, for example, transmissions and receptions at different layers of the stack.
A callback invoked to inform the application that a stack token has changed.
A callback to allow the application to manage idling the MCU.
A callback to request the application to wake up the stack task.
Copy a neighbor table entry to the structure that result points to. Neighbor table entries are stored in ascending order by node ID, with all unused entries at the end of the table. The number of active neighbors can be obtained using emberNeighborCount().
Set the routing shortcut threshold to directly use a neighbor instead of performing routing.
Get the routing shortcut threshold used to separate between directly using a neighbor vs. performing routing.
Set neighbor's initial outgoing link cost.
Get neighbor's initial outgoing link cost.
Indicate whether a rejoining neighbor's incoming FC should be reset.
Check whether resetting the incoming FC for a rejoining neighbor is enabled.
Get the last received frame counter as found in the Network Auxiliary header for the specified neighbor or child.
Sets the frame counter for the specified neighbor or child.
Copy a route table entry to the structure that the result points to. Unused route table entries have a destination of 0xFFFF. The route table size can be obtained via emberRouteTableSize().
Return the stack profile of the network which the node has joined.
Return the security level of the network which the node has joined.
Return the depth of the node in the network.
Return the number of active entries in the neighbor table.
Return the size of the route table.
Increment and returns the Zigbee sequence number.
Get maximum number of NWK retries.
This indicates the presence, absence, or status of an Ember stack library.
Macros#
Software version. High byte = release number, low byte = patch number.
Radio-specific Functions Documentation#
emberSetTxPowerMode#
EmberStatus emberSetTxPowerMode (uint16_t txPowerMode)
Enable boost power mode and/or the alternate transmit path.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | txPowerMode | Specifies which transmit power mode options should be activated. This parameter should be set to one of the literal values described in stack/include/ember-types.h. Any power option not specified in the txPowerMode parameter will be deactivated. |
Boost power mode is a high-performance radio mode, which offers increased transmit power and receive sensitivity at the cost of an increase in power consumption. emberInit() calls this function using the power mode and transmitter output settings as specified in the MFG_PHY_CONFIG token (with each bit inverted so that the default token value of 0xffff corresponds to normal power mode and bi-directional RF transmitter output). The application only needs to call emberSetTxPowerMode() to use a power mode or transmitter output setting different than specified in the MFG_PHY_CONFIG token. After the initial call to emberSetTxPowerMode(), the stack will automatically maintain the specified power mode configuration across sleep/wake cycles.
Returns
EMBER_SUCCESS if successful; an error code otherwise.
emberGetTxPowerMode#
uint16_t emberGetTxPowerMode (void )
Return the current configuration of boost power mode and alternate transmitter output.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current TX power mode.
emberSetNodeId#
EmberStatus emberSetNodeId (EmberNodeId nodeId)
Set the short node ID of the node. Notice that it can only be set if the stack is in the INITAL state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | nodeId | Specifies the short ID to be assigned to the node. |
Returns
EMBER_SUCCESS if successful; an error code otherwise.
emberGetPhyInterfaceCount#
uint8_t emberGetPhyInterfaceCount (void )
Return the number of PHY interfaces present.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The number of PHY interface(s).
emberRadioNeedsCalibratingHandler#
void emberRadioNeedsCalibratingHandler (void )
The radio calibration callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
The Voltage Controlled Oscillator (VCO) can drift with temperature changes. During every call to emberTick(), the stack will check to see if the VCO has drifted. If the VCO has drifted, the stack will call emberRadioNeedsCalibratingHandler() to inform the application that it should perform calibration of the current channel as soon as possible. Calibration can take up to 150 ms. The default callback function implementation provided here performs the calibration immediately. The application can define its own callback by defining ::EMBER_APPLICATION_HAS_CUSTOM_RADIO_CALIBRATION_CALLBACK in its CONFIGURATION_HEADER. It can then failsafe any critical processes or peripherals before calling ::emberCalibrateCurrentChannel(). The application must call ::emberCalibrateCurrentChannel() in response to this callback to maintain expected radio performance.
sl_mac_calibrate_current_channel#
void sl_mac_calibrate_current_channel (void )
Calibrate the current channel. The stack will notify the application of the need for channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick(). This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Calibration can take up to 150 ms. Note if this function is called when the radio is off, it will turn the radio on and leave it on.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emberSetLongUpTime#
void emberSetLongUpTime (bool hasLongUpTime)
Set the device uptime to be long or short the uptime is then advertised in the beacons.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | hasLongUpTime |
emberSetHubConnectivity#
void emberSetHubConnectivity (bool connected)
Set the hub connectivity to be true or false the hub connectivity is then advertised in the beacons.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | connected |
emberIsUpTimeLong#
bool emberIsUpTimeLong (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
True if device uptime is long, false otherwise
emberIsHubConnected#
bool emberIsHubConnected (void )
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
True if there is hub connectivity, false otherwise
emberRadioGetSchedulerPriorities#
EmberStatus emberRadioGetSchedulerPriorities (EmberMultiprotocolPriorities * priorities)
Get the current scheduler priorities used for Zigbee multiprotocol operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberMultiprotocolPriorities * | N/A | priorities | A pointer to a structure to store the current priorities in. This must not be NULL. |
Returns
EMBER_SUCCESS if called in a multiprotocol app and EMBER_INVALID_CALL otherwise.
For more details on what these priorities are and how to use them see UG305, the Dynamic Multiprotocol User Guide.
emberRadioSetSchedulerPriorities#
EmberStatus emberRadioSetSchedulerPriorities (const EmberMultiprotocolPriorities * priorities)
Set the current scheduler priorities used for Zigbee multiprotocol operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const EmberMultiprotocolPriorities * | N/A | priorities | A pointer to a structure of the new priorities to use. This must not be NULL. |
Returns
EMBER_SUCCESS if called in a multiprotocol app and EMBER_INVALID_CALL otherwise.
For more details on what these priorities are and how to use them see UG305, the Dynamic Multiprotocol User Guide.
emberRadioSetSchedulerSliptime#
EmberStatus emberRadioSetSchedulerSliptime (uint32_t slipTime)
Set the multiprotocol slip time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | slipTime | The value to set the slip time to for each transmit. |
Returns
EMBER_SUCCESS if called in a multiprotocol app and EMBER_INVALID_CALL otherwise.
Use this to update the slip time passed to the radio scheduler for each transmit from the PHY layer. The smaller this is set the lower the potential multi-protocol induced latency is, but it makes packets more likely to fail to be transmitted. For more details on slip time see UG305.
emberRadioGetSchedulerSliptime#
EmberStatus emberRadioGetSchedulerSliptime (uint32_t * slipTime)
Get the multiprotocol slip time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | N/A | slipTime | A pointer to the place to store the current slip time |
Returns
EMBER_SUCCESS if called in a multiprotocol app and EMBER_INVALID_CALL otherwise.
Use this to get the current value of the multiprotocol slip time used for each transmit at the PHY layer. For more details on slip time see UG305.
emberGetBeaconClassificationParams#
EmberStatus emberGetBeaconClassificationParams (EmberBeaconClassificationParams * param)
Get current beacon classification parameter settings.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberBeaconClassificationParams * | N/A | param |
emberSetBeaconClassificationParams#
EmberStatus emberSetBeaconClassificationParams (EmberBeaconClassificationParams * param)
Set current beacon classification parameters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberBeaconClassificationParams * | N/A | param |
slx_zigbee_routing_set_route_record_policy#
EmberStatus slx_zigbee_routing_set_route_record_policy (sl_zigbee_route_record_policy_type_t policy)
Set the route record policy.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_zigbee_route_record_policy_type_t | N/A | policy | A pointer to the place to store the current slip time |
Returns
EMBER_SUCCESS if route record policy was sucessfully set EMBER_BAD_ARGUMENT otherwise.
Use this to set the policy for senidng a route record message to a concentrator Note that policies other than the default ROUTE_RECORD_POLICY_ACK_BY_SOURCE_ROUTED_MESSAGE may result in behaviour not compliant with the Zigbee specification
slx_zigbee_routing_get_route_record_policy#
uint8_t slx_zigbee_routing_get_route_record_policy (void )
Get the route record policy.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The route record policy
Use this to get the current value of the route record policy
Variable Documentation#
emberStackProfileId#
const uint8_t emberStackProfileId[]
The application must provide a definition for this variable.
profileId#
uint16_t EmberEndpointDescription::profileId
Identifies the endpoint's application profile.
deviceId#
uint16_t EmberEndpointDescription::deviceId
The endpoint's device ID within the application profile.
outputClusterCount#
uint8_t EmberEndpointDescription::outputClusterCount
The number of output clusters.
inputClusterList#
uint16_t const* EmberEndpoint::inputClusterList
Input clusters the endpoint will accept.
outputClusterList#
uint16_t const* EmberEndpoint::outputClusterList
Output clusters the endpoint may send.
emberEndpointCount#
uint8_t emberEndpointCount
The application must provide a definition for this variable.
emberEndpoints#
EmberEndpoint emberEndpoints[]
If emberEndpointCount is nonzero, the application must provide descriptions for each endpoint.
This can be done either by providing a definition of emberEndpoints or by providing definitions of emberGetEndpoint(), emberGetEndpointDescription() and emberGetEndpointCluster(). Using the array is often simpler, but consumes large amounts of memory if emberEndpointCount is large.
If the application provides definitions for the three functions, it must define EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
Function Documentation#
emberStackStatusHandler#
void emberStackStatusHandler (EmberStatus status)
A callback invoked when the status of the stack changes. If the status parameter equals EMBER_NETWORK_UP, the emberGetNetworkParameters() function can be called to get the new network parameters. If any of the parameters are stored in nonvolatile memory by the application, the stored values should be updated.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberStatus | N/A | status | Stack status. One of the following: |
The application is free to begin messaging after it receives the EMBER_NETWORK_UP status. However, routes discovered immediately after the stack comes up may be suboptimal because the routes are based on the neighbor table's information about two-way links with neighboring nodes, which is obtained from periodic ZigBee Link Status messages. It can take two or three link status exchange periods (of 16 seconds each) before the neighbor table has a good estimate of link quality to neighboring nodes. Therefore, the application may improve the quality of initially discovered routes by waiting after startup to give the neighbor table time to be populated.
emberNetworkState#
EmberNetworkStatus emberNetworkState (void )
Return the current join status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns a value indicating whether the node is joining, joined to, or leaving a network.
Returns
An EmberNetworkStatus value indicating the current join status.
emberStackIsUp#
bool emberStackIsUp (void )
Indicate whether the stack is currently up.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns true if the stack is joined to a network and ready to send and receive messages. This reflects only the state of the local node; it does not indicate whether other nodes are able to communicate with this node.
Returns
True if the stack is up, false otherwise.
emberWriteNodeData#
EmberStatus emberWriteNodeData (bool erase)
Write node data to the stack token.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | erase | Indicates whether the node type should be erased. |
Returns
The status of the operation and an error code if unsuccessful.
emberMsToNextStackEvent#
uint32_t emberMsToNextStackEvent (void )
Check when the next stack event is scheduled to run.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Returns the number of milliseconds before the next stack event is scheduled to run.
emberSetPowerDescriptor#
void emberSetPowerDescriptor (uint16_t descriptor)
Set the power descriptor to the specified value. The power descriptor is a dynamic value, therefore this function should be called whenever the value changes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | descriptor | The new power descriptor for the local node. |
emberGetEui64#
EmberEUI64 emberGetEui64 (void )
Return the EUI64 ID of the local node.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The 64-bit ID.
emberIsLocalEui64#
bool emberIsLocalEui64 (EmberEUI64 eui64)
Determine whether eui64 is the local node's EUI64 ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | eui64 | An EUI64 ID. |
Returns
True if
eui64is the local node's ID, otherwise false.
emberGetNodeId#
EmberNodeId emberGetNodeId (void )
Return the 16-bit node ID of local node on the current logical network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The 16-bit ID.
emberRadioGetNodeId#
EmberNodeId emberRadioGetNodeId (void )
Return the 16-bit node ID of local node on the network it is currently tuned on.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The 16-bit ID.
emberSetManufacturerCode#
void emberSetManufacturerCode (uint16_t code)
Set the manufacturer code to the specified value. The manufacturer code is one of the fields of the node descriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | code | The manufacturer code for the local node. |
emberSetMaximumIncomingTransferSize#
void emberSetMaximumIncomingTransferSize (uint16_t size)
Set the maximum incoming transfer size to the specified value. The maximum incoming transfer size is one of the fields of the node descriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | size | The maximum incoming transfer size for the local node. |
emberSetMaximumOutgoingTransferSize#
void emberSetMaximumOutgoingTransferSize (uint16_t size)
Set the maximum outgoing transfer size to the specified value. The maximum outgoing transfer size is one of the fields of the node descriptor.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | size | The maximum outgoing transfer size for the local node. |
emberSetDescriptorCapability#
void emberSetDescriptorCapability (uint8_t capability)
Set the descriptor capability field of the node.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | capability | The descriptor capability of the local node. |
emberGetNetworkParameters#
EmberStatus emberGetNetworkParameters (EmberNetworkParameters * parameters)
Copy the current network parameters into the structure provided by the caller.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNetworkParameters * | N/A | parameters | A pointer to an EmberNetworkParameters value into which the current network parameters will be copied. |
Returns
An EmberStatus value indicating the success or failure of the command.
emberGetRadioParameters#
EmberStatus emberGetRadioParameters (uint8_t phyIndex, EmberMultiPhyRadioParameters * parameters)
Copy the current radio parameters into the structure provided by the caller.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | phyIndex | The index of the PHY interface for radio parameters.
|
| EmberMultiPhyRadioParameters * | N/A | parameters |
Returns
An EmberStatus value indicating the success or failure of the command.
emberGetNodeType#
EmberStatus emberGetNodeType (EmberNodeType * resultLocation)
Copy the current node type into the location provided by the caller.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeType * | N/A | resultLocation | A pointer to an EmberNodeType value into which the current node type will be copied. |
Returns
An EmberStatus value that indicates the success or failure of the command.
emberSetRadioChannel#
EmberStatus emberSetRadioChannel (uint8_t channel)
Set the channel to use for sending and receiving messages on the current logical network. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | channel | The desired radio channel. |
Note: When using this API, all devices on a network must use the same channel.
Returns
An EmberStatus value indicating the success or failure of the command.
emberSetLogicalAndRadioChannel#
EmberStatus emberSetLogicalAndRadioChannel (uint8_t channel)
Set the current logical and physical channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | channel |
emberGetRadioChannel#
uint8_t emberGetRadioChannel (void )
Get the radio channel to which a node is set on the current logical network. The possible return values depend on the radio in use. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current radio channel.
emberSetRadioPower#
EmberStatus emberSetRadioPower (int8_t power)
Set the radio output power at which a node is to operate for the current logical network. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit. Note that using this API on a running network will directly impact the established link qualities which the neighboring nodes have with the node on which it is called. This can lead to disruption of existing routes and erratic network behavior. Note that, if the requested power level is not available on a given radio, this function will use the next higher available power level.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int8_t | N/A | power | A desired radio output power, in dBm. |
Returns
An EmberStatus value indicating the success or failure of the command. Failure indicates that the requested power level is out of range.
emberGetRadioPower#
int8_t emberGetRadioPower (void )
Get the radio output power of the current logical network at which a node is operating. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current radio output power, in dBm.
emberGetRailHandle#
void* emberGetRailHandle (void )
Return the RAIL level handle required to make RAIL API calls. Will return NULL if RAIL is not in use.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A RAIL handle
emberGetPanId#
EmberPanId emberGetPanId (void )
Return the local node's PAN ID of the current logical network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A PAN ID.
emberRadioGetPanId#
EmberPanId emberRadioGetPanId (void )
Return the local node's PAN ID of the current radio network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A PAN ID.
emberSetRadioIeee802154CcaMode#
EmberStatus emberSetRadioIeee802154CcaMode (uint8_t ccaMode)
Set the configured 802.15.4 CCA mode in the radio. For a list of CCA modes, please refer to RAIL documentation regarding RAIL_IEEE802154_CcaMode_t.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | ccaMode | A RAIL_IEEE802154_CcaMode_t value |
Returns
EMBER_SUCCESS upon success, EMBER_ERR_FATAL otherwise.
Note
The default CCA mode for zigbee is RAIL_IEEE802154_CCA_MODE_RSSI.
As mentioned in the RAIL documentation, on platforms that don't support different CCA modes, a call to this function will do nothing.
emberGetExtendedPanId#
void emberGetExtendedPanId (uint8_t * resultLocation)
Fetch a node's 8 byte Extended PAN identifier. If this is called when a device is not currently on a network (see emberNetworkState), the Extended PAN ID returned will be an invalid value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | N/A | resultLocation |
emberGetEndpoint#
uint8_t emberGetEndpoint (uint8_t index)
Retrieve the endpoint number for the index'th endpoint. index must be less than the value of emberEndpointCount.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | The index of an endpoint (as distinct from its endpoint number). This must be less than the value of emberEndpointCount. |
This function is provided by the stack, using the data from emberEndpoints, unless the application defines EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
Returns
The endpoint number for the index'th endpoint.
emberGetEndpointDescription#
bool emberGetEndpointDescription (uint8_t endpoint, EmberEndpointDescription * result)
Retrieve the endpoint description for the given endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | The endpoint whose description is to be returned. |
| EmberEndpointDescription * | N/A | result | A pointer to the location to which to copy the endpoint description. |
This function is provided by the stack, using the data from emberEndpoints, unless the application defines ::EMBER_APPLICATION_HAS_GET_ENDPOINT in its ::CONFIGURATION_HEADER.
Returns
True if the description was copied to result, or false if the endpoint is not active.
emberGetEndpointCluster#
uint16_t emberGetEndpointCluster (uint8_t endpoint, EmberClusterListId listId, uint8_t listIndex)
Retrieve a cluster ID from one of the cluster lists associated with the given endpoint.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | endpoint | The endpoint from which the cluster ID is to be read. |
| EmberClusterListId | N/A | listId | The list from which the cluster ID is to be read. |
| uint8_t | N/A | listIndex | The index of the desired cluster ID in the list. This value must be less than the length of the list. The length can be found in the EmberEndpointDescription for this endpoint. |
This function is provided by the stack, using the data from emberEndpoints, unless the application defines ::EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
Returns
The cluster ID at position listIndex in the specified endpoint cluster list.
emberIsNodeIdValid#
bool emberIsNodeIdValid (EmberNodeId nodeId)
Determine whether nodeId is valid.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | nodeId | A node ID. |
Returns
True if
nodeIdis valid, false otherwise.
emberLookupNodeIdByEui64#
EmberNodeId emberLookupNodeIdByEui64 (EmberEUI64 eui64)
Return the node ID that corresponds to the specified EUI64. The node ID is found by searching through all stack tables for the specified EUI64.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | eui64 | The EUI64 of the node to look up. |
Returns
The short ID of the node or EMBER_NULL_NODE_ID if the short ID is not known.
emberLookupEui64ByNodeId#
EmberStatus emberLookupEui64ByNodeId (EmberNodeId nodeId, EmberEUI64 eui64Return)
Return the EUI64 that corresponds to the specified node ID. The EUI64 is found by searching through all stack tables for the specified node ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | nodeId | The short ID of the node to look up. |
| EmberEUI64 | N/A | eui64Return | The EUI64 of the node is copied here if it is known. |
Returns
An EmberStatus value:
EMBER_SUCCESS - eui64Return has been set to the EUI64 of the node.
EMBER_ERR_FATAL - The EUI64 of the node is not known.
emberCounterHandler#
void emberCounterHandler (EmberCounterType type, EmberCounterInfo info)
A callback invoked to inform the application of the occurrence of an event defined by EmberCounterType, for example, transmissions and receptions at different layers of the stack.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberCounterType | N/A | type | Type of the event. |
| EmberCounterInfo | N/A | info | could map to:
|
The application must define ::EMBER_APPLICATION_HAS_COUNTER_HANDLER in its CONFIGURATION_HEADER to use this. This function may be called in ISR context, so processing should be kept to a minimum.
emberCounterRequiresPhyIndex#
bool emberCounterRequiresPhyIndex (EmberCounterType type)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberCounterType | N/A | type |
emberCounterRequiresDestinationNodeId#
bool emberCounterRequiresDestinationNodeId (EmberCounterType type)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberCounterType | N/A | type |
emberStackTokenChangedHandler#
void emberStackTokenChangedHandler (uint16_t tokenAddress)
A callback invoked to inform the application that a stack token has changed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | tokenAddress | The address of the stack token that has changed. |
emberRtosIdleHandler#
bool emberRtosIdleHandler (uint32_t * idleTimeMs)
A callback to allow the application to manage idling the MCU.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | N/A | idleTimeMs | The time in millisecond the stack is allowed to idle. |
Returns
True if the application is managing idling the MCU, false otherwise. If this function returns false, the stack will manage idling the MCU.
emberRtosStackWakeupIsrHandler#
void emberRtosStackWakeupIsrHandler (void )
A callback to request the application to wake up the stack task.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emberGetNeighbor#
EmberStatus emberGetNeighbor (uint8_t index, EmberNeighborTableEntry * result)
Copy a neighbor table entry to the structure that result points to. Neighbor table entries are stored in ascending order by node ID, with all unused entries at the end of the table. The number of active neighbors can be obtained using emberNeighborCount().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | The index of a neighbor table entry. |
| EmberNeighborTableEntry * | N/A | result | A pointer to the location to which to copy the neighbor table entry. |
Returns
EMBER_ERR_FATAL if the index is greater or equal to the number of active neighbors, or if the device is an end device. Returns EMBER_SUCCESS otherwise.
emberSetRoutingShortcutThreshold#
EmberStatus emberSetRoutingShortcutThreshold (uint8_t costThresh)
Set the routing shortcut threshold to directly use a neighbor instead of performing routing.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | costThresh | the routing shortcut value that should be used to directly use a neighbor instead of performing routing. |
Returns
::return EMBER_BAD_ARGUMENT if the costThresh is not 1, 3, 5, 7 Returns EMBER_SUCCESS otherwise.
emberGetRoutingShortcutThreshold#
uint8_t emberGetRoutingShortcutThreshold (void )
Get the routing shortcut threshold used to separate between directly using a neighbor vs. performing routing.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
the routingShortcutThresh which takes one of the following values: 1, 3, 5, or 7.
emberSetInitialNeighborOutgoingCost#
EmberStatus emberSetInitialNeighborOutgoingCost (uint8_t cost)
Set neighbor's initial outgoing link cost.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | cost | The new default cost. |
Returns
EMBER_BAD_ARGUMENT if the cost is not any of 0, 1, 3, 5, or 7. Returns EMBER_SUCCESS otherwise NOTE: There is no EZSP version of this function yet.
emberGetInitialNeighborOutgoingCost#
uint8_t emberGetInitialNeighborOutgoingCost (void )
Get neighbor's initial outgoing link cost.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The default cost associated with new neighbor's outgoing links. NOTE: There is no EZSP version of this function yet.
emberResetRejoiningNeighborsFC#
void emberResetRejoiningNeighborsFC (bool reset)
Indicate whether a rejoining neighbor's incoming FC should be reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | reset | True or False. |
Returns
::void NOTE: There is no EZSP version of this function yet.
emberIsResetRejoiningNeighborsFCEnabled#
bool emberIsResetRejoiningNeighborsFCEnabled (void )
Check whether resetting the incoming FC for a rejoining neighbor is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
::True or False. NOTE: There is no EZSP version of this function yet.
emberGetNeighborFrameCounter#
EmberStatus emberGetNeighborFrameCounter (EmberEUI64 nodeEui64, uint32_t * returnFrameCounter)
Get the last received frame counter as found in the Network Auxiliary header for the specified neighbor or child.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | nodeEui64 | The neighbor or child EUI to search. |
| uint32_t * | N/A | returnFrameCounter | The frame counter variable to fill in. |
Returns
EmberStatus depending on whether the frame counter is found in the neighbor or child table.
emberSetNeighborFrameCounter#
EmberStatus emberSetNeighborFrameCounter (EmberEUI64 nodeEui64, uint32_t frameCounter)
Sets the frame counter for the specified neighbor or child.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberEUI64 | N/A | nodeEui64 | The neighbor or child EUI to search. |
| uint32_t | N/A | frameCounter | The frame counter to set. |
Returns
EmberStatus depending on whether the frame counter is set in the neighbor or child table.
emberGetRouteTableEntry#
EmberStatus emberGetRouteTableEntry (uint8_t index, EmberRouteTableEntry * result)
Copy a route table entry to the structure that the result points to. Unused route table entries have a destination of 0xFFFF. The route table size can be obtained via emberRouteTableSize().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | The index of a route table entry. |
| EmberRouteTableEntry * | N/A | result | A pointer to the location to which to copy the route table entry. |
Returns
EMBER_ERR_FATAL if the index is out of range or the device is an end device, and EMBER_SUCCESS otherwise.
emberStackProfile#
uint8_t emberStackProfile (void )
Return the stack profile of the network which the node has joined.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The stack profile.
emberSecurityLevel#
uint8_t emberSecurityLevel (void )
Return the security level of the network which the node has joined.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The security level.
emberTreeDepth#
uint8_t emberTreeDepth (void )
Return the depth of the node in the network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current depth.
emberNeighborCount#
uint8_t emberNeighborCount (void )
Return the number of active entries in the neighbor table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The number of active entries in the neighbor table.
emberRouteTableSize#
uint8_t emberRouteTableSize (void )
Return the size of the route table.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The size of the route table.
emberNextZigbeeSequenceNumber#
uint8_t emberNextZigbeeSequenceNumber (void )
Increment and returns the Zigbee sequence number.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The next Zigbee sequence number.
emberGetMaxNwkRetries#
uint8_t emberGetMaxNwkRetries (void )
Get maximum number of NWK retries.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns the maximum number of NWK retries that will be attempted
Returns
uint8_t Max NWK retries
emberGetLibraryStatus#
enum EmberLibraryStatus enum EmberLibraryId define EMBER_LIBRARY_NAMES EmberLibraryStatus emberGetLibraryStatus (EmberLibraryId libraryId)
This indicates the presence, absence, or status of an Ember stack library.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberLibraryId | N/A | libraryId |
An enumerated list of library identifiers.
This routine takes a library identifier and returns whether the library is enabled or not. See ::EmberLibraryStatus for return codes.
Macro Definition Documentation#
EMBER_FULL_VERSION#
#define EMBER_FULL_VERSIONValue:
SOFTWARE_VERSION#
#define SOFTWARE_VERSIONValue:
EMBER_FULL_VERSION
Software version. High byte = release number, low byte = patch number.