Stack Tokens#
These tokens are divided into three sections (the three main types of tokens mentioned in token.h):
manufacturing
stack
application
For a full explanation of the tokens, see hal/micro/token.h. See token-stack.h for source code.
A set of tokens is predefined in the APPLICATION DATA section at the end of token-stack.h because these tokens are required by the stack, but they are classified as application tokens since they are sized by the application via its CONFIGURATION_HEADER.
The user application can include its own tokens in a header file similar to this one. The macro ::APPLICATION_TOKEN_HEADER should be defined to equal the name of the header file in which application tokens are defined. See the APPLICATION DATA section at the end of token-stack.h for examples of token definitions.
Since token-stack.h contains both the typedefs and the token defs, two #defines are used to select which one is needed when this file is included. #define DEFINETYPES is used to select the type definitions and #define DEFINETOKENS is used to select the token definitions. See token.h and token.c to see how these are used.
Convenience Macros#
The following convenience macros are used to simplify the definition process for commonly specified parameters to the basic TOKEN_DEF macro. See hal/micro/token.h for a more complete explanation.
Creator Codes#
The CREATOR is used as a distinct identifier tag for the token.The CREATOR is necessary because the token name is defined differently depending on the hardware platform. Therefore, the CREATOR ensures that token definitions and data stay tagged and known. The only requirement is that each creator definition must be unique. See hal/micro/token.h for a more complete explanation.
NVM3 Object Keys#
The NVM3 object key is used as a distinct identifier tag for a token stored in NVM3.Every token must have a defined NVM3 object key and the object key must be unique. The object key defined must be in the following format: NVM3KEY_tokennamewhere tokenname is the name of the token without NVM3KEY_ or TOKEN_ prefix.
Macros#
By default, tokens are automatically located after the previous token.
The current version number of the stack tokens. MSB is the version, LSB is a complement.
Convenience Macros Documentation#
DEFINE_FIXED_BASIC_TOKEN#
#define DEFINE_FIXED_BASIC_TOKENValue:
DEFINE_FIXED_COUNTER_TOKEN#
#define DEFINE_FIXED_COUNTER_TOKENValue:
DEFINE_FIXED_INDEXED_TOKEN#
#define DEFINE_FIXED_INDEXED_TOKENValue:
DEFINE_MFG_TOKEN#
#define DEFINE_MFG_TOKENValue:
Creator Codes Documentation#
CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEY#
#define CREATOR_MULTI_NETWORK_STACK_ALTERNATE_KEYValue:
0xE212
CREATOR_MULTI_NETWORK_STACK_TRUST_CENTER#
#define CREATOR_MULTI_NETWORK_STACK_TRUST_CENTERValue:
0xE213
CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT#
#define CREATOR_MULTI_NETWORK_STACK_NETWORK_MANAGEMENTValue:
0xE214
CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTER#
#define CREATOR_MULTI_NETWORK_STACK_NONCE_COUNTERValue:
0xE220
CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO#
#define CREATOR_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFOValue:
0xE221
NVM3 Object Keys Documentation#
NVM3KEY_STACK_NVDATA_VERSION#
#define NVM3KEY_STACK_NVDATA_VERSIONValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xFF01)
NVM3KEY_STACK_NONCE_COUNTER#
#define NVM3KEY_STACK_NONCE_COUNTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE563)
NVM3KEY_STACK_ANALYSIS_REBOOT#
#define NVM3KEY_STACK_ANALYSIS_REBOOTValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE162)
NVM3KEY_STACK_ALTERNATE_KEY#
#define NVM3KEY_STACK_ALTERNATE_KEYValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE475)
NVM3KEY_STACK_APS_FRAME_COUNTER#
#define NVM3KEY_STACK_APS_FRAME_COUNTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE123)
NVM3KEY_STACK_NETWORK_MANAGEMENT#
#define NVM3KEY_STACK_NETWORK_MANAGEMENTValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE125)
NVM3KEY_STACK_PARENT_ADDITIONAL_INFO#
#define NVM3KEY_STACK_PARENT_ADDITIONAL_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE127)
NVM3KEY_STACK_MULTI_PHY_NWK_INFO#
#define NVM3KEY_STACK_MULTI_PHY_NWK_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE128)
NVM3KEY_STACK_MIN_RECEIVED_RSSI#
#define NVM3KEY_STACK_MIN_RECEIVED_RSSIValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE129)
NVM3KEY_MULTI_NETWORK_STACK_KEYS#
#define NVM3KEY_MULTI_NETWORK_STACK_KEYSValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0000)
NVM3KEY_MULTI_NETWORK_STACK_NODE_DATA#
#define NVM3KEY_MULTI_NETWORK_STACK_NODE_DATAValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0080)
NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEY#
#define NVM3KEY_MULTI_NETWORK_STACK_ALTERNATE_KEYValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0100)
NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTER#
#define NVM3KEY_MULTI_NETWORK_STACK_TRUST_CENTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0180)
NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENT#
#define NVM3KEY_MULTI_NETWORK_STACK_NETWORK_MANAGEMENTValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0200)
NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFO#
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0280)
NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTER#
#define NVM3KEY_MULTI_NETWORK_STACK_NONCE_COUNTERValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0xE220)
NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFO#
#define NVM3KEY_MULTI_NETWORK_STACK_PARENT_ADDITIONAL_INFOValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0300)
NVM3KEY_STACK_GP_PROXY_TABLE#
#define NVM3KEY_STACK_GP_PROXY_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0380)
NVM3KEY_STACK_GP_SINK_TABLE#
#define NVM3KEY_STACK_GP_SINK_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0400)
NVM3KEY_STACK_GP_INCOMING_FC#
#define NVM3KEY_STACK_GP_INCOMING_FCValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0480)
NVM3KEY_STACK_BINDING_TABLE#
#define NVM3KEY_STACK_BINDING_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0500)
NVM3KEY_STACK_CERTIFICATE_TABLE#
#define NVM3KEY_STACK_CERTIFICATE_TABLEValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0680)
NVM3KEY_STACK_ADDITIONAL_CHILD_DATA#
#define NVM3KEY_STACK_ADDITIONAL_CHILD_DATAValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0700)
NVM3KEY_STACK_GP_INCOMING_FC_IN_SINK#
#define NVM3KEY_STACK_GP_INCOMING_FC_IN_SINKValue:
(NVM3KEY_DOMAIN_ZIGBEE | 0x0780)
Macro Definition Documentation#
TOKEN_NEXT_ADDRESS#
#define TOKEN_NEXT_ADDRESS
By default, tokens are automatically located after the previous token.
If a token needs to be placed at a specific location, one of the DEFINE_FIXED_* definitions should be used. This macro is inherently used in the DEFINE_FIXED_* definition to locate a token and under special circumstances (such as manufacturing tokens) it may be explicitly used.
CURRENT_STACK_TOKEN_VERSION#
#define CURRENT_STACK_TOKEN_VERSIONValue:
0x03FC
The current version number of the stack tokens. MSB is the version, LSB is a complement.
See hal/micro/token.h for a more complete explanation.