Smart Energy Security#

This file describes functionality for Certificate Based Key Exchange (CBKE). This is used by Smart Energy devices to generate and store ephemeral ECC keys, derive the SMACs for the Key establishment protocol, and sign messages using their private key for the Demand Response Load Control client cluster.

See cbke-crypto-engine.h for source code.

Functions#

emberGetCertificate(EmberCertificateData *result)

Retrieves the implicit certificate stored in the MFG tokens of the device.

This function begins the process of generating an ephemeral public/private ECC key pair.

emberCalculateSmacs(bool amInitiator, EmberCertificateData *partnerCert, EmberPublicKeyData *partnerEphemeralPublicKey)

This function will begin the process of generating the shared secret, the new link key, and the Secured Message Authentication Code (SMAC).

This function should be called when all CBKE operations are done. Any temporary data created during calls to emberGenerateCbkeKeys() or emberCalculateSmacs() is wiped out. If the local device has validated that the partner device has generated the same SMACS as itself, it should set 'storeLinkKey' to true. Otherwise it should pass in false.

emberDsaSign(EmberMessageBuffer messageToSign)
void
emberGenerateCbkeKeysHandler(EmberStatus status, EmberPublicKeyData *ephemeralPublicKey)
void
emberCalculateSmacsHandler(EmberStatus status, EmberSmacData *initiatorSmac, EmberSmacData *responderSmac)
void
emberDsaSignHandler(EmberStatus status, EmberMessageBuffer signedMessage)
emberSetPreinstalledCbkeData(EmberPublicKeyData *caPublic, EmberCertificateData *myCert, EmberPrivateKeyData *myKey)
bool
emberGetStackCertificateEui64(EmberEUI64 certEui64)
emberDsaVerify(EmberMessageDigest *digest, EmberCertificateData *signerCertificate, EmberSignatureData *receivedSig)
void
emberDsaVerifyHandler(EmberStatus status)
emberGetCertificate283k1(EmberCertificate283k1Data *result)

Retrieves the implicit certificate stored in the MFG tokens of the device.

This function begins the process of generating an ephemeral public/private ECC key pair.

emberCalculateSmacs283k1(bool amInitiator, EmberCertificate283k1Data *partnerCert, EmberPublicKey283k1Data *partnerEphemeralPublicKey)

This function will begin the process of generating the shared secret, the new link key, and the Secured Message Authentication Code (SMAC).

This function should be called when all CBKE 283k1 operations are done. Any temporary data created during calls to emberGenerateCbkeKeys283k1() or emberCalculateSmacs283k1() is wiped out. If the local device has validated that the partner device has generated the same SMACS as itself, it should set 'storeLinkKey' to true. Otherwise it should pass in false.

void
emberGenerateCbkeKeysHandler283k1(EmberStatus status, EmberPublicKey283k1Data *ephemeralPublicKey)
void
emberCalculateSmacsHandler283k1(EmberStatus status, EmberSmacData *initiatorSmac, EmberSmacData *responderSmac)
emberSetPreinstalledCbkeData283k1(EmberPublicKey283k1Data *caPublic, EmberCertificate283k1Data *myCert, EmberPrivateKey283k1Data *myKey)
emberDsaVerify283k1(EmberMessageDigest *digest, EmberCertificate283k1Data *signerCertificate, EmberSignature283k1Data *receivedSig)

Function Documentation#

emberGetCertificate#

EmberStatus emberGetCertificate (EmberCertificateData * result)

Retrieves the implicit certificate stored in the MFG tokens of the device.

Parameters
TypeDirectionArgument NameDescription
EmberCertificateData *N/Aresult

A pointer to an EmberCertificateData structure where the retrieved certificate will be stored.

Returns


emberGenerateCbkeKeys#

EmberStatus emberGenerateCbkeKeys (void )

This function begins the process of generating an ephemeral public/private ECC key pair.

Parameters
TypeDirectionArgument NameDescription
voidN/A

If no other ECC operation is going on, it will immediately return with EMBER_OPERATION_IN_PROGRESS. It will delay a period of time to let APS retries take place, but then it will shutdown the radio and consume the CPU processing until the key generation is complete. This may take up to 1 second.

The generated results of the key generation is returned via emberGenerateCbkeKeysHandler().

Returns


emberCalculateSmacs#

EmberStatus emberCalculateSmacs (bool amInitiator, EmberCertificateData * partnerCert, EmberPublicKeyData * partnerEphemeralPublicKey)

This function will begin the process of generating the shared secret, the new link key, and the Secured Message Authentication Code (SMAC).

Parameters
TypeDirectionArgument NameDescription
boolN/AamInitiator

This bool indicates whether or not the device is the one that initiated the CBKE with the remote device, or whether it was the responder to the exchange.

EmberCertificateData *N/ApartnerCert

A pointer to an EmberCertificateData structure that contains the CBKE partner's implicit certificate.

EmberPublicKeyData *N/ApartnerEphemeralPublicKey

A pointer to an EmberPublicKeyData structure that contains the CBKE partner's ephemeral public key.

If no other ECC operation is going on, it will immediately return with EMBER_OPERATION_IN_PROGRESS. It will delay a period of time to let APS retries take place, but then it will shutdown the radio and consume the CPU processing until SMACs calculations are complete. This may take up to 3.5 seconds.

The calculated SMACS are returned via emberCalculateSmacsHandler().

Returns


emberClearTemporaryDataMaybeStoreLinkKey#

EmberStatus emberClearTemporaryDataMaybeStoreLinkKey (bool storeLinkKey)

This function should be called when all CBKE operations are done. Any temporary data created during calls to emberGenerateCbkeKeys() or emberCalculateSmacs() is wiped out. If the local device has validated that the partner device has generated the same SMACS as itself, it should set 'storeLinkKey' to true. Otherwise it should pass in false.

Parameters
TypeDirectionArgument NameDescription
boolN/AstoreLinkKey

This tells the stack whether to store the newly generated link key, or discard it.

Returns

  • If storeLinkkey is false, this function returns EMBER_ERR_FATAL always. If storeLinkKey is true, then this function returns the results of whether or not the link key was stored. EMBER_SUCCESS is returned when key was stored successfully.


emberDsaSign#

EmberStatus emberDsaSign (EmberMessageBuffer messageToSign)
Parameters
TypeDirectionArgument NameDescription
EmberMessageBufferN/AmessageToSign

emberGenerateCbkeKeysHandler#

void emberGenerateCbkeKeysHandler (EmberStatus status, EmberPublicKeyData * ephemeralPublicKey)
Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Astatus
EmberPublicKeyData *N/AephemeralPublicKey

emberCalculateSmacsHandler#

void emberCalculateSmacsHandler (EmberStatus status, EmberSmacData * initiatorSmac, EmberSmacData * responderSmac)
Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Astatus
EmberSmacData *N/AinitiatorSmac
EmberSmacData *N/AresponderSmac

emberDsaSignHandler#

void emberDsaSignHandler (EmberStatus status, EmberMessageBuffer signedMessage)
Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Astatus
EmberMessageBufferN/AsignedMessage

emberSetPreinstalledCbkeData#

EmberStatus emberSetPreinstalledCbkeData (EmberPublicKeyData * caPublic, EmberCertificateData * myCert, EmberPrivateKeyData * myKey)
Parameters
TypeDirectionArgument NameDescription
EmberPublicKeyData *N/AcaPublic
EmberCertificateData *N/AmyCert
EmberPrivateKeyData *N/AmyKey

emberGetStackCertificateEui64#

bool emberGetStackCertificateEui64 (EmberEUI64 certEui64)
Parameters
TypeDirectionArgument NameDescription
EmberEUI64N/AcertEui64

emberDsaVerify#

EmberStatus emberDsaVerify (EmberMessageDigest * digest, EmberCertificateData * signerCertificate, EmberSignatureData * receivedSig)
Parameters
TypeDirectionArgument NameDescription
EmberMessageDigest *N/Adigest
EmberCertificateData *N/AsignerCertificate
EmberSignatureData *N/AreceivedSig

emberDsaVerifyHandler#

void emberDsaVerifyHandler (EmberStatus status)
Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Astatus

emberGetCertificate283k1#

EmberStatus emberGetCertificate283k1 (EmberCertificate283k1Data * result)

Retrieves the implicit certificate stored in the MFG tokens of the device.

Parameters
TypeDirectionArgument NameDescription
EmberCertificate283k1Data *N/Aresult

A pointer to an EmberCertificate283k1Data structure where the retrieved certificate will be stored.

Returns


emberGenerateCbkeKeys283k1#

EmberStatus emberGenerateCbkeKeys283k1 (void )

This function begins the process of generating an ephemeral public/private ECC key pair.

Parameters
TypeDirectionArgument NameDescription
voidN/A

If no other ECC operation is going on, it will immediately return with EMBER_OPERATION_IN_PROGRESS. It will delay a period of time to let APS retries take place, but then it will shutdown the radio and consume the CPU processing until the key generation is complete. This may take up to 1 second.

The generated results of the key generation is returned via emberGenerateCbkeKeysHandler283k1().

Returns


emberCalculateSmacs283k1#

EmberStatus emberCalculateSmacs283k1 (bool amInitiator, EmberCertificate283k1Data * partnerCert, EmberPublicKey283k1Data * partnerEphemeralPublicKey)

This function will begin the process of generating the shared secret, the new link key, and the Secured Message Authentication Code (SMAC).

Parameters
TypeDirectionArgument NameDescription
boolN/AamInitiator

This bool indicates whether or not the device is the one that initiated the CBKE with the remote device, or whether it was the responder to the exchange.

EmberCertificate283k1Data *N/ApartnerCert

A pointer to an EmberCertificate283k1Data structure that contains the CBKE partner's implicit certificate.

EmberPublicKey283k1Data *N/ApartnerEphemeralPublicKey

A pointer to an EmberPublicKey283k1Data structure that contains the CBKE partner's ephemeral public key.

If no other ECC operation is going on, it will immediately return with EMBER_OPERATION_IN_PROGRESS. It will delay a period of time to let APS retries take place, but then it will shutdown the radio and consume the CPU processing until SMACs calculations are complete. This may take up to 3.5 seconds.

The calculated SMACS are returned via emberCalculateSmacsHandler().

Returns


emberClearTemporaryDataMaybeStoreLinkKey283k1#

EmberStatus emberClearTemporaryDataMaybeStoreLinkKey283k1 (bool storeLinkKey)

This function should be called when all CBKE 283k1 operations are done. Any temporary data created during calls to emberGenerateCbkeKeys283k1() or emberCalculateSmacs283k1() is wiped out. If the local device has validated that the partner device has generated the same SMACS as itself, it should set 'storeLinkKey' to true. Otherwise it should pass in false.

Parameters
TypeDirectionArgument NameDescription
boolN/AstoreLinkKey

This tells the stack whether to store the newly generated link key, or discard it.

Returns

  • If storeLinkkey is false, this function returns EMBER_ERR_FATAL always. If storeLinkKey is true, then this function returns the results of whether or not the link key was stored. EMBER_SUCCESS is returned when key was stored successfully.


emberGenerateCbkeKeysHandler283k1#

void emberGenerateCbkeKeysHandler283k1 (EmberStatus status, EmberPublicKey283k1Data * ephemeralPublicKey)
Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Astatus
EmberPublicKey283k1Data *N/AephemeralPublicKey

emberCalculateSmacsHandler283k1#

void emberCalculateSmacsHandler283k1 (EmberStatus status, EmberSmacData * initiatorSmac, EmberSmacData * responderSmac)
Parameters
TypeDirectionArgument NameDescription
EmberStatusN/Astatus
EmberSmacData *N/AinitiatorSmac
EmberSmacData *N/AresponderSmac

emberSetPreinstalledCbkeData283k1#

EmberStatus emberSetPreinstalledCbkeData283k1 (EmberPublicKey283k1Data * caPublic, EmberCertificate283k1Data * myCert, EmberPrivateKey283k1Data * myKey)
Parameters
TypeDirectionArgument NameDescription
EmberPublicKey283k1Data *N/AcaPublic
EmberCertificate283k1Data *N/AmyCert
EmberPrivateKey283k1Data *N/AmyKey

emberDsaVerify283k1#

EmberStatus emberDsaVerify283k1 (EmberMessageDigest * digest, EmberCertificate283k1Data * signerCertificate, EmberSignature283k1Data * receivedSig)
Parameters
TypeDirectionArgument NameDescription
EmberMessageDigest *N/Adigest
EmberCertificate283k1Data *N/AsignerCertificate
EmberSignature283k1Data *N/AreceivedSig