Zigbee Event Logger APIs#
This file describes functionality for the Zigbee Event Logger feature. This feature is used to record salient events in the stack and application layer. The system event data is stored in a buffer, with hooks for the application to print and decode the logged data.
See zigbee-event-logger-gen.h for source code.
Enumerations#
A list of identifiers for system events.
A list of facilities for system events, identifying which layer they occurred in.
Functions#
Record an event indicating that the device has booted.
Record an event indicating that a network was successfully joined.
Record an event indicating that a trust center rejoin was attempted.
Record an event indicating that a secure rejoin was attempted.
Record an event indicating that a device has left-without-rejoin.
Record an event indicating that a device has left-with-rejoin.
Record an event indicating that an attempt was made to update the trust center link key.
Record an event indicating that the network key sequence number has changed.
Record an event indicating that the local device has reset.
Record an event indicating that the network's channel has changed.
Record an event indicating that the local device's parent has changed.
Record an event indicating that the duty cycle has changed.
Record an event indicating that a child device has joined the local device.
Record an event indicating that a child device has been removed from the local device.
Record an event indicating that a child device has been timed out by the local device.
Record an event indicating that the stack status has changed.
Record an event indicating that the clock time has been synchronized.
Record an event indicating that a device has attempted to join or rejoin the network.
Macros#
The version of this feature.
The length of the Boot Event event data.
The length of the Join Network event data.
The length of the Trust Center Rejoin event data.
The length of the Secure Rejoin event data.
The length of the Leave Without Rejoin event data.
The length of the Leave With Rejoin event data.
The length of the Trust Center Link Key Change event data.
The length of the Network Key Sequence Number Change event data.
The length of the Reset event data.
The length of the Channel Change event data.
The length of the Parent Change event data.
The length of the Duty Cycle Change event data.
The length of the Child Added event data.
The length of the Child Removed event data.
The length of the Child Timed Out event data.
The length of the Stack Status event data.
The length of the Time Sync event data.
The length of the Trust Center Join Decision event data.
Enumeration Documentation#
EmberZigbeeLoggerEventTypes#
EmberZigbeeLoggerEventTypes
A list of identifiers for system events.
| Enumerator | |
|---|---|
| EMBER_LOGGER_ZIGBEE_BOOT_EVENT_ID | |
| EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_ID | |
| EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_ID | |
| EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_ID | |
| EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_ID | |
| EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_ID | |
| EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_RESET_ID | |
| EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_ID | |
| EMBER_LOGGER_ZIGBEE_CHILD_ADDED_ID | |
| EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_ID | |
| EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_ID | |
| EMBER_LOGGER_ZIGBEE_STACK_STATUS_ID | |
| EMBER_LOGGER_ZIGBEE_TIME_SYNC_ID | |
| EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_ID | |
| EMBER_LOGGER_ZIGBEE_NULL_ID | |
EmberZigbeeLoggerFacilityTypes#
EmberZigbeeLoggerFacilityTypes
A list of facilities for system events, identifying which layer they occurred in.
| Enumerator | |
|---|---|
| EMBER_LOGGER_ZIGBEE_FACILITY_BASE | |
| EMBER_LOGGER_ZIGBEE_FACILITY_MAC | |
| EMBER_LOGGER_ZIGBEE_FACILITY_NETWORK | |
| EMBER_LOGGER_ZIGBEE_FACILITY_APS | |
| EMBER_LOGGER_ZIGBEE_FACILITY_SECURITY | |
| EMBER_LOGGER_ZIGBEE_FACILITY_ZDO | |
| EMBER_LOGGER_ZIGBEE_FACILITY_ZCL | |
| EMBER_LOGGER_ZIGBEE_FACILITY_BDB | |
| EMBER_LOGGER_ZIGBEE_FACILITY_SMART_ENERGY | |
Function Documentation#
emberAfPluginZigBeeEventLoggerAddBootEvent#
void emberAfPluginZigBeeEventLoggerAddBootEvent (uint32_t bootCount, uint16_t resetType)
Record an event indicating that the device has booted.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | bootCount | The number of times the device has booted. |
| uint16_t | N/A | resetType | A reset cause. See micro.h and reset-def.h. |
Note
This API only works on SoC. It does not work on host or NCP.
emberAfPluginZigBeeEventLoggerAddJoinNetwork#
void emberAfPluginZigBeeEventLoggerAddJoinNetwork (EmberPanId panId, uint8_t channelNumber, uint8_t page, uint8_t * extendedPanId)
Record an event indicating that a network was successfully joined.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberPanId | N/A | panId | The PAN ID of the network. |
| uint8_t | N/A | channelNumber | The channel of the network. |
| uint8_t | N/A | page | The page of the network joined. |
| uint8_t * | N/A | extendedPanId | The extended PAN ID of the network. |
emberAfPluginZigBeeEventLoggerAddTrustCenterRejoin#
void emberAfPluginZigBeeEventLoggerAddTrustCenterRejoin (uint32_t channelMask, EmberRejoinReason reason)
Record an event indicating that a trust center rejoin was attempted.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | channelMask | The channel mask used when searching for the network. |
| EmberRejoinReason | N/A | reason | An EmberRejoinReason enumeration, indicating why the rejoin was initiated. |
Note
This event only indicates that a rejoin was attempted, not that it was successful. A Join Network event, following this event, indicates success.
emberAfPluginZigBeeEventLoggerAddSecureRejoin#
void emberAfPluginZigBeeEventLoggerAddSecureRejoin (uint32_t channelMask, EmberRejoinReason reason)
Record an event indicating that a secure rejoin was attempted.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | channelMask | The channel mask used when searching for the network. |
| EmberRejoinReason | N/A | reason | An EmberRejoinReason enumeration, indicating why the rejoin was initiated. |
Note
This event only indicates that a rejoin was attempted, not that it was successful. A Join Network event, following this event, indicates success.
emberAfPluginZigBeeEventLoggerAddLeaveWithoutRejoin#
void emberAfPluginZigBeeEventLoggerAddLeaveWithoutRejoin (EmberNodeId sourceNode, EmberLeaveReason reason)
Record an event indicating that a device has left-without-rejoin.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | sourceNode | The node ID of the device leaving. |
| EmberLeaveReason | N/A | reason | An EmberLeaveReason enumeration, indicating why the device left. |
emberAfPluginZigBeeEventLoggerAddLeaveWithRejoin#
void emberAfPluginZigBeeEventLoggerAddLeaveWithRejoin (EmberNodeId sourceNode, EmberLeaveReason reason)
Record an event indicating that a device has left-with-rejoin.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | sourceNode | The node ID of the device leaving-and-rejoining. |
| EmberLeaveReason | N/A | reason | An EmberLeaveReason enumeration, indicating why the device left. |
emberAfPluginZigBeeEventLoggerAddTrustCenterLinkKeyChange#
void emberAfPluginZigBeeEventLoggerAddTrustCenterLinkKeyChange (void )
Record an event indicating that an attempt was made to update the trust center link key.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
emberAfPluginZigBeeEventLoggerAddNetworkKeySequenceChange#
void emberAfPluginZigBeeEventLoggerAddNetworkKeySequenceChange (uint8_t sequence)
Record an event indicating that the network key sequence number has changed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | sequence | The new network key sequence number. |
emberAfPluginZigBeeEventLoggerAddReset#
void emberAfPluginZigBeeEventLoggerAddReset (uint8_t resetCode, uint8_t extendedReason)
Record an event indicating that the local device has reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | resetCode | The reset code. See reset-def.h. |
| uint8_t | N/A | extendedReason | The extended reset reason. See reset-def.h. |
emberAfPluginZigBeeEventLoggerAddChannelChange#
void emberAfPluginZigBeeEventLoggerAddChannelChange (uint8_t page, uint8_t channel)
Record an event indicating that the network's channel has changed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | page | The new page number. |
| uint8_t | N/A | channel | The new channel number. |
emberAfPluginZigBeeEventLoggerAddParentChange#
void emberAfPluginZigBeeEventLoggerAddParentChange (EmberNodeId parentNodeId, EmberEUI64 parentEui64)
Record an event indicating that the local device's parent has changed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | parentNodeId | The new parent's short address. |
| EmberEUI64 | N/A | parentEui64 | The new parent's long address. |
emberAfPluginZigBeeEventLoggerAddDutyCycleChange#
void emberAfPluginZigBeeEventLoggerAddDutyCycleChange (EmberDutyCycleState state, EmberDutyCycleHectoPct limitThreshold, EmberDutyCycleHectoPct criticalThreshold, EmberDutyCycleHectoPct suspendedLimit)
Record an event indicating that the duty cycle has changed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberDutyCycleState | N/A | state | An EmberDutyCycleState state. |
| EmberDutyCycleHectoPct | N/A | limitThreshold | An EmberDutyCycleHectoPct limit. |
| EmberDutyCycleHectoPct | N/A | criticalThreshold | An EmberDutyCycleHectoPct critical threshold. |
| EmberDutyCycleHectoPct | N/A | suspendedLimit | An EmberDutyCycleHectoPct suspend limit. |
emberAfPluginZigBeeEventLoggerAddChildAdded#
void emberAfPluginZigBeeEventLoggerAddChildAdded (EmberNodeId childNodeId, EmberEUI64 childEui64)
Record an event indicating that a child device has joined the local device.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | childNodeId | The child's short address. |
| EmberEUI64 | N/A | childEui64 | The child's long address. |
emberAfPluginZigBeeEventLoggerAddChildRemoved#
void emberAfPluginZigBeeEventLoggerAddChildRemoved (EmberNodeId childNodeId, EmberEUI64 childEui64)
Record an event indicating that a child device has been removed from the local device.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | childNodeId | The child's short address. |
| EmberEUI64 | N/A | childEui64 | The child's long address. |
emberAfPluginZigBeeEventLoggerAddChildTimedOut#
void emberAfPluginZigBeeEventLoggerAddChildTimedOut (EmberNodeId childNodeId, EmberEUI64 childEui64)
Record an event indicating that a child device has been timed out by the local device.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | childNodeId | The child's short address. |
| EmberEUI64 | N/A | childEui64 | The child's long address. |
emberAfPluginZigBeeEventLoggerAddStackStatus#
void emberAfPluginZigBeeEventLoggerAddStackStatus (EmberStatus status)
Record an event indicating that the stack status has changed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberStatus | N/A | status | An EmberStatus value indicating the change. |
emberAfPluginZigBeeEventLoggerAddTimeSync#
void emberAfPluginZigBeeEventLoggerAddTimeSync (uint32_t utcTime, uint32_t secondsSinceBoot)
Record an event indicating that the clock time has been synchronized.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | utcTime | The updated UTC time. |
| uint32_t | N/A | secondsSinceBoot | The number of seconds that have elapsed since boot. |
emberAfPluginZigBeeEventLoggerAddTrustCenterJoinDecision#
void emberAfPluginZigBeeEventLoggerAddTrustCenterJoinDecision (EmberNodeId nodeId, uint8_t decision)
Record an event indicating that a device has attempted to join or rejoin the network.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | nodeId | The short address of the device attempting to join or rejoin. |
| uint8_t | N/A | decision | The join or rejoin decision taken by the local device. |
Note
This event is only recorded on a trust center device.
Macro Definition Documentation#
EMBER_LOGGER_ZIGBEE_BOOT_EVENT_LENGTH#
#define EMBER_LOGGER_ZIGBEE_BOOT_EVENT_LENGTHValue:
6
The length of the Boot Event event data.
EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_LENGTH#
#define EMBER_LOGGER_ZIGBEE_JOIN_NETWORK_LENGTHValue:
12
The length of the Join Network event data.
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_LENGTH#
#define EMBER_LOGGER_ZIGBEE_TRUST_CENTER_REJOIN_LENGTHValue:
5
The length of the Trust Center Rejoin event data.
EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_LENGTH#
#define EMBER_LOGGER_ZIGBEE_SECURE_REJOIN_LENGTHValue:
5
The length of the Secure Rejoin event data.
EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_LENGTH#
#define EMBER_LOGGER_ZIGBEE_LEAVE_WITHOUT_REJOIN_LENGTHValue:
3
The length of the Leave Without Rejoin event data.
EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_LENGTH#
#define EMBER_LOGGER_ZIGBEE_LEAVE_WITH_REJOIN_LENGTHValue:
3
The length of the Leave With Rejoin event data.
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_LENGTH#
#define EMBER_LOGGER_ZIGBEE_TRUST_CENTER_LINK_KEY_CHANGE_LENGTHValue:
0
The length of the Trust Center Link Key Change event data.
EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_LENGTH#
#define EMBER_LOGGER_ZIGBEE_NETWORK_KEY_SEQUENCE_NUMBER_CHANGE_LENGTHValue:
1
The length of the Network Key Sequence Number Change event data.
EMBER_LOGGER_ZIGBEE_RESET_LENGTH#
#define EMBER_LOGGER_ZIGBEE_RESET_LENGTHValue:
2
The length of the Reset event data.
EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_LENGTH#
#define EMBER_LOGGER_ZIGBEE_CHANNEL_CHANGE_LENGTHValue:
2
The length of the Channel Change event data.
EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_LENGTH#
#define EMBER_LOGGER_ZIGBEE_PARENT_CHANGE_LENGTHValue:
10
The length of the Parent Change event data.
EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_LENGTH#
#define EMBER_LOGGER_ZIGBEE_DUTY_CYCLE_CHANGE_LENGTHValue:
7
The length of the Duty Cycle Change event data.
EMBER_LOGGER_ZIGBEE_CHILD_ADDED_LENGTH#
#define EMBER_LOGGER_ZIGBEE_CHILD_ADDED_LENGTHValue:
10
The length of the Child Added event data.
EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_LENGTH#
#define EMBER_LOGGER_ZIGBEE_CHILD_REMOVED_LENGTHValue:
10
The length of the Child Removed event data.
EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_LENGTH#
#define EMBER_LOGGER_ZIGBEE_CHILD_TIMED_OUT_LENGTHValue:
10
The length of the Child Timed Out event data.
EMBER_LOGGER_ZIGBEE_STACK_STATUS_LENGTH#
#define EMBER_LOGGER_ZIGBEE_STACK_STATUS_LENGTHValue:
1
The length of the Stack Status event data.
EMBER_LOGGER_ZIGBEE_TIME_SYNC_LENGTH#
#define EMBER_LOGGER_ZIGBEE_TIME_SYNC_LENGTHValue:
8
The length of the Time Sync event data.
EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_LENGTH#
#define EMBER_LOGGER_ZIGBEE_TRUST_CENTER_JOIN_DECISION_LENGTHValue:
3
The length of the Trust Center Join Decision event data.