Cluster Commands: Events#

This group describes the CLI commands for the Events cluster. Listed below is a description of the cluster: This cluster provides an interface on which applications can use event-based protocols.

Macros#

#define

zcl events get-event-log [eventControlLogId:1] [eventId:2] [startTime:4] [endTime:4] [numberOfEvents:1] [eventOffset:2]

#define

zcl events clear-event-log [logId:1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_EVENTS_GET_EVENT_LOG#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_EVENTS_GET_EVENT_LOG

zcl events get-event-log [eventControlLogId:1] [eventId:2] [startTime:4] [endTime:4] [numberOfEvents:1] [eventOffset:2]

  • The GetEventLog command allows a client to request events from a server's event logs. One or more PublishEventLog commands are returned on receipt of this command.

    • eventControlLogId - EventControlLogId [BITMAP8]

    • eventId - INT16U

    • startTime - UTC_TIME

    • endTime - UTC_TIME

    • numberOfEvents - INT8U

    • eventOffset - INT16U


Definition at line 1058 of file app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_EVENTS_CLEAR_EVENT_LOG#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_EVENTS_CLEAR_EVENT_LOG

zcl events clear-event-log [logId:1]

  • The ClearEventLogRequest command requests that an Events server device clear the specified event log(s).


Definition at line 1066 of file app/framework/test/headers/cli.doc