Concentrator Support#
API and Callbacks for the Concentrator Support Component.
Code that handles periodically broadcasting a many-to-one-route-request (MTORR) so that the device will act as a concentrator (sink) in the network.
Note: NCP/SOC source route table size can be now defined as part of the source routing library.
Enumerations#
enum
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_NONE = NONE
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL = FULL
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_MAX = SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL
}
Typedefs#
typedef uint8_t
Variables#
sl_zigbee_event_control_t
Macros#
#define
LOW_RAM_CONCENTRATOR SL_ZIGBEE_LOW_RAM_CONCENTRATOR
#define
HIGH_RAM_CONCENTRATOR SL_ZIGBEE_HIGH_RAM_CONCENTRATOR
#define
sl_zigbee_af_concentrator_get_router_behavior ()
#define
sl_zigbee_af_concentrator_set_router_behavior (behavior)
API Documentation#
sl_zigbee_af_concentrator_queue_discovery#
uint32_t sl_zigbee_af_concentrator_queue_discovery (void )
Concentrator source route discovery.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
uint32_t
sl_zigbee_af_concentrator_stop_discovery#
void sl_zigbee_af_concentrator_stop_discovery (void )
Concentrator stop source route discover.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Enumeration Documentation#
sl_zigbee_af_plugin_concentrator_router_behavior_t#
sl_zigbee_af_plugin_concentrator_router_behavior_t
| Enumerator | |
|---|---|
| SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_NONE | |
| SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL | |
| SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_MAX | |
Typedef Documentation#
sl_zigbee_af_plugin_concentrator_router_behavior_t#
typedef uint8_t sl_zigbee_af_plugin_concentrator_router_behavior_t
Variable Documentation#
sl_zigbee_af_concentrator_update_event_control#
sl_zigbee_event_control_t sl_zigbee_af_concentrator_update_event_control
sli_zigbee_af_concentrator_router_behaviors#
sl_zigbee_af_plugin_concentrator_router_behavior_t sli_zigbee_af_concentrator_router_behaviors[]