A struct for keeping track of all of the header info.

A struct for keeping track of all of the interpan header info.

Public Attributes#

uint16_t
sl_802154_short_addr_t
sl_802154_long_addr_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

messageType#

uint8_t sli_zigbee_interpan_header_t::messageType

Definition at line 62 of file app/util/zigbee-framework/ami-inter-pan.h

panId#

uint16_t sli_zigbee_interpan_header_t::panId

Definition at line 67 of file app/util/zigbee-framework/ami-inter-pan.h

hasLongAddress#

bool sli_zigbee_interpan_header_t::hasLongAddress

Definition at line 68 of file app/util/zigbee-framework/ami-inter-pan.h

shortAddress#

sl_802154_short_addr_t sli_zigbee_interpan_header_t::shortAddress

Definition at line 69 of file app/util/zigbee-framework/ami-inter-pan.h

longAddress#

sl_802154_long_addr_t sli_zigbee_interpan_header_t::longAddress

Definition at line 70 of file app/util/zigbee-framework/ami-inter-pan.h

profileId#

uint16_t sli_zigbee_interpan_header_t::profileId

Definition at line 73 of file app/util/zigbee-framework/ami-inter-pan.h

clusterId#

uint16_t sli_zigbee_interpan_header_t::clusterId

Definition at line 74 of file app/util/zigbee-framework/ami-inter-pan.h

groupId#

uint16_t sli_zigbee_interpan_header_t::groupId

Definition at line 75 of file app/util/zigbee-framework/ami-inter-pan.h