Defines an entry in the binding table.
A binding entry specifies a local endpoint, a remote endpoint, a cluster ID and either the destination EUI64 (for unicast bindings) or the 64-bit group address (for multicast bindings).
Public Attribute Documentation#
clusterId#
uint16_t sl_zigbee_binding_table_entry_t::clusterId
A cluster ID that matches one from the local endpoint's simple descriptor. This cluster ID is set by the provisioning application to indicate which part an endpoint's functionality is bound to this particular remote node and is used to distinguish between unicast and multicast bindings. Note that a binding can be used to to send messages with any cluster ID, not just that listed in the binding.
remote#
uint8_t sl_zigbee_binding_table_entry_t::remote
The endpoint on the remote node (specified by identifier). 
identifier#
sl_802154_long_addr_t sl_zigbee_binding_table_entry_t::identifier
A 64-bit identifier. This is either:
- The destination EUI64, for unicasts. 
- A 16-bit multicast group address, for multicasts. 
networkIndex#
uint8_t sl_zigbee_binding_table_entry_t::networkIndex
The index of the network the binding belongs to.