You are viewing documentation for version:
A structure containing the information of a token. 
Public Attribute Documentation#
nvm3Key#
uint32_t sl_zigbee_token_info_t::nvm3Key
NVM3 token key. 
isCnt#
bool sl_zigbee_token_info_t::isCnt
The token is a counter token type. 
isIdx#
bool sl_zigbee_token_info_t::isIdx
The token is an indexed token type. 
size#
uint8_t sl_zigbee_token_info_t::size
Size of the object of the token. 
arraySize#
uint8_t sl_zigbee_token_info_t::arraySize
The array size for the token when it is an indexed token.