Comms Hub Function#

API and Callbacks for the Comms Hub Function Component.

Silicon Labs implementation of the Comms Hub Function (CHF).

Modules#

Comms Hub

API#

sl_zigbee_af_comms_hub_function_send(sl_802154_long_addr_t destinationDeviceId, uint16_t length, uint8_t *payload, uint16_t messageCode)

Pass a message to be tunneled over the HAN using either a sleepy buffer system (GSME) or directly to the device by initiating a tunnel (ESME, HCALCS, PPMID, TYPE2).

void

Set the default remote part message timeout.

sli_zigbee_af_update_functional_notification_flags_by_eui64(sl_802154_long_addr_t deviceId, uint32_t resetMask, uint32_t setMask)

Update Functional Notification Flags for the given device.

sli_zigbee_af_update_functional_notification_flags_by_endpoint(uint8_t endpoint, uint32_t resetMask, uint32_t setMask)

Update Functional Notification Flags on the given endpoint.

Enumerations#

enum
SL_ZIGBEE_AF_CHF_STATUS_SUCCESS = 0x00
SL_ZIGBEE_AF_CHF_STATUS_TOO_MANY_PEND_MESSAGES = 0xFA
SL_ZIGBEE_AF_CHF_STATUS_FNF_ATTR_FAILURE = 0xFB
SL_ZIGBEE_AF_CHF_STATUS_NO_MIRROR = 0xFC
SL_ZIGBEE_AF_CHF_STATUS_TUNNEL_FAILURE = 0xFD
SL_ZIGBEE_AF_CHF_STATUS_NO_ACCESS = 0xFE
SL_ZIGBEE_AF_CHF_STATUS_SEND_TIMEOUT = 0xFF
}

API Documentation#

sl_zigbee_af_comms_hub_function_send#

sl_zigbee_af_plugin_comms_hub_function_status_t sl_zigbee_af_comms_hub_function_send (sl_802154_long_addr_t destinationDeviceId, uint16_t length, uint8_t * payload, uint16_t messageCode)

Pass a message to be tunneled over the HAN using either a sleepy buffer system (GSME) or directly to the device by initiating a tunnel (ESME, HCALCS, PPMID, TYPE2).

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/AdestinationDeviceId

The EUI64 of the destination device.

uint16_tN/Alength

The length in octets of the data.

uint8_t *N/Apayload

The buffer (memory location at WAN Message Handler) containing the raw octets of the message (GBCS Message)

uint16_tN/AmessageCode

The GBCS Message Code for the data that is being sent.

This function is used to transfer data to a device on the HAN.

Returns


sli_zigbee_af_comms_hub_function_set_default_timeout#

void sli_zigbee_af_comms_hub_function_set_default_timeout (uint32_t timeout)

Set the default remote part message timeout.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/Atimeout

Timeout in seconds.

This function is used to set the default timeout for all messages destined for a sleepy device. If the device does not retrieve the message before this time, it will be discarded and a SL_ZIGBEE_AF_CHF_STATUS_SEND_TIMEOUT error will be return in sl_zigbee_af_comms_hub_function_send_cb().


sli_zigbee_af_update_functional_notification_flags_by_eui64#

sl_zigbee_af_plugin_comms_hub_function_status_t sli_zigbee_af_update_functional_notification_flags_by_eui64 (sl_802154_long_addr_t deviceId, uint32_t resetMask, uint32_t setMask)

Update Functional Notification Flags for the given device.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/AdeviceId

Identifier of the device for which the notification flags are to be updated

uint32_tN/AresetMask

Each flag to be reset has the corresponding bit set to 0, all other flags have the corresponding bit set to 1

uint32_tN/AsetMask

Each flag to be set has the corresponding bit set to 1, all other flags have the corresponding bit set to 0


sli_zigbee_af_update_functional_notification_flags_by_endpoint#

sl_zigbee_af_plugin_comms_hub_function_status_t sli_zigbee_af_update_functional_notification_flags_by_endpoint (uint8_t endpoint, uint32_t resetMask, uint32_t setMask)

Update Functional Notification Flags on the given endpoint.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aendpoint

An endpoint on which the notification flags are to be updated.

uint32_tN/AresetMask

Each flag to be reset has the corresponding bit set to 0, all other flags have the corresponding bit set to 1.

uint32_tN/AsetMask

Each flag to be set has the corresponding bit set to 1, all other flags have the corresponding bit set to 0.


Enumeration Documentation#

sl_zigbee_af_plugin_comms_hub_function_status_t#

sl_zigbee_af_plugin_comms_hub_function_status_t
Enumerator
SL_ZIGBEE_AF_CHF_STATUS_SUCCESS
SL_ZIGBEE_AF_CHF_STATUS_TOO_MANY_PEND_MESSAGES
SL_ZIGBEE_AF_CHF_STATUS_FNF_ATTR_FAILURE
SL_ZIGBEE_AF_CHF_STATUS_NO_MIRROR
SL_ZIGBEE_AF_CHF_STATUS_TUNNEL_FAILURE
SL_ZIGBEE_AF_CHF_STATUS_NO_ACCESS
SL_ZIGBEE_AF_CHF_STATUS_SEND_TIMEOUT

Macro Definition Documentation#

sl_zigbee_af_comms_hub_function_print#

#define sl_zigbee_af_comms_hub_function_print
Value:
(...)

sl_zigbee_af_comms_hub_function_println#

#define sl_zigbee_af_comms_hub_function_println
Value:
(...)

sl_zigbee_af_comms_hub_function_warn#

#define sl_zigbee_af_comms_hub_function_warn
Value:
(...)

sl_zigbee_af_comms_hub_function_warnln#

#define sl_zigbee_af_comms_hub_function_warnln
Value:
(...)

sl_zigbee_af_comms_hub_function_error#

#define sl_zigbee_af_comms_hub_function_error
Value:
(...)

sl_zigbee_af_comms_hub_function_errorln#

#define sl_zigbee_af_comms_hub_function_errorln
Value:
(...)

sl_zigbee_af_comms_hub_function_debug_exec#

#define sl_zigbee_af_comms_hub_function_debug_exec
Value:
(x)

sl_zigbee_af_comms_hub_function_print_buffer#

#define sl_zigbee_af_comms_hub_function_print_buffer
Value:
(buffer, len, withSpace)