Concentrator Support#

API and Callbacks for the Concentrator Support Component.

Code that handles periodically broadcasting a many-to-one-route-request (MTORR) so that the device will act as a concentrator (sink) in the network.

  • Note: NCP/SOC source route table size can be now defined as part of the source routing library.

API#

sl_status_t
sl_zigbee_af_concentrator_change_router_behavior(sl_zigbee_af_plugin_concentrator_router_behavior_t behavior)

Enable/disable the node concentrator behavior.

uint32_t

Schedule a concentrator source route discovery.

void

Stop a concentrator source route discovery request.

Enumerations#

enum
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_NONE = NONE
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL = FULL
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_MAX = SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL
}

Macros#

#define
LOW_RAM_CONCENTRATOR SL_ZIGBEE_LOW_RAM_CONCENTRATOR
#define
HIGH_RAM_CONCENTRATOR SL_ZIGBEE_HIGH_RAM_CONCENTRATOR
#define
INACTIVE_CONCENTRATOR SL_ZIGBEE_INACTIVE_CONCENTRATOR

API Documentation#

sl_zigbee_af_concentrator_change_router_behavior#

sl_status_t sl_zigbee_af_concentrator_change_router_behavior (sl_zigbee_af_plugin_concentrator_router_behavior_t behavior)

Enable/disable the node concentrator behavior.

Parameters
TypeDirectionArgument NameDescription
sl_zigbee_af_plugin_concentrator_router_behavior_t[in]behavior

concentrator router behavior.

Returns

  • An ::sl_status_t value that indicates the success or failure of the API call.

    • ::SL_STATUS_OK if successful.

    • ::SL_STATUS_NOT_AVAILABLE if the node is coordinator and behavior is switched to a non-concentrator.

    • ::SL_STATUS_INVALID_STATE if the behavior argument is invalid.


sl_zigbee_af_concentrator_queue_discovery#

uint32_t sl_zigbee_af_concentrator_queue_discovery (void )

Schedule a concentrator source route discovery.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Delay till the source route discovery is transmitted in quarter seconds.


sl_zigbee_af_concentrator_stop_discovery#

void sl_zigbee_af_concentrator_stop_discovery (void )

Stop a concentrator source route discovery request.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Enumeration Documentation#

sl_zigbee_af_plugin_concentrator_router_behavior_t#

sl_zigbee_af_plugin_concentrator_router_behavior_t
Enumerator
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_NONE
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL
SL_ZIGBEE_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_MAX

Typedef Documentation#

sl_zigbee_af_plugin_concentrator_router_behavior_t#

typedef uint8_t sl_zigbee_af_plugin_concentrator_router_behavior_t

Variable Documentation#

sl_zigbee_af_concentrator_update_event_control#

sl_zigbee_event_control_t sl_zigbee_af_concentrator_update_event_control

sli_zigbee_af_concentrator_router_behaviors#

sl_zigbee_af_plugin_concentrator_router_behavior_t sli_zigbee_af_concentrator_router_behaviors[]

Macro Definition Documentation#

LOW_RAM_CONCENTRATOR#

#define LOW_RAM_CONCENTRATOR
Value:
SL_ZIGBEE_LOW_RAM_CONCENTRATOR

HIGH_RAM_CONCENTRATOR#

#define HIGH_RAM_CONCENTRATOR
Value:
SL_ZIGBEE_HIGH_RAM_CONCENTRATOR

INACTIVE_CONCENTRATOR#

#define INACTIVE_CONCENTRATOR
Value:
SL_ZIGBEE_INACTIVE_CONCENTRATOR

sl_zigbee_af_concentrator_get_router_behavior#

#define sl_zigbee_af_concentrator_get_router_behavior
Value:
()

sl_zigbee_af_concentrator_set_router_behavior#

#define sl_zigbee_af_concentrator_set_router_behavior
Value:
(behavior)