MAC Address Filtering#

API and Callbacks for the MAC Address Filtering Component.

This plugin artificially limits what the stack hears by filtering the packets just above the lower MAC. The plugin can be configured on the fly via CLI with the short or long address of devices whose packets will be dropped or allowed. There are two lists, a short address list (2-byte node ID) and a long address list (8-byte IEEE address). Each list may be configured as either an allow list or block list. The default is a block list with no addresses configured (accept all packets normally). A separate option allows or drops packets with no address information (e.g., Beacon Requests). NOTE: The radio will still generate and process MAC ACKs for packets. This plugin cannot be used to effect the behavior of MAC ACKs, which are handled by the RAIL library and radio hardware.

Modules#

sli_802154_mac_address_filter_option_description_t

sli_zigbee_long_addres_filter_match_struct_t

sli_zigbee_short_addres_filter_match_struct_t

sli_802154_pan_id_filter_match_struct_t

sli_802154_mac_address_filter_globals_t

MAC Address Filtering

API#

void

Clear all lists for MAC address filtering.

void

Clears all packet counts for all modes.

sl_status_t
sl_zigbee_af_mac_address_filtering_get_stats_for_short_address(uint8_t index, uint32_t *matchCountForIndexPtr)

Get stats for a short address.

void
sl_zigbee_af_mac_address_filtering_get_stats(bool shortMode, uint32_t *allowedPacketCountPtr, uint32_t *droppedPacketCountPtr, uint32_t *totalPacketCountPtr)

Get MAC address filtering stats. Get the allowed, dropped and total packet counts.

void

Set the decision to manupulate the MAC address filtering tables.

void

Add the short address.

void

Add the long address.

void

Add the panID.

void

Set the short address list type.

void

Set the long address list type.

void

Set the list type of panId list.

Enumerations#

enum
MAC_ADDRESS_MODE_NONE = 0
MAC_ADDRESS_MODE_SHORT = 1
MAC_ADDRESS_MODE_LONG = 2
}
enum
MAC_FILTER_TYPE_NO_ADDRESS = 0
MAC_FILTER_TYPE_SHORT_ADDRESS = 1
MAC_FILTER_TYPE_LONG_ADDRESS = 2
MAC_FILTER_TYPE_PAN_ID = 3
}
enum
ALLOW_PACKET = 0
DROP_PACKET = 1
}

Typedefs#

Macros#

#define
#define
debug (...)
#define
MAC_FILTER_OPTIONS_NO_ADDRESS_MASK (1 << MAC_FILTER_TYPE_NO_ADDRESS)
#define
MAC_FILTER_OPTIONS_SHORT_ADDRESS_LIST_MASK (1 << MAC_FILTER_TYPE_SHORT_ADDRESS)
#define
MAC_FILTER_OPTIONS_LONG_ADDRESS_LIST_MASK (1 << MAC_FILTER_TYPE_LONG_ADDRESS)
#define
MAC_FILTER_OPTIONS_DEST_PAN_ID_LIST_MASK (1 << MAC_FILTER_TYPE_PAN_ID)
#define

API Documentation#

sl_zigbee_af_mac_address_filtering_clear_all#

void sl_zigbee_af_mac_address_filtering_clear_all (void )

Clear all lists for MAC address filtering.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_zigbee_af_mac_address_filtering_clear_stats#

void sl_zigbee_af_mac_address_filtering_clear_stats (void )

Clears all packet counts for all modes.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_zigbee_af_mac_address_filtering_get_stats_for_short_address#

sl_status_t sl_zigbee_af_mac_address_filtering_get_stats_for_short_address (uint8_t index, uint32_t * matchCountForIndexPtr)

Get stats for a short address.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aindex

Ver.: always

uint32_t *N/AmatchCountForIndexPtr

Ver.: always

Returns

  • sl_status_t status code


sl_zigbee_af_mac_address_filtering_get_stats#

void sl_zigbee_af_mac_address_filtering_get_stats (bool shortMode, uint32_t * allowedPacketCountPtr, uint32_t * droppedPacketCountPtr, uint32_t * totalPacketCountPtr)

Get MAC address filtering stats. Get the allowed, dropped and total packet counts.

Parameters
TypeDirectionArgument NameDescription
boolN/AshortMode

Ver.: always

uint32_t *N/AallowedPacketCountPtr

Ver.: always

uint32_t *N/AdroppedPacketCountPtr

Ver.: always

uint32_t *N/AtotalPacketCountPtr

Ver.: always


sl_zigbee_af_mac_address_filtering_filter_no_address#

void sl_zigbee_af_mac_address_filtering_filter_no_address (bool filterNoAddress)

Set the decision to manupulate the MAC address filtering tables.

Parameters
TypeDirectionArgument NameDescription
boolN/AfilterNoAddress

Ver.:always


sl_zigbee_af_mac_address_filtering_add_short_address#

void sl_zigbee_af_mac_address_filtering_add_short_address (sl_802154_short_addr_t nodeId)

Add the short address.

Parameters
TypeDirectionArgument NameDescription
sl_802154_short_addr_tN/AnodeId

Ver.:always


sl_zigbee_af_mac_address_filtering_add_long_address#

void sl_zigbee_af_mac_address_filtering_add_long_address (sl_802154_long_addr_t eui64)

Add the long address.

Parameters
TypeDirectionArgument NameDescription
sl_802154_long_addr_tN/Aeui64

Ver.:always


sl_zigbee_af_mac_address_filtering_add_pan_id#

void sl_zigbee_af_mac_address_filtering_add_pan_id (sl_802154_pan_id_t panId)

Add the panID.

Parameters
TypeDirectionArgument NameDescription
sl_802154_pan_id_tN/ApanId

Ver.:always


sl_zigbee_af_mac_address_filtering_set_short_address_list_type#

void sl_zigbee_af_mac_address_filtering_set_short_address_list_type (uint8_t * listType)

Set the short address list type.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/AlistType

Ver.:always, listType can be "set-whitelist" or "set-blacklist".


sl_zigbee_af_mac_address_filtering_set_long_address_list_type#

void sl_zigbee_af_mac_address_filtering_set_long_address_list_type (uint8_t * listType)

Set the long address list type.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/AlistType

Ver.:always, listType can be "set-whitelist" or "set-blacklist".


sl_zigbee_af_mac_address_filtering_set_pan_id_list_type#

void sl_zigbee_af_mac_address_filtering_set_pan_id_list_type (uint8_t * listType)

Set the list type of panId list.

Parameters
TypeDirectionArgument NameDescription
uint8_t *N/AlistType

Ver.:always, listType can be "set-whitelist" or "set-blacklist".


Enumeration Documentation#

sli_802154_mac_address_mode_t#

sli_802154_mac_address_mode_t
Enumerator
MAC_ADDRESS_MODE_NONE
MAC_ADDRESS_MODE_SHORT
MAC_ADDRESS_MODE_LONG

sli_802154_mac_filter_type_t#

sli_802154_mac_filter_type_t
Enumerator
MAC_FILTER_TYPE_NO_ADDRESS
MAC_FILTER_TYPE_SHORT_ADDRESS
MAC_FILTER_TYPE_LONG_ADDRESS
MAC_FILTER_TYPE_PAN_ID

sli_zigbee_filter_result_t#

sli_zigbee_filter_result_t
Enumerator
ALLOW_PACKET
DROP_PACKET

Typedef Documentation#

MacAddressFilterOptions#

typedef uint8_t MacAddressFilterOptions

Variable Documentation#

macAddressFilterData#

sli_802154_mac_address_filter_globals_t macAddressFilterData

zeroEui64#

const sl_802154_long_addr_t zeroEui64

Macro Definition Documentation#

expectCheckpoint#

#define expectCheckpoint

debug#

#define debug

SL_ZIGBEE_TEST_ASSERT#

#define SL_ZIGBEE_TEST_ASSERT

MAC_FILTER_OPTIONS_NO_ADDRESS_MASK#

#define MAC_FILTER_OPTIONS_NO_ADDRESS_MASK
Value:
  (1 << MAC_FILTER_TYPE_NO_ADDRESS)

MAC_FILTER_OPTIONS_SHORT_ADDRESS_LIST_MASK#

#define MAC_FILTER_OPTIONS_SHORT_ADDRESS_LIST_MASK
Value:
  (1 << MAC_FILTER_TYPE_SHORT_ADDRESS)

MAC_FILTER_OPTIONS_LONG_ADDRESS_LIST_MASK#

#define MAC_FILTER_OPTIONS_LONG_ADDRESS_LIST_MASK
Value:
  (1 << MAC_FILTER_TYPE_LONG_ADDRESS)

MAC_FILTER_OPTIONS_DEST_PAN_ID_LIST_MASK#

#define MAC_FILTER_OPTIONS_DEST_PAN_ID_LIST_MASK
Value:
  (1 << MAC_FILTER_TYPE_PAN_ID)

MAC_FILTER_OPTIONS_COUNT#

#define MAC_FILTER_OPTIONS_COUNT
Value:
4

MAC_FILTER_OPTIONS_DROP_NO_ADDRESS#

#define MAC_FILTER_OPTIONS_DROP_NO_ADDRESS
Value:
0x00

MAC_FILTER_OPTIONS_SHORT_ADDRESS_BLACKLIST#

#define MAC_FILTER_OPTIONS_SHORT_ADDRESS_BLACKLIST
Value:
0x00

MAC_FILTER_OPTIONS_LONG_ADDRESS_BLACKLIST#

#define MAC_FILTER_OPTIONS_LONG_ADDRESS_BLACKLIST
Value:
0x00

MAC_FILTER_OPTIONS_ALLOW_NO_ADDRESS#

#define MAC_FILTER_OPTIONS_ALLOW_NO_ADDRESS
Value:
0x01

MAC_FILTER_OPTIONS_SHORT_ADDRESS_WHITELIST#

#define MAC_FILTER_OPTIONS_SHORT_ADDRESS_WHITELIST
Value:
0x02

MAC_FILTER_OPTIONS_LONG_ADDRESS_WHITELIST#

#define MAC_FILTER_OPTIONS_LONG_ADDRESS_WHITELIST
Value:
0x04

MAC_FILTER_OPTIONS_DEST_PAN_ID_WHITELIST#

#define MAC_FILTER_OPTIONS_DEST_PAN_ID_WHITELIST
Value:
0x08

MAC_FILTER_OPTIONS_DEST_PAN_ID_BLACKLIST#

#define MAC_FILTER_OPTIONS_DEST_PAN_ID_BLACKLIST
Value:
0x00

BROADCAST_PAN_ID#

#define BROADCAST_PAN_ID
Value:
0xFFFF

MAC_FILTER_OPTIONS_DEFAULTS#

#define MAC_FILTER_OPTIONS_DEFAULTS
Value:
(MAC_FILTER_OPTIONS_SHORT_ADDRESS_BLACKLIST \
| MAC_FILTER_OPTIONS_LONG_ADDRESS_BLACKLIST \
| MAC_FILTER_OPTIONS_ALLOW_NO_ADDRESS \
| MAC_FILTER_OPTIONS_DEST_PAN_ID_BLACKLIST)

MAC_FRAME_CONTROL_FRAME_TYPE_MASK#

#define MAC_FRAME_CONTROL_FRAME_TYPE_MASK
Value:
0x0007

MAC_FRAME_CONTROL_FRAME_TYPE_BEACON#

#define MAC_FRAME_CONTROL_FRAME_TYPE_BEACON
Value:
0x0000

MAC_FRAME_CONTROL_FRAME_TYPE_DATA#

#define MAC_FRAME_CONTROL_FRAME_TYPE_DATA
Value:
0x0001

MAC_FRAME_CONTROL_FRAME_TYPE_ACK#

#define MAC_FRAME_CONTROL_FRAME_TYPE_ACK
Value:
0x0002

MAC_FRAME_CONTROL_FRAME_TYPE_COMMAND#

#define MAC_FRAME_CONTROL_FRAME_TYPE_COMMAND
Value:
0x0003

MAC_FRAME_CONTROL_VERSION_MASK#

#define MAC_FRAME_CONTROL_VERSION_MASK
Value:
0x3000

MAC_FRAME_CONTROL_VERSION_SHIFT#

#define MAC_FRAME_CONTROL_VERSION_SHIFT
Value:
12

MAC_FRAME_CONTROL_VERSION_2003#

#define MAC_FRAME_CONTROL_VERSION_2003
Value:
0x0000

MAC_FRAME_CONTROL_VERSION_2012#

#define MAC_FRAME_CONTROL_VERSION_2012
Value:
0x0002

MAC_FRAME_CONTROL_SOURCE_ADDRESS_MODE_SHIFT#

#define MAC_FRAME_CONTROL_SOURCE_ADDRESS_MODE_SHIFT
Value:
14

MAC_FRAME_CONTROL_ADDRESS_MODE_MASK#

#define MAC_FRAME_CONTROL_ADDRESS_MODE_MASK
Value:
0x0003

MAC_FRAME_CONTROL_ADDRESS_MODE_NONE#

#define MAC_FRAME_CONTROL_ADDRESS_MODE_NONE
Value:
0x0000

MAC_FRAME_CONTROL_ADDRESS_MODE_RESERVED#

#define MAC_FRAME_CONTROL_ADDRESS_MODE_RESERVED
Value:
0x0001

MAC_FRAME_CONTROL_ADDRESS_MODE_SHORT#

#define MAC_FRAME_CONTROL_ADDRESS_MODE_SHORT
Value:
0x0002

MAC_FRAME_CONTROL_ADDRESS_MODE_LONG#

#define MAC_FRAME_CONTROL_ADDRESS_MODE_LONG
Value:
0x0003

MAC_FRAME_CONTROL_DEST_ADDRESS_MODE_SHIFT#

#define MAC_FRAME_CONTROL_DEST_ADDRESS_MODE_SHIFT
Value:
10

MAC_FRAME_CONTROL_DEST_ADDRESS_MODE_NONE#

#define MAC_FRAME_CONTROL_DEST_ADDRESS_MODE_NONE
Value:
0x0000

MAC_FRAME_CONTROL_PANID_COMPRESSION#

#define MAC_FRAME_CONTROL_PANID_COMPRESSION
Value:
0x0040

WHITELIST_CHARACTER_INDEX#

#define WHITELIST_CHARACTER_INDEX
Value:
4