GATT Configurator User’s Guide for Bluetooth LE and Bluetooth Mesh#
Note: This section replaces UG438: GATT Configurator User’s Guide for Bluetooth LE and Bluetooth Mesh. Further updates to this user guide will be provided here.
This guide provides the information needed to effectively use the Bluetooth GATT Configurator provided as a part of Simplicity Studio® 5 with Bluetooth SDK 3.x and Bluetooth Mesh SDK 2.x. The GATT Configurator is an intuitive interface providing access to all the Profiles, Services, Characteristics, and Descriptors as defined in the Bluetooth specification. It also supports creating, importing, or exporting custom GATT profiles for Bluetooth applications. This guide reviews the user interface and covers some of the most common uses of the Configurator, and the usage of the Dynamic GATT Configurator.
Additional Information#
For more information on specific use cases in the GATT Configurator, see Bluetooth GATT Configurator.