sl_bt_evt_gatt_server_execute_write_completedGATT Server#

Execute write completed event indicates that the execute write command from a remote GATT client has completed with the given result.

Data Structures#

struct

sl_bt_evt_gatt_server_execute_write_completed_s

Data structure of the execute_write_completed event.

Macros#

# define

sl_bt_evt_gatt_server_execute_write_completed_id 0x040a00a0

Identifier of the execute_write_completed event.

Detailed Description#

Execute write completed event indicates that the execute write command from a remote GATT client has completed with the given result.


Data Structure Documentation#

◆ sl_bt_evt_gatt_server_execute_write_completed_s#

struct sl_bt_evt_gatt_server_execute_write_completed_s#

Data structure of the execute_write_completed event.

Data Fields

uint8_t

connection

Connection handle

uint16_t

result

Execute write result