sl_bt_evt_gatt_server_attribute_valueGATT Server#
Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.
Data Structures#
struct | sl_bt_evt_gatt_server_attribute_value_s | Data structure of the attribute_value event.
Macros#
define | sl_bt_evt_gatt_server_attribute_value_id 0x000a00a0#
| Identifier of the attribute_value event.
Detailed Description#
Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.
The parameter att_opcode describes which GATT procedure was used to change
the value.
Data Structure Documentation#
◆ sl_bt_evt_gatt_server_attribute_value_s#
struct sl_bt_evt_gatt_server_attribute_value_s#
Data structure of the attribute_value event.
Data Fields#
uint8_t | connection |
Connection handle
uint16_t | attribute |
Attribute Handle
uint8_t | att_opcode |
Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received.
uint16_t | offset |
Value offset
uint8array | value |
Value