sl_bt_evt_gatt_server_user_write_requestGATT Server#
Indicates that a remote GATT client is attempting to write a value of an attribute into the local GATT database, where the attribute was defined in the GATT database XML file to have the type="user".
Data Structures#
struct | sl_bt_evt_gatt_server_user_write_request_s | Data structure of the user_write_request event.
Macros#
define | sl_bt_evt_gatt_server_user_write_request_id#
0x020a00a0 | Identifier of the user_write_request event.
Detailed Description#
Indicates that a remote GATT client is attempting to write a value of an attribute into the local GATT database, where the attribute was defined in the GATT database XML file to have the type="user".
The parameter att_opcode informs which attribute procedure was used to write
the value. If the att_opcode is sl_bt_gatt_write_request
(see sl_bt_gatt_att_opcode_t), the application needs to respond to
this request by using the
sl_bt_gatt_server_send_user_write_response command within 30 seconds,
otherwise further GATT transactions are not allowed by the remote side. If the
att_opcode is sl_bt_gatt_prepare_write_request,
the application needs to respond to this request by using the
sl_bt_gatt_server_send_user_prepare_write_response command within 30 seconds,
otherwise further GATT transactions are not allowed by the remote side. If the
value of att_opcode is sl_bt_gatt_execute_write_request, it
indicates that there was one or more prepare writes earlier and now the GATT
server is processing the execute write, the value of characteristic is set
to 0 and should be ignored. The event
sl_bt_evt_gatt_server_execute_write_completed will be emitted after responding to
sl_bt_gatt_execute_write_request by
using sl_bt_gatt_server_send_user_write_response.
Data Structure Documentation#
◆ sl_bt_evt_gatt_server_user_write_request_s#
struct sl_bt_evt_gatt_server_user_write_request_s#
Data structure of the user_write_request event.
Data Fields#
uint8_t | connection |
Connection handle
uint16_t | characteristic |
GATT characteristic handle. This value is normally received from the gatt_characteristic event.
uint8_t | att_opcode |
Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received.
uint16_t | offset |
Value offset
uint8array | value |
Value